The implementation of this logger is fast with minimal stack usage
making it appropriate for a realtime application.
This logger writes all Log events to a circular buffer. As a
result, the execution time of all Log methods bound to this type
of logger are deterministic (and quite short) because there are no
additional memory allocation calls after the circular buffer was
allocated.
If this logger is used in a preemptive environment, then an appropriate
gate must be assigned to the module. For example, if events are generated
from an interrupt context, then a gate that disables interrupts
must be used.
enum LoggerBuf_BufType |
![](../../Arrow_up.png) |
Type of log buffer
typedef enum LoggerBuf_BufType {
LoggerBuf_BufType_CIRCULAR,
// The log buffer wraps, overwriting old entries
LoggerBuf_BufType_FIXED
// The log buffer halts collection when full
} LoggerBuf_BufType;
config LoggerBuf_E_badLevel // module-wide |
![](../../Arrow_up.png) |
Error raised if get or setFilterLevel receives a bad level value
extern const Error_Id LoggerBuf_E_badLevel;
config LoggerBuf_enableFlush // module-wide |
![](../../Arrow_up.png) |
Flush all logs at system exit
extern const Bool LoggerBuf_enableFlush;
config LoggerBuf_filterByLevel // module-wide |
![](../../Arrow_up.png) |
Support filtering of events by event level
extern const Bool LoggerBuf_filterByLevel;
DETAILS
To improve logging performance, this feature can be disabled by setting
filterByLevel to false.
See '
setFilterLevel' for an explanation of level filtering.
config LoggerBuf_level1Mask // module-wide |
![](../../Arrow_up.png) |
Mask of diags categories whose initial filtering level is Diags.LEVEL1
DETAILS
See '
level4Mask' for details.
config LoggerBuf_level2Mask // module-wide |
![](../../Arrow_up.png) |
Mask of diags categories whose initial filtering level is Diags.LEVEL2
DETAILS
See '
level4Mask' for details.
config LoggerBuf_level3Mask // module-wide |
![](../../Arrow_up.png) |
Mask of diags categories whose initial filtering level is Diags.LEVEL3
DETAILS
See '
level4Mask' for details.
config LoggerBuf_level4Mask // module-wide |
![](../../Arrow_up.png) |
Mask of diags categories whose initial filtering level is Diags.LEVEL4
DETAILS
If
IFilterLogger.filterByLevel is
true, then all
LoggerBuf instances will filter incoming events based on their
event level.
The LoggerBuf module allows for specifying a different filter level
for every Diags bit. These filtering levels are module wide;
LoggerBuf does not support specifying the levels on a per-instance
basis.
The
IFilterLogger.setFilterLevel function can be used to
change the filtering levels at runtime.
The default filtering levels are assigned using the level1Mask -
level4Mask config parameters. These are used to specify, for each of
the four event levels, the set of bits which should filter at that
level by default.
The default filtering configuration sets the filter level to
Diags.LEVEL4 for all logging-related diags bits so that all events
are logged by default.
config LoggerBuf_statusLogger // module-wide |
![](../../Arrow_up.png) |
Route all 'STATUS' (error and warning) events to this logger
DETAILS
If a statusLogger is specified, all LoggerBuf instances will check to
determine if any of the events they receive are errors or warnings (if
their diags mask includes the STATUS category), and will log these
events to the statusLogger.
Error events are infrequent, but it's generally critical that they be
seen. In a typical system, non-error events easily outnumber any error
events, and the logger is likely to wrap, overwriting any error events.
To protect these events from being overwritten and lost, they can be
sent to their own separate logger to preserve them.
The default value is null, indicating that the STATUS events will just
be logged by the logger they were sent to.
LoggerBuf_flushAll() // module-wide |
![](../../Arrow_up.png) |
Flush logs of all instances that set exitFlush to true
Void LoggerBuf_flushAll();
DETAILS
The user is responsible for making sure that no LoggerBuf instances
are created or deleted during the execution of this function.
Module-Wide Built-Ins |
![](../../Arrow_up.png) |
// Get this module's unique id
Bool LoggerBuf_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool LoggerBuf_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 LoggerBuf_Module_getMask();
// Returns the diagnostics mask for this module
Void LoggerBuf_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types |
![](../../Arrow_up.png) |
typedef struct LoggerBuf_Object LoggerBuf_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct LoggerBuf_Struct LoggerBuf_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
Instance Config Parameters |
![](../../Arrow_up.png) |
typedef struct LoggerBuf_Params {
// Instance config-params structure
// Common per-instance configs
// The heap that contains the Log buffer for dynamic instances
// Log buffer type
Bool exitFlush;
// Flush log at system exit
Int numEntries;
// Number of entries in buffer
} LoggerBuf_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
config LoggerBuf_bufHeap // instance |
![](../../Arrow_up.png) |
The heap that contains the Log buffer for dynamic instances
DETAILS
The default value
null means the buffer will be allocated from
the
Memory.defaultHeapInstance heap.
config LoggerBuf_bufType // instance |
![](../../Arrow_up.png) |
Log buffer type
config LoggerBuf_exitFlush // instance |
![](../../Arrow_up.png) |
Flush log at system exit
DETAILS
Only used when module parameter
enableFlush is
true.
config LoggerBuf_numEntries // instance |
![](../../Arrow_up.png) |
Number of entries in buffer
DETAILS
Each entry is large enough to store one
Log event containing up to
4 optional arguments. Events containing more than 4 arguments (such
as those from
Log.write5) use 2 entries.
numEntries must be a power of 2.
Instance Creation |
![](../../Arrow_up.png) |
// Allocate and initialize a new instance object and return its handle
// Initialize a new instance object inside the provided structure
ARGUMENTS
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
SEE
Instance Deletion |
![](../../Arrow_up.png) |
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
// Finalize the instance object inside the provided structure
LoggerBuf_disable() // instance |
![](../../Arrow_up.png) |
Disable a log
ARGUMENTS
handle
handle of a previously-created LoggerBuf instance object
DETAILS
Events written to a disabled log are silently discarded.
RETURNS
The function returns the state of the log (TRUE if enabled,
FALSE if disabled) before the call. This return value allows
clients to restore the previous state.
Note: not thread safe.
LoggerBuf_enable() // instance |
![](../../Arrow_up.png) |
Enable a log
ARGUMENTS
handle
handle of a previously-created LoggerBuf instance object
RETURNS
The function returns the state of the log (TRUE if enabled,
FALSE if disabled) before the call. This return value allows
clients to restore the previous state.
Note: not thread safe.
LoggerBuf_flush() // instance |
![](../../Arrow_up.png) |
Read, clear, and output the contents of the log
ARGUMENTS
handle
handle of a previously-created LoggerBuf instance object
DETAILS
This method reads, clears, and "prints" each
Log event (via
System.printf) in the log.
LoggerBuf_getFilterLevel() // instance |
![](../../Arrow_up.png) |
Returns the mask of diags categories currently set to the specified
level
ARGUMENTS
handle
handle of a previously-created LoggerBuf instance object
DETAILS
See '
setFilterLevel' for an explanation of level filtering.
LoggerBuf_getNextEntry() // instance |
![](../../Arrow_up.png) |
Fills the passed Log.EventRec with the next entry in the log
ARGUMENTS
handle
handle of a previously-created LoggerBuf instance object
evtRec
pointer to a supplied EventRec object where the next
entry in the log is copied to
DETAILS
This function is used to read and clear Log events from the
buffer maintained by the LoggerBuf instance. The Log event can
then be transmitted and displayed on a host.
A read pointer is maintained in the
LoggerBuf instance and
points to the next record to read. Entries are not necessarily
returned in chronological order, since buffers of type
BufType_CIRCULAR can wrap.
RETURNS
This function reports the number of entries actually read. The only
values that can be returned are:
- 0 no more entries to read
- 1 or 2 read a complete entry written by write4 or write8
- -1 cleared an incomplete/overwritten entry, more entries to read
LoggerBuf_reset() // instance |
![](../../Arrow_up.png) |
Reset a log to empty state and enable it
ARGUMENTS
handle
handle of a previously-created LoggerBuf instance object
WARNING
This method is not synchronized with other instance
methods and, as a result, it must never be called when there is a
chance that another instance method is currently in operation or
when another method on this instance may preempt this call.
LoggerBuf_setFilterLevel() // instance |
![](../../Arrow_up.png) |
Set the level of detail that instances will log
ARGUMENTS
handle
handle of a previously-created LoggerBuf instance object
mask
The diags categories to set the level for
filterLevel
The new filtering level for the specified
categories
DETAILS
Events with the specified level or higher will be logged, events
below the specified level will be dropped.
Events are filtered first by diags category, then by level. If an
event's diags category is disabled in the module's diags mask, then it
will be filtered out regardless of level. The event will not even be
passed to the logger.
This API allows for setting the filtering level for more than one
diags category at a time. The mask parameter can be a single category
or multiple categories combined, and the level will be set for all of
those categories.
LoggerBuf_write0() // instance |
![](../../Arrow_up.png) |
Process a log event with 0 arguments
ARGUMENTS
handle
handle of a previously-created LoggerBuf instance object
DETAILS
Same as write4 except with 0 arguments rather than 4.
SEE
LoggerBuf_write1() // instance |
![](../../Arrow_up.png) |
Process a log event with 1 arguments
ARGUMENTS
handle
handle of a previously-created LoggerBuf instance object
DETAILS
Same as write4 except with 1 arguments rather than 4.
SEE
LoggerBuf_write2() // instance |
![](../../Arrow_up.png) |
Process a log event with 2 arguments
ARGUMENTS
handle
handle of a previously-created LoggerBuf instance object
DETAILS
Same as write4 except with 2 arguments rather than 4.
SEE
LoggerBuf_write4() // instance |
![](../../Arrow_up.png) |
Process a log event with up to 4 arguments
ARGUMENTS
handle
handle of a previously-created LoggerBuf instance object
evt
event to be logged
mid
module ID of the module which logged the event
a1
arbitrary argument passed by caller
DETAILS
The
evt argument is of type Log.Event, which encodes the
Log.EventId, the
Diags.Mask, and the
Diags.EventLevel of the event. The event ID can be obtained
via
Types.getEventId(evt), the Diags mask can be obtained via
Diags.getMask(evt), and the event level can be obtained via
Diags.getLevel(evt).
The modId argument is the module ID of the module that logged the
event.
The event information can be used by the logger to handle different
events specially. For example, the event ID can be used to compare
against other known Log.Events.
if (Log_getEventId(MY_EVENT) == Log_getEventId(evt)) {
:
}
The Diags mask and event level can be used for filtering of events
based on event level (see
IFilterLogger), or even routing
events to separate loggers based on diags category (see, for example,
LoggerBuf.statusLogger).
The Diags mask and event level are useful for handling the event, but
are generally not recorded by the logger because they are not needed in
decoding and displaying the event. A more suitable value to record is a
Types.Event, which encodes the event ID and module ID. For
example, the
Log.EventRec type stores a
Types.Event
in its record definition. A
Types.Event can be created using
the
Types.makeEvent API given the event ID and module ID.
The event ID value of
0 is used to indicate an event triggered by a
call to one of the
Log_print[0-6] methods. These
methods take a format string rather than a
Log_Event argument and,
as a result, the event ID encoded in
evt is
0 and the parameter
a1 is the format string.
Non-zero event IDs can also be used to access the
msg string
associated with the
Log.EventDesc that originally
defined the
Log event.
Log_EventId id = Log_getEventId(evt));
if (id != 0) {
String msg = Text_ropeText(id);
System_aprintf(msg, a1, a2, a3, a4);
}
This works because an event's ID is simply an offset into a table
of characters (maintained by the
Text module)
containing the event's msg string.
The arguments a1, a2, etc. are parameters that are to be interpreted
according to the message format string associated with evt.
SEE
LoggerBuf_write8() // instance |
![](../../Arrow_up.png) |
Process a log event with up to 8 arguments
Void LoggerBuf_write8(
LoggerBuf_Handle handle,
Log_Event evt,
Types_ModuleId mid,
IArg a1,
IArg a2,
IArg a3,
IArg a4,
IArg a5,
IArg a6,
IArg a7,
IArg a8);
ARGUMENTS
handle
handle of a previously-created LoggerBuf instance object
DETAILS
Same as write4 except with 8 arguments rather than 4.
SEE
Instance Convertors |
![](../../Arrow_up.png) |
// unconditionally move one level up the inheritance hierarchy
// conditionally move one level down the inheritance hierarchy; NULL upon failure
// unconditionally move 2 levels up the inheritance hierarchy
// conditionally move 2 levels down the inheritance hierarchy; NULL upon failure
Instance Built-Ins |
![](../../Arrow_up.png) |
Int LoggerBuf_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object
proxy LoggerBuf.TimestampProxy |
![](../../Arrow_up.png) |
User supplied time-stamp proxy
XDCscript usage |
meta-domain |
// explicit access to the currently bound delegate module
DETAILS
This proxy allows
LoggerBuf to use a timestamp server different
from the server used by
xdc.runtime.Timestamp. However, if
not supplied by a user, this proxy defaults to whichever timestamp
server is used by
Timestamp.
enum LoggerBuf.BufType |
![](../../Arrow_up.png) |
Type of log buffer
XDCscript usage |
meta-domain |
values of type LoggerBuf.BufType
const LoggerBuf.BufType_CIRCULAR;
// The log buffer wraps, overwriting old entries
const LoggerBuf.BufType_FIXED;
// The log buffer halts collection when full
C SYNOPSIS
metaonly struct LoggerBuf.BasicView |
![](../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var obj = new LoggerBuf.BasicView;
obj.label = String ...
obj.lastSerial = Int ...
obj.numEntries = Int ...
obj.type = String ...
obj.enabledFlag = Bool ...
metaonly struct LoggerBuf.RecordView |
![](../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var obj = new LoggerBuf.RecordView;
obj.serial = Int ...
obj.timestampRaw = Long ...
obj.modName = String ...
obj.text = String ...
obj.eventId = Int ...
obj.eventName = String ...
obj.arg0 = IArg ...
obj.arg1 = IArg ...
obj.arg2 = IArg ...
obj.arg3 = IArg ...
obj.arg4 = IArg ...
obj.arg5 = IArg ...
obj.arg6 = IArg ...
obj.arg7 = IArg ...
metaonly struct LoggerBuf.StopModeData |
![](../../Arrow_up.png) |
Data added to the RTA MetaData file to support stop mode RTA
XDCscript usage |
meta-domain |
var obj = new LoggerBuf.StopModeData;
obj.bufferSymbol = String ...
obj.bufferSize = Int ...
config LoggerBuf.E_badLevel // module-wide |
![](../../Arrow_up.png) |
Error raised if get or setFilterLevel receives a bad level value
XDCscript usage |
meta-domain |
msg: "E_badLevel: Bad filter level value: %d"
};
C SYNOPSIS
config LoggerBuf.enableFlush // module-wide |
![](../../Arrow_up.png) |
Flush all logs at system exit
XDCscript usage |
meta-domain |
LoggerBuf.enableFlush = Bool false;
C SYNOPSIS
config LoggerBuf.filterByLevel // module-wide |
![](../../Arrow_up.png) |
Support filtering of events by event level
XDCscript usage |
meta-domain |
LoggerBuf.filterByLevel = Bool false;
DETAILS
To improve logging performance, this feature can be disabled by setting
filterByLevel to false.
See '
setFilterLevel' for an explanation of level filtering.
C SYNOPSIS
config LoggerBuf.level1Mask // module-wide |
![](../../Arrow_up.png) |
Mask of diags categories whose initial filtering level is Diags.LEVEL1
XDCscript usage |
meta-domain |
LoggerBuf.level1Mask = Bits16 0;
DETAILS
See '
level4Mask' for details.
C SYNOPSIS
config LoggerBuf.level2Mask // module-wide |
![](../../Arrow_up.png) |
Mask of diags categories whose initial filtering level is Diags.LEVEL2
XDCscript usage |
meta-domain |
LoggerBuf.level2Mask = Bits16 0;
DETAILS
See '
level4Mask' for details.
C SYNOPSIS
config LoggerBuf.level3Mask // module-wide |
![](../../Arrow_up.png) |
Mask of diags categories whose initial filtering level is Diags.LEVEL3
XDCscript usage |
meta-domain |
LoggerBuf.level3Mask = Bits16 0;
DETAILS
See '
level4Mask' for details.
C SYNOPSIS
config LoggerBuf.level4Mask // module-wide |
![](../../Arrow_up.png) |
Mask of diags categories whose initial filtering level is Diags.LEVEL4
XDCscript usage |
meta-domain |
DETAILS
If
IFilterLogger.filterByLevel is
true, then all
LoggerBuf instances will filter incoming events based on their
event level.
The LoggerBuf module allows for specifying a different filter level
for every Diags bit. These filtering levels are module wide;
LoggerBuf does not support specifying the levels on a per-instance
basis.
The
IFilterLogger.setFilterLevel function can be used to
change the filtering levels at runtime.
The default filtering levels are assigned using the level1Mask -
level4Mask config parameters. These are used to specify, for each of
the four event levels, the set of bits which should filter at that
level by default.
The default filtering configuration sets the filter level to
Diags.LEVEL4 for all logging-related diags bits so that all events
are logged by default.
C SYNOPSIS
config LoggerBuf.statusLogger // module-wide |
![](../../Arrow_up.png) |
Route all 'STATUS' (error and warning) events to this logger
XDCscript usage |
meta-domain |
DETAILS
If a statusLogger is specified, all LoggerBuf instances will check to
determine if any of the events they receive are errors or warnings (if
their diags mask includes the STATUS category), and will log these
events to the statusLogger.
Error events are infrequent, but it's generally critical that they be
seen. In a typical system, non-error events easily outnumber any error
events, and the logger is likely to wrap, overwriting any error events.
To protect these events from being overwritten and lost, they can be
sent to their own separate logger to preserve them.
The default value is null, indicating that the STATUS events will just
be logged by the logger they were sent to.
C SYNOPSIS
metaonly config LoggerBuf.common$ // module-wide |
![](../../Arrow_up.png) |
Common module configuration parameters
XDCscript usage |
meta-domain |
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
metaonly LoggerBuf.getMetaArgs() // module-wide |
![](../../Arrow_up.png) |
Returns any meta data needed to support RTA
XDCscript usage |
meta-domain |
LoggerBuf.getMetaArgs(Any inst, Any instNum) returns Any
DETAILS
This meta data should be returned in the form of a structure which
can be converted into XML. This data is added to the RTA XML file
during the application's configuration, and can be accessed later
through the xdc.rta.MetaData module.
The MetaData is returned per instance of the ILogger module. The
instance object is passed to the function as the first argument.
The second argument is the index of the instance in the list of
the ILogger's static instances.
Instance Config Parameters |
![](../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params = new LoggerBuf.Params;
// Instance config-params object
// The heap that contains the Log buffer for dynamic instances
params.bufSection = String null;
// Section name for the buffer managed by the static instance
// Log buffer type
params.exitFlush = Bool false;
// Flush log at system exit
params.numEntries = Int 64;
// Number of entries in buffer
config LoggerBuf.bufHeap // instance |
![](../../Arrow_up.png) |
The heap that contains the Log buffer for dynamic instances
XDCscript usage |
meta-domain |
var params = new LoggerBuf.Params;
...
DETAILS
The default value
null means the buffer will be allocated from
the
Memory.defaultHeapInstance heap.
C SYNOPSIS
config LoggerBuf.bufType // instance |
![](../../Arrow_up.png) |
Log buffer type
XDCscript usage |
meta-domain |
var params = new LoggerBuf.Params;
...
C SYNOPSIS
config LoggerBuf.exitFlush // instance |
![](../../Arrow_up.png) |
Flush log at system exit
XDCscript usage |
meta-domain |
var params = new LoggerBuf.Params;
...
params.exitFlush = Bool false;
DETAILS
Only used when module parameter
enableFlush is
true.
C SYNOPSIS
config LoggerBuf.numEntries // instance |
![](../../Arrow_up.png) |
Number of entries in buffer
XDCscript usage |
meta-domain |
var params = new LoggerBuf.Params;
...
params.numEntries = Int 64;
DETAILS
Each entry is large enough to store one
Log event containing up to
4 optional arguments. Events containing more than 4 arguments (such
as those from
Log.write5) use 2 entries.
numEntries must be a power of 2.
C SYNOPSIS
metaonly config LoggerBuf.bufSection // instance |
![](../../Arrow_up.png) |
Section name for the buffer managed by the static instance
XDCscript usage |
meta-domain |
var params = new LoggerBuf.Params;
...
params.bufSection = String null;
DETAILS
The default section is the 'dataSection' in the platform.
Instance Creation |
![](../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params =
new LoggerBuf.
Params;
// Allocate instance config-params
params.config = ...
// Assign individual configs
var inst = LoggerBuf.create(params);
// Create an instance-object
ARGUMENTS
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
SEE