1.3.7. Preprocessor Options

With the -E option, you can instruct the tiarmclang compiler to stop after the preprocessor phase of compilation:

-E, --preprocess

Halt compilation after running the C preprocessor.

1.3.7.1. Preprocessor Options

tiarmclang options that control the behavior of the C preprocessor:

-C, --comments

Include comments in preprocessed output.

-CC, --comments-in-macros

Include comments from within macros in preprocessed output.

-D<macro>=<value>

Define <macro> symbol to <value> (or 1 if <value> omitted).

-H, --trace-includes

Show header includes and nesting depth.

-P, --no-line-commands

Disable linemarker output in -E mode.

-U<macro>

Undefine <macro> symbol.

-Wp,<arg1>,<arg2>...

Pass the comma separated arguments in <argN> to the preprocessor.

-Xpreprocessor <option>

Pass <option> to the preprocessor.

1.3.7.2. Dependency File Generation

tiarmclang options that control generation of a dependency file for make-like build systems.

-M, --dependencies

Like -MD, but also implies -E and writes to stdout by default.

-MD, --write-dependencies

Write a dependency file containing user and system headers.

-MF<file>

Write dependency file output from -MMD, -MD, -MM, or -M to specified <file>.

-MG, --print-missing-file-dependencies

Add missing headers to dependency file.

-MJ<arg>

Write a compilation database entry per input.

-MM, --user-dependencies

Like -MMD, but also implies -E and writes to stdout by default.

-MMD, --write-user-dependencies

Write a dependency file containing user headers.

-MP

Create phony target for each dependency (other than main file).

-MQ<arg>

Specify name of main file output to quote in dependency file.

-MT<arg>

Specify name of main file output in dependency file

1.3.7.3. Dumping Preprocessor State

tiarmclang options that allow the state of the preprocessor to be dumped in various ways.

-dD

Print macro definitions in -E mode in addition to normal output.

-dI

Print include directives in -E mode in addition to normal output.

-dM

Print macro definitions in -E mode instead of normal output.