14.5. tiarmreadelf - Object File Reader¶
The tiarmreadelf tool displays low-level format-specific information about one or more object files.
14.5.1. Usage¶
tiarmreadelf [options] [filenames …]
tiarmreadelf - is the command used to invoke the object file reader.
options - affect the behavior of tiarmreadelf.
filenames - identifies one or more ELF object files as input to tiarmreadelf. If - is specified as the input file, tiarmreadelf will read its input from stdin.
14.5.2. Options¶
- --all¶
Equivalent to specifying all the main display options.
- --addrsig¶
Display the address-significance table.
- --arch-specific, -A¶
Display architecture-specific information.
- --color¶
Use colors in the output for warnings and errors.
- --demangle, -C¶
Display demangled C++ symbol names in the output.
- --dyn-relocations¶
Display the dynamic relocation entries.
- --dyn-symbols, --dyn-syms¶
Display the dynamic symbol table.
- --dynamic-table, --dynamic, -d¶
Display the dynamic table.
- --cg-profile¶
Display the callgraph profile section.
- --elf-hash-histogram, --histogram, -I¶
Display a bucket list histogram for dynamic symbol hash tables.
- --elf-linker-options¶
Display the linker options section.
- --elf-section-groups, --section-groups, -g¶
Display section groups.
- --expand-relocs¶
When used with the --relocations, --expand-relocs will instruct tiarmreadelf to display each relocation in an expanded multi-line format.
- --file-headers, -h¶
Display file headers.
- --hash-symbols¶
Display the expanded hash table with dynamic symbol data.
- --hash-table¶
Display the hash table for dynamic symbols.
- --headers, -e¶
Equivalent to combining the --file-headers, --program-headers, and --sections options.
- --help¶
Display a summary of command line options.
- --help-list¶
Display an uncategorized summary of command line options.
- --hex-dump=<section1>[,<section2>,...], -x¶
Display the specified <sectionN> as hexadecimal bytes. A given <sectionN> argument may be a section index or section name.
- --needed-libs¶
Display the needed libraries.
- --notes, -n¶
Display all notes.
- --program-headers, --segments, -l¶
Display the program headers.
- --raw-relr¶
Do not decode relocations in RELR relocation sections when displaying them.
- --relocations, --relocs, -r¶
Display the relocation entries in the file.
- --sections, --section-headers, -S¶
Display all sections.
- --section-data¶
When used with the --sections option, this option instructs tiarmreadelf to display section data for each section shown.
- --section-details, -t¶
Display all section details. Used as an alternative to the --sections option.
- --section-mapping¶
Display the section to segment mapping.
- --section-relocations¶
When used with the --sections option, this option instructs tiarmreadelf to display relocations for each section shown.
- --section-symbols¶
When used with the --sections option, the --section-symbols option will instruct tiarmreadelf to display symbols for each section shown.
- --stackmap¶
Display contents of the stackmap section.
- --string-dump=<section1>[,<section2>,...], -p¶
Display the specified <sectionN> as a list of strings. <sectionN> may be a section index or section name.
- --symbols, --syms, -s¶
Display the symbol table.
- --unwind, -u¶
Display stack unwinding information.
- --version¶
Display the version of the tiarmreadelf executable.
- --version-info, -V¶
Display version sections.
- @<file>¶
Read command-line options from specified <file>.
14.5.3. Exit Status¶
tiarmreadelf returns 0 under normal operation. It returns a non-zero exit code if there were any errors.