1.3.2. Processor Options

The tiarmclang compiler provides various options to control use of hardware-related functionality.

1.3.2.1. Select Processor

-mcpu=<arg>

Instruct the compiler to generate code for the Arm processor variant indicated by <arg>, where <arg> can be:

  • cortex-m0

  • cortex-m0plus

  • cortex-m3

  • cortex-m4

  • cortex-m33

Note

-mcpu=cortex-m33+nodsp - Disabling DSP Instructions on Cortex-M33

Adding the +nodsp extension to the -mcpu=cortex-m33 option will instruct the compiler to avoid generating DSP instructions when compiling code to be run on a Cortex-M33 device configured to disable the execution of DSP instructions.

To build a simple application intended to run on a Cortex-M33 device configured to disallow the execution of DSP instructions, specify the -mcpu=cortex-m33+nodsp option on the tiarmclang command-line, like so:

%> tiarmclang -mcpu=cortex-m33+nodsp -O3 myapp.c -o myapp.out -Wl,mylnk.cmd

If, at link-time, an object file compiled for a Cortex-M33 with DSP instructions disabled is combined with an object file or library compiled for a Cortex-M33 with DSP instructions enabled, the linker will emit an error diagnostic reporting an incompatibility between the input object files.

  • cortex-m55

  • cortex-m85

  • cortex-r4

  • cortex-r5

  • cortex-r52

Note

Enabling Use of CDE Intrinsics with *+cdecp0* Extension

The +cdecp0 extension can be appended to an -mcpu=cortex-m33, -mcpu=cortex-m33+nodsp, -mcpu=cortex-m55, or -mcpu=cortex-m85 option to enable use of CDE intrinsics on a Cortex-M33, M55, or M85 device equipped with a coprocessor that can execute CDE instructions. See Custom Datapath Extension (CDE) Intrinsics for more information.

1.3.2.2. Select Architecture

-march=<arg>

Instruct the compiler to generate code for the Arm architecture variant indicated by <arg>, where <arg> can be:

  • thumbv6m - appropriate for -mcpu=cortex-m0 or -mcpu=cortex-m0plus

  • thumbv7m - appropriate for -mcpu=cortex-m3

  • thumbv7em - appropriate for -mcpu=cortex-m4

  • thumbv8m.main - appropriate for -mcpu=cortex-m33

  • thumbv8-m.main - appropriate for -mcpu=cortex-m33

  • thumbv8.1m.main - appropriate for -mcpu=cortex-m55 or -mcpu=cortex-m85

  • thumbv8.1-m.main - appropriate for -mcpu=cortex-m55 or -mcpu=cortex-m85

  • armv7r - appropriate for -mcpu=cortex-r4 or -mcpu=cortex-r5 with -marm and -mlittle-endian

  • armv7reb - appropriate for -mcpu=cortex-r4 or -mcpu=cortex-r5 with -marm and -mbig-endian

  • armv8r - appropriate for -mcpu=cortex-r52 with -marm and -mlittle-endian

  • armv8reb - appropriate for -mcpu=cortex-r52 with -marm and -mbig-endian

  • thumbv7r - appropriate for -mcpu=cortex-r4 or -mcpu=cortex-r5 with -mthumb and -mlittle-endian

  • thumbebv7r - appropriate for -mcpu=cortex-r4 or -mcpu=cortex-r5 with -mthumb and -mbig-endian

  • thumbv8r - appropriate for -mcpu=cortex-r52 with -mthumb and -mlittle-endian

  • thumbv8reb - appropriate for -mcpu=cortex-r52 with -mthumb and -mbig-endian

Note

Enabling Use of CDE Intrinsics with *+cdecp0* Extension

The +cdecp0 extension can be appended to any of the following -march options:

  • -march=thumbv8m.main

  • -march=thumbv8-m.main

  • -march=thumbv8.1m.main

  • -march=thumbv8.1-m.main

to enable use of CDE intrinsics on a Cortex-M33, M55, or M85 device equipped with a coprocessor that can execute CDE instructions. See Custom Datapath Extension (CDE) Intrinsics for more information.

1.3.2.3. Select Instruction Set

-mthumb

Instruct the compiler to generate THUMB mode instructions (16-bit THUMB or T32 THUMB depending on which processor variant is selected) for current compilation; default for Cortex-M type architectures

-marm

Instruct the compiler to generate ARM mode instructions for current compilation; default for Cortex-R series processors

1.3.2.4. Select Floating-Point Code Generated

-mfloat-abi=<arg>

Instruct the compiler to generate code in accordance with the floating-point ABI indicated by <arg>, where <arg> can be:

  • hard - assume floating=point hardware (FPU) is available; pass floating-point type arguments and return values in FPU registers; generate FPU instructions for floating-point type operations

  • soft - assume no floating-point hardware is available; pass arguments and return values in general-purpose registers (GPRs); perform floating-point operations in software with CPU instructions or in calls to runtime support library functions.

-mfpu=<arg>

Instruct compiler to use floating-point hardware (FPU) registers and instructions to perform floating-point operations; select the FPU specified by <arg>, where <arg> can be:

  • vfpv3-d16 - available in combination with -mcpu=cortex-r4 or -mcpu=cortex-r5

  • neon-fp-armv8 - available in combination with -mcpu=cortex-r52

  • fpv4-sp-d16 - available in combination with -mcpu=cortex-m4

  • fpv5-sp-d16 - available in combination with -mcpu=cortex-m33

1.3.2.5. Select Endianness

-mlittle-endian, -EL

Instruct the compiler to generate little-endian object code; default.

-mbig-endian, -EB

Instruct the compiler to generate big-endian object code; only applicable for Cortex-R series processors.

1.3.2.6. Select Math Accelerator

-mmathacl

Enable hardware integer division routines using the MSPM0 IQmath accelerator. This accelerator is available only for TI MSPM0 Cortex-M0+ devices. See the MSPM0 IQMath User’s Guide for details about using this accelerator.