1.3.7. Optimization Options¶
To enable optimization passes in the tiarmclang compiler, select a level of optimization from among the following -O[0|1|2|3|g|s|z] options. In general, the options below represent various levels of optimization with some options designed to favor smaller compiler generated code size over performance, while others favor performance at the cost of increased compiler generated code size.
For a more precise list of optimizations performed for each level, please see Details of Optimizations Performed at Each Level.
1.3.7.1. Optimization Level Options¶
Note
Optimization Option Recommendations
The -Oz option is recommended if small compiler generated code size is a priority.
The -O3 option is recommended for optimizing performance, but it is likely to increase compiler-generated code size.
- -O0¶
Performs no optimization.
- -O1, -O¶
Enables restricted optimizations, providing a good trade-off between code size and debuggability. This option is recommended for maximum debuggability.
- -O2¶
Enables most optimizations, but disables some optimizations that may result in larger compiler-generated code size.
- -O3¶
Enables all optimizations available at -O2 plus others that may increase compiler-generated code size. This option is recommended for optimizing performance, but it is likely to increase code size.
- -Og¶
Enables restricted optimizations while preserving debuggability. All optimizations available at -O1 are performed with the addition of some optimizations from -O2.
By default, the -Og option enables the -fextend-variable-liveness=all option, which improves debuggability of user variables.
- -Os¶
Enables all optimizations available at -O2 plus additional optimizations designed to reduce code size. In comparison to the -Oz option, the -Os option avoids code size optimizations that are likely to harm performance.
- -Oz¶
Enables all optimizations available at -O2 plus additional optimizations designed to reduce code size. In comparison to the -Os option, the -Oz option performs additional code size optimizations that may harm performance. This optimization setting is recommended if small code size is a priority.
- -Ofast¶
This option is deprecated. It enables all optimizations available at -O3 plus additional aggressive optimizations that are not guaranteed to be in strict compliance with language standards. If you want this behavior, it is recommended that you use the -O3 option in combination with -ffast-math.
1.3.7.2. Link-Time Optimization¶
- -flto -O<1|2|3|fast|s|z>¶
When link-time optimization is enabled in the tiarmclang toolchain via the -flto compiler/linker option, the linker is able to combine all input object files into a merged representation of the application and present that representation back to the compiler where inter-module optimizations can be performed.
The types of inter-module optimizations that are performed depends on which of the -O<1|2|3|s|z> options is specified in combination with -flto:
-flto -O1 - perform basic inter-module optimizations.
-flto -O2 - perform all -O1 level inter-module optimizations plus performance-oriented inter-module optimizations, such as function inlining and global duplicate constant merging.
-flto -O3 - perform all -O2 level inter-module optimizations plus aggressive performance-oriented inter-module optimizations, like loop optimizations and call-site splitting. Performance improving inter-module optimizations are favored over code size reducing inter-module optimizations.
-flto -Os - perform all -O2 level inter-module optimizations, but several of these optimizations will favor reducing code size over improving performance.
-flto -Oz - perform all -O2 level inter-module optimizations plus other code size reducing optimizations, like machine outlining. Also, several -O2 optimizations are tuned to favor aggressive code size reduction even if performance is degraded.
1.3.7.3. More Specialized Optimization Options¶
1.3.7.3.1. Floating-Point Arithmetic¶
- -ffast-math, -fno-fast-math¶
Enable or disable ‘fast-math’ mode during compilation. By default, the ‘fast-math’ mode is disabled. Enabling ‘fast-math’ mode allows the compiler to perform aggressive, not necessarily value-safe, assumptions about floating-point math, such as:
Assume floating-point math is consistent with regular algebraic rules for real numbers (e.g. addition and multiplication are associative, x/y == x * 1/y, and (a + b) * c == a * c + b * c).
Operands to floating-point operations are never NaNs or Inf values.
+0 and -0 are interchangeable.
Enabling the -ffast-math option also causes the following options to be set:
-ffp-contract=fast
-fno-honor-nans
-ffp-model=fast
-fno-rounding-math
-fno-signed-zeros
Use of the ‘fast-math’ mode also instructs the compiler to predefine the __FAST_MATH__ macro symbol.
The deprecated -Ofast optimization option automatically enabled the -ffast-math option. If you want the behavior provided by the -Ofast option, it is recommended that you use the -O3 and -ffast-math options in combination.
- -ffp-model=<precise|strict|fast>¶
-ffp-model is an umbrella option that is used to establish a model of floating-point semantics that the compiler will operate under. The available arguments to the -ffp-model option will imply settings for the other, single-purpose floating-point options, including -ffast-math, -ffp-contract, and frounding-math (described below).
The available arguments to the -ffp-model option are:
precise - With the exception of floating-point contraction optimizations, all other optimizations that are not value-safe on floating-point data are disabled (ffp-contract=on and -fno-fast-math). The tiarmclang compiler assumes this floating-point model by default.
strict - Disables floating-point contraction optimizations (-ffp-contract=off), honors dynamically-set floating-point rounding modes (-frounding-math), and disables all ‘fast-math’ floating-point optimizations (-fno-fast-math). Also sets -ffp-exception-behavior=strict.
fast - Enables all ‘fast-math’ floating-point optimizations (-ffast-math) and enables floating-point contraction optimizations across C/C++ statements (-ffp-contract=fast).
- -ffp-contract=<fast|on|off|fast-honor-pragmas>¶
Instruct the compiler whether and to what degree it is allowed to form fused floating-point operations, such as floating-point multiply and add (FMA) instructions. This optimization is also known as floating-point contraction. Fused floating-point operations are permitted to produce more precise results than would be otherwise computed if the operations were performed separately.
The available arguments to the -ffp-contract option are:
fast - Allows fusing of floating-point operations across C/C++ statements, and ignores any FP_CONTRACT or clang fp contract pragmas that would otherwise affect the compiler’s ability to apply floating-point contraction optimizations.
on - Allows floating-point contraction within a given C/C++ statement. The floating-point contraction behavior can be affected by the use of FP_CONTRACT or clang fp contract pragmas.
off - Disables all floating-point contraction optimizations.
fast-honor-pragma - Same as the fast argument, but the user can alter the behavior via the use of the FP_CONTRACT and/or clang fp contract pragmas.
- -ffp-exception-behavior=<ignore|strict|maytrap>¶
This option determines the behavior in coordination with potential floating-point hardware exceptions.
ignore - This is the default setting. The compiler expects exception status flags to not be read and floating point exceptions to be masked.
maytrap - This setting causes the compiler to avoid performing floating point transformations that may raise exceptions if the original code would not have raise them. The compiler may still perform constant folding.
strict - This setting causes the compiler to strictly preserve the floating point exception semantics of the original code when performing any floating point transformations. Setting -ffp-model=strict causes -ffp-exception-behavior to be set to strict.
The maytrap and strict settings also prevent the following optimizations:
Floating point instruction speculation
Hoisting floating point instructions into code where they may execute despite guard conditions that would otherwise prevent their execution
Floating-Point Speculation Example
Consider a floating-point divide operation that is guarded by an if statement in a C function:
__attribute__((noinline)) void cp_fpu_trace(float32 *f_Info) { float32 f_array[10] = {0}; float32 float1 = *f_Info; if (float1 > CP_MIN) { f_array[1u] = (1.f / *f_Info); } else { f_array[1u] = CP_MAX; } *f_Info = f_array[1u]; }
In this code the if statement is intended to prevent the floating-point divide operation from performing a divide-by-zero that will trigger a hardware floating-point exception. However, if optimization is enabled to perform floating-point speculation, the compiler may generate code to perform the divide instruction prior to the compare instruction that carries out the intent of the if statement:
... cp_fpu_trace: vldr s0, [r0] vmov.f32 s2, #1.000000e+00 vldr s4, .LCPI1_0 ; <- load of CP_MIN vldr s6, .LCPI1_1 ; <- load of CP_MAX vdiv.f32 s2, s2, s0 ; <- divide vcmp.f32 s0, s4 ; <- compare vmrs APSR_nzcv, fpscr vmovgt.f32 s6, s2 ; <- conditional move: ; if (float1 > CP_MIN) ; s6 = result of divide vstr s6, [r0] bx lr ...
In this case, if the value loaded into s0 is zero, then the divide instruction will trigger a floating-point hardware exception before the compare instruction has a chance to prevent that from happening. As mentioned above, including the -ffp-exception-behavior=maytrap or -ffp-exception-behavior=strict option on the compiler command-line will prevent the compiler from performing floating-point speculation optimizations and generating code that will execute the divide instruction prior to the compare and conditional move instructions.
- -fhonor-nans, -fno-honor-nans¶
Instructs the compiler to check for and properly handle floating-point NaN values. Use of the -fno-honor-nans can improve code if the compiler can assume that it doesn’t need to check for and enforce the proper handling of floating-point NaN values.
- -frounding-math, -fno-rounding-math¶
By default, the compiler assumes that the -fno-rounding-mode option is in effect. This instructs the compiler to always round-to-nearest for floating-point operations.
The C standard runtime library provides functions such as fesetround and fesetenv that allow you to dynamically alter the floating-point rounding mode. If the -frounding-math option is specified, the compiler honors any dynamically-set floating-point rounding mode. This can be used to prevent optimizations that may affect the result of a floating-point operation if the current rounding mode has changed or is different from the default (round-to-nearest). For example, floating-point constant folding may be inhibited if the result is not exactly representable.
- -fsigned-zeros, -fno-signed-zeros¶
Assumes the presence of signed floating-point zero values. Use of the -fno-signed-zeros option can improve code if the compiler can assume that it doesn’t need to account for the presence of signed floating-point zero values.
1.3.7.3.2. Inlining and Outlining¶
- -finline-functions, -fno-inline-functions¶
Inline suitable functions. The -fno-inline-functions option disables this optimization.
- -finline-hint-functions¶
Inline functions that are explicitly or implicitly marked as inline.
- -mllvm -arm-memset-max-stores=<n>¶
When optimization is turned on during a compilation, the tiarmclang compiler inlines calls to the memset and memclr runtime support routines if the size of the data is below a certain threshold. For example, in the following source file:
#include <string.h> struct { int t1; int t2; int t3; int t4; short t5; long t6; } my_struct_inline; void func() { memset(&my_struct_inline, 0, sizeof(my_struct_inline)); }
When compiled with -O[1|2|3], the call to memset is inlined if the clearing of the my_struct_inline data object can be done with <= 8 store instructions:
%> tiarmclang -mcpu=cortex-m0 -O3 -S struct_inline.c %> cat struct_inline.s ... func: ldr r0, .LCPI0_0 movs r1, #0 str r1, [r0] str r1, [r0, #4] str r1, [r0, #8] str r1, [r0, #12] str r1, [r0, #16] str r1, [r0, #20] bx lr .p2align 2 .LCPI0_0: .long my_struct_inline ...
However, when compiled with -O[s|z}, where the compiler is attempting to generate smaller code, the call to memset is inlined only if clearing the my_struct_inline data object can be done with <= 4 store instructions. When compiled in combination with the -mcpu=cortex-m0 option, the call to memset is not inlined, but it will be implemented with a call to __aeabi_memclr:
%> tiamclang -mcpu=cortex-m0 -Oz -S struct_inline.c %> cat struct_inline.s ... func: push {r7, lr} ldr r0, .LCPI0_0 movs r1, #24 bl __aeabi_memclr4 pop {r7, pc} .p2align 2 .LCPI0_0: .long my_struct_inline
The -mllvm -arm-memset-max-stores=<n> option allows you to control the criteria used by the compiler to decide whether or not to inline a call to the memset or memclr function. If the above example is re-compiled with -mcpu=cortex-m0 -Oz -mllvm -arm-memset-max_stores=6, then the call to memset will get inlined since the clearing of my_struct_inline can be accomplished on Cortex-M0 with 6 store instructions:
%> tiarmclang -mcpu=cortex-m0 -Oz -mllvm -arm-memset-max-stores=6 -S struct_inline.c %> cat struct_inline.s ... func: ldr r0, .LCPI0_0 movs r1, #0 str r1, [r0] str r1, [r0, #4] str r1, [r0, #8] str r1, [r0, #12] str r1, [r0, #16] str r1, [r0, #20] bx lr .p2align 2 .LCPI0_0: .long my_struct_inline ...
The optimal value for the argument <n> to use with the -mllvm -arm-memset-max-stores=<n> option will vary depending on each particular use-case. Adjusting this value will only be beneficial if you are able to control the limit as needed.
Note
Use Caution When Defining Symbols Inside an asm() Statement
Inlining a function that contains an asm() statement that contains a symbol definition when compiling with the tiarmclang compiler can cause a “symbol multiply defined” error.
Please see Inlining Functions that Contain asm() Statements for more details.
- -moutline¶
Function outlining (aka “machine outlining”) is an optimization that saves code size by identifying recurring sequences of machine code and replacing each instance of the sequence with a call to a new function that the identified sequence of operations.
Function outlining is enabled when the -Oz option is specified on the tiarmclang command line. There are 3 settings for the function outlining optimization when using the -Oz option:
The -moutline option is the default setting; it performs machine outlining within functions. This is less aggressive than -moutline-inter-function, but it is guaranteed to be applied only when doing so will reduce the net code size.
- -moutline-inter-function¶
The -moutline-inter-function option can be specified in combination with the -Oz option to enable inter-function outlining. While this is the more aggressive of the function outlining settings, it does not always guarantee an overall code size reduction if, for example, outlining occurs across multiple functions in a given compilation unit yet only one of those functions is included in the linked application, the application will include the outlined code as well as the additional instructions required to call that code. However, it is likely to be beneficial when all functions defined in a given compilation unit are included in the linked application.
- -mno-outline¶
The -mno-outline option can be used to disable function outlining for a given compilation unit when using the -Oz option.
1.3.7.3.3. Loop Unrolling¶
- -funroll-loops, -fno-unroll-loops¶
Enable optimizer to unroll loops. The -fno-unroll-loops option disables this optimization.
1.3.7.3.4. Variable Liveness¶
- -fextend-variable-liveness=[all|this|none]¶
This option causes user variables (and the this pointer in C++ non-static member functions) to remain “live” during compilation so that they are not optimized out. The result is easier debugging and profiling, but less efficient generated code. This behavior is useful when debugging applications that require some level of optimization in order to run.
The possible settings are as follows:
all This setting causes all user variables and the “this” pointer to remain live. This is the default if the -fextend-variable-liveness option is used with no setting specified. The -Og option enables this setting by default.
this Only the “this” pointer in C++ non-static member functions remains live.
none Variables may be optimized out by the compiler. This is the same as not specifying the -fextend-variable-liveness option at all.
1.3.7.4. Details of Optimizations Performed at Each Level¶
This table lists examples of optimizations performed at each optimization level. (These optimizations are not listed in the order they are performed.)
Optimization Level |
Optimizations Performed |
|---|---|
|
None |
|
|
|
|
|
|
|
|
|
|
|
|