10.11.3. Setting the Size of the Stack and Heap Sections¶
The C/C++ language uses two uninitialized sections called .sysmem and .stack for the memory pool used by the malloc( ) functions and the run-time stacks, respectively. You can set the size of these by using the --heap_size or --stack_size option and specifying the size of the section as a 4-byte constant immediately after the option. If the options are not used, the default size of the heap is 2K bytes and the default size of the stack is 2K bytes.
See Define Heap Size (--heap_size Option) for setting heap sizes and Define Stack Size (--stack_size Option) for setting stack sizes.
To debug issues related to the stack size, we recommend using the CCS Stack Usage view to see the static stack usage of each function in the application. See Stack Usage View in CCS for more information. Using the Stack Usage View requires that source code be built with debug enabled. This feature relies on the –call_graph capability provided by the tiarmofd - Object File Display Utility.