10.3. Invoking the Linker

The default behavior of the tiarmclang compiler is to compile specified C, C++, or assembly source files into temporary object files and then pass those object files along with any explicitly specified object files and any specified linker options to the linker.

Alternately, if you specify only object files as input to the tiarmclang compiler, the compiler passes those files to the linker along with any specified options that are applicable to the link.

10.3.3. Passing Options to the Linker

The tiarmclang command line provides the following ways to pass options to the linker:

  • The -Wl option passes a comma-separated list of options to the linker.

  • The -Xlinker option passes a single option to the linker and can be used multiple times on the same command line.

  • A linker command file can specify options to pass to the linker.

For example, the following command line passes several linker options using the -Wl option:

tiarmclang -mcpu=cortex-m0 hello.c -o a.out -Wl,-stack=0x8000,--ram_model,link_test.cmd

The following command line passes the same linker options using the -Xlinker option:

tiarmclang -mcpu=cortex-m0 hello.c -o a.out -Xlinker -stack=0x8000 -Xlinker --ram_model
-Xlinker link_test.cmd

The following lines from a linker command file, pass the same linker options to the linker:

/*********************************************************************/
/* Example Linker Command File                                       */
/*********************************************************************/
-stack  0x8000                  /* SOFTWARE STACK SIZE               */
--ram_model                     /* INITIALIZE VARIABLES AT LOAD TIME */

10.3.4. File and Path Names Containing Special Characters

A reference to a normal file name, such as file.o in a link command line or in a linker command file is handled as expected by the linker. You can also specify path information or include special characters, like hyphens, in a file name specification. In most cases, a file name specification containing path information should be properly interpreted by the linker, but in some cases, especially when a file name specification contains a special character, like a hyphen, you should enclose the file name specification in double-quotes to ensure that it is properly interpreted.

Specifically in the case of a hyphen, the reason that a file name specification containing a hyphen must be enclosed in double-quotes is because a hyphen can be legitimately interpreted as a subtraction operator.

For example, file or library names containing hyphens referenced in a linker command file without enclosing double-quotes cause problems at link time:

SECTIONS
{
  ....

  .mytext1    : { lib-with-dashes.lib(.text) } > 0x00010000
  .mytext2    : { name-with-dashes.o(.text)  } > 0x10000000

  ...
}
%> tiarmlnk.cmd -mcpu=cortex-m4 name-with-dashes.o -o a.out -Wl,badlnk.cmd,-ma.map
"badlnk.cmd", line 24: error: cannot find file "lib"
"badlnk.cmd", line 24: error: -l must specify a filename
"badlnk.cmd", line 24: error: cannot find file "with"
"badlnk.cmd", line 24: error: cannot find file "dashes.lib"
"badlnk.cmd", line 25: error: cannot find file "name"
"badlnk.cmd", line 25: error: -l must specify a filename
"badlnk.cmd", line 25: error: cannot find file "with"
"badlnk.cmd", line 25: error: cannot find file "dashes.o"
"badlnk.cmd", line 24: warning: no matching section
"badlnk.cmd", line 25: warning: no matching section
"badlnk.cmd", line 24: warning: no matching section
"badlnk.cmd", line 24: warning: no matching section
"badlnk.cmd", line 25: warning: no matching section
"badlnk.cmd", line 25: warning: no matching section

undefined first referenced
 symbol       in file
--------- ----------------
my_func   name-with-dashes.o

error: unresolved symbols remain
error: errors encountered during linking; "a.out" not built

If the referenced file names are enclosed in double-quotes, the link succeeds:

SECTIONS
{
  ....

  .mytext1    : { "lib-with-dashes.lib"(.text) } > 0x00010000
  .mytext2    : { "name-with-dashes.o"(.text)  } > 0x10000000

  ...
}
%> tiarmlnk.cmd -mcpu=cortex-m4 name-with-dashes.o -o a.out -Wl,goodlnk.cmd,-ma.map
%> cat a.map
...
SECTION ALLOCATION MAP

 output                                  attributes/
section   page    origin      length       input sections
--------  ----  ----------  ----------   ----------------
...

.mytext1   0    00010000    00000018
                  00010000    00000010     lib-with-dashes.lib : my-func.o (.text.my_func)
                  00010010    00000008     libc.a : printf.c.obj (.tramp.printf.1)

.mytext2   0    10000000    0000001c
                  10000000    00000014     name-with-dashes.o (.text.main)
                  10000014    00000008     lib-with-dashes.lib : my-func.o (.tramp.my_func.1)

It is recommended that if your file name specification contains unusual or special characters that might not be interpreted by the linker as an obvious part of a file or path name, then you should try enclosing your file name specification in double-quotes to ensure that it is properly interpreted.

10.3.5. Wildcards in File, Section, and Symbol Patterns

The linker allows file, section, and symbol names to be specified using the asterisk (*) and question mark (?) wildcards. Using * matches any number of characters. Using ? matches a single character. Wildcards can make it easier to handle related objects, provided they follow a suitable naming convention.

For example:

mp3*.o      /* matches anything .o that begins with mp3    */
task?.o*    /* matches task1.o, task2.c.o, taskX.o55, etc. */

SECTIONS
{
    .fast_code: { *.o(*fast*) }                > FAST_MEM
    .vectors  : { vectors.c.o(.vector:part1:*) > 0xFFFFFF00
    .str_code : { rts*.lib<str*.c.o>(.text) }  > S1ROM
}

10.3.6. Specifying C/C++ Symbols with Linker Options

The link-time symbol is the same as the high-level language name.

For more information on symbol names, see tiarmnm - Name Utility. For information specifically about C++ symbol naming, see tiarmdem - C++ Name Demangler Utility. See Using Linker Symbols in C/C++ Applications for information about referring to linker symbols in C/C++ code.