7.7.8.32. GEL_HandleTargetError()¶
Handle error messages from the target driver
Syntax
GEL_HandleTargetError( regex, newText, replaceText, buttonText, handlerExpression );
Parameters
regex: is a string that is used to match against the target error messages
newText: is a string to be appended to whatever the driver returns. It can be blank. If replaceText is true, it replaces the driver error text.
replaceText: is a boolean indicating whether the text returned by the driver should be replaced by newText.
buttonText: is a string to be used as the name of a new button in the error dialog. It will be ignored if it is blank.
handlerExpression: is a string representing the GEL expression to be executed when the button is pressed.
Description
This function lets a GEL script update and/or replace the text of a specific error, and also add its own optional handling of the problem.
UI requests are not blocked while the handler expression is executing.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: No
Example
GEL_HandleTargetError(
".*-1170.*",
"\nNo connection possible. You have the option to either toggle reset or try to use SWD instead.\n ",
0,
"Toggle RST",
"MSP432_Board_Reset()"
);