7.7.8.8. GEL_BreakPtDisable¶
Disables a software breakpoint at the specified address.
Syntax
GEL_BreakPtDisable( address );
Parameters
address: specifies the location of the software breakpoint.
Description
The software breakpoint at the specified address is disabled. If the breakpoint does not exist or is already disabled, no action is taken. This function will not disable the breakpoint if it is a hardware breakpoint.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: No
Example
GEL_BreakPtDisable(0x2000);
GEL_BreakPtDisable(main + 100);
Related Topics