7.7.8.7. GEL_BreakPtDel()¶
Delete a breakpoint.
Syntax
GEL_BreakPtDel( address );
Parameters
address: identifies the location of the breakpoint.
Description
This function clears a software breakpoint at a specific address. If there is no software breakpoint set at address, nothing happens. The address can be an absolute address, any C expression, the name of a C function, or the name of an assembly language label.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: No
Example
GEL_BreakPtDel(0x2000);
GEL_BreakPtDel(TargetLabel + 100);
Related Topics