7.9.8.103. OnTargetConnect()ΒΆ
Called every time a target is connected.
Format
OnTargetConnect()
Parameters
None
Description
OnTargetConnect() is called every time a target is connected. Its execution will finish before anything else occurs. Note: If you connect to the target in real-time mode, you can connect unobtrusively and leave the target in a running state. Issuing a command in OnTargetConnect() that modifies the target state (such as GEL_Reset), will halt the target and defeat the ability to connect unobtrusively.
Example
OnTargetConnect()
Related Topics