7.9.8.87. GEL_SyncStepOverΒΆ

Performs a StepOver operation on every target that is in the same group as the current target.

Format

GEL_SyncStepOver([iterations]);

Parameters

iterations(optional) specifies the number of times the command is to be repeated. If iterations is not specified, a single StepOver is performed.

Description

Performs a StepOver operation on every target that is in the same group as the current target. The operation performed is the same as the StepOver option selected from the PDM debug menu.

As with the other synchronous operations, the operation is performed on all targets simultaneously.

Synchronous

Synchronous from GEL: No

Completely synchronous: No

Example

GEL_SyncStepOver(5);

GEL_SyncStepOver ( );

Related Topics

GEL_SyncStepOut

GEL_SyncStepInto

GEL_SyncRun

GEL_SyncHalt