7.9.8.62. GEL_Restart()ΒΆ
Resets the PC to the program entry point.
Syntax
GEL_Restart();
Parameters
None.
Description
The GEL_Restart() function resets the program to its entry point. This assumes that a program (with symbol information) has been loaded into the target and the target program is able to be restarted. If the target program relies on the loader to initialize various RAM locations, the program may not function correctly after being restarted.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: Yes
Example
GEL_Reset();
Related Topics