|
MAVRK Embedded Software 0.91
Software Libraries for the MAVRK motherboard and related components
|
Files | |
| file | Generic_Temp_Sensor.h [code] |
| file | Generic_Temp_Sensor_Functions.c |
Functions related to TMP20 sensor functionality. | |
| file | Generic_Temp_Sensor_PC_Interface_Command_Decode.c |
Decodes command coming from the PC. | |
| file | Humidity_Sensor.h [code] |
| file | Humidity_Sensor_Functions.c |
Functionality pertaining to humidity sensor. | |
| file | Humidity_Sensor_PC_Interface_Command_Decode.c |
Used to decode the commands coming from the PC QT GUI for the humidity sensor. | |
| file | Light_Sensor.h [code] |
| file | Light_Sensor_Functions.c |
Used for light sensor functions that perform various light sensor tasks. | |
| file | Light_Sensor_PC_Interface_Command_Decode.c |
Used to decode commands comming from the PC QT interface, specifically for the lights sensor. | |
| file | Passive_Sensor.h [code] |
| file | Passive_Sensor_API.c |
Performs PC Interface functions between a Passive Sensor part and the PC Interface. | |
1.7.3