MAVRK Embedded Software 0.91
Software Libraries for the MAVRK motherboard and related components

Passive_Sensor_Template Directory Reference

Files

file  Generic_Temp_Sensor.h [code]
file  Generic_Temp_Sensor_Functions.c
 

Functions related to TMP20 sensor functionality.


file  Generic_Temp_Sensor_PC_Interface_Command_Decode.c
 

Decodes command coming from the PC.


file  Humidity_Sensor.h [code]
file  Humidity_Sensor_Functions.c
 

Functionality pertaining to humidity sensor.


file  Humidity_Sensor_PC_Interface_Command_Decode.c
 

Used to decode the commands coming from the PC QT GUI for the humidity sensor.


file  Light_Sensor.h [code]
file  Light_Sensor_Functions.c
 

Used for light sensor functions that perform various light sensor tasks.


file  Light_Sensor_PC_Interface_Command_Decode.c
 

Used to decode commands comming from the PC QT interface, specifically for the lights sensor.


file  Passive_Sensor.h [code]
file  Passive_Sensor_API.c
 

Performs PC Interface functions between a Passive Sensor part and the PC Interface.


 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines