8.2. Quantization

Quantization reduces model precision from 32-bit floating point to lower bit widths (8-bit, 4-bit, or 2-bit integers), dramatically reducing model size and improving inference speed.

8.2.1. Overview

Why quantize?

  • Smaller models: 4x reduction (float32 → int8)

  • Faster inference: Integer operations are faster

  • NPU requirement: TI’s NPU requires quantized models

  • Lower power: Reduced memory bandwidth

8.2.2. Configuration Parameters

Quantization in Tiny ML Tensorlab is controlled by four parameters in the training section of the config YAML:

Option

Values

Description

quantization

0, 1, 2

Quantization mode. 0 = floating point training (no quantization). 1 = standard PyTorch Quantization. 2 = TI style optimised Quantization.

quantization_method

'PTQ', 'QAT'

Quantization method. Only applicable when quantization is 1 or 2.

quantization_weight_bitwidth

8, 4, 2

Bit width for weight quantization. Only applicable when quantization is 1 or 2.

quantization_activation_bitwidth

8, 4, 2

Bit width for activation quantization. Only applicable when quantization is 1 or 2.

Note

quantization_method, quantization_weight_bitwidth, and quantization_activation_bitwidth are only used when quantization is set to 1 or 2. When quantization is 0 (floating point training), these parameters have no effect.

8.2.3. Quantization Modes

Floating Point Training (quantization: 0)

Standard float32 training with no quantization applied:

training:
  model_name: 'CLS_4k_NPU'
  quantization: 0

Standard PyTorch Quantization (quantization: 1)

Uses standard PyTorch quantization APIs (GenericTinyMLQATFxModule / GenericTinyMLPTQFxModule). Suitable for general-purpose CPU deployment:

training:
  model_name: 'CLS_4k'
  quantization: 1
  quantization_method: 'QAT'
  quantization_weight_bitwidth: 8
  quantization_activation_bitwidth: 8

For more details on the underlying wrappers, see Quantization Wrapper Architecture below.

TI Style Optimised Quantization (quantization: 2)

Uses TI’s NPU-optimised quantization (TINPUTinyMLQATFxModule / TINPUTinyMLPTQFxModule). This incorporates the constraints of TI NPU Hardware accelerator and is required for NPU deployment:

training:
  model_name: 'CLS_4k_NPU'
  quantization: 2
  quantization_method: 'QAT'
  quantization_weight_bitwidth: 8
  quantization_activation_bitwidth: 8

8.2.4. Quantization Methods

Post-Training Quantization (PTQ)

Quantizes a trained float model after training:

training:
  model_name: 'CLS_4k_NPU'
  quantization: 2
  quantization_method: 'PTQ'
  quantization_weight_bitwidth: 8
  quantization_activation_bitwidth: 8
  • Pros: Fast, simple, no retraining required

  • Cons: May lose accuracy for some models

Quantization-Aware Training (QAT)

Simulates quantization during training for better accuracy retention:

training:
  model_name: 'CLS_4k_NPU'
  quantization: 2
  quantization_method: 'QAT'
  quantization_weight_bitwidth: 8
  quantization_activation_bitwidth: 8
  • Pros: Better accuracy retention

  • Cons: Longer training time

8.2.5. Bit Widths

8-bit Quantization

Most common choice, good accuracy retention:

training:
  quantization: 2
  quantization_method: 'QAT'
  quantization_weight_bitwidth: 8
  quantization_activation_bitwidth: 8
  • Model size: 4x smaller than float32

  • Accuracy loss: Usually <1%

4-bit Quantization

Aggressive compression for size-constrained devices:

training:
  quantization: 2
  quantization_method: 'QAT'
  quantization_weight_bitwidth: 4
  quantization_activation_bitwidth: 4
  • Model size: 8x smaller than float32

  • Accuracy loss: 1-5% typical

2-bit Quantization

Maximum compression, limited use cases:

training:
  quantization: 2
  quantization_method: 'QAT'
  quantization_weight_bitwidth: 2
  quantization_activation_bitwidth: 2
  • Model size: 16x smaller than float32

  • Accuracy loss: Can be significant

Note

Weight and activation bit widths can be set independently. For example, you can use 8-bit activations with 4-bit weights:

training:
  quantization: 2
  quantization_method: 'QAT'
  quantization_weight_bitwidth: 4
  quantization_activation_bitwidth: 8

8.2.6. NPU Quantization Requirements

TI’s NPU requires TI style optimised quantization (quantization: 2):

common:
  target_device: 'F28P55'

training:
  model_name: 'CLS_4k_NPU'
  quantization: 2
  quantization_method: 'QAT'
  quantization_weight_bitwidth: 8
  quantization_activation_bitwidth: 8

NPU Constraints:

  • Must use quantization: 2 (TI style optimised)

  • INT8 or INT4 bit widths recommended

  • Symmetric quantization preferred

  • Per-channel quantization for weights

  • Per-tensor quantization for activations

8.2.7. Output Files

After quantization, you’ll find:

.../training/
├── base/
│   └── best_model.pt          # Float32 model
└── quantization/
    ├── best_model.onnx        # Quantized ONNX
    └── quantization_config.yaml

8.2.8. Accuracy Comparison

Typical accuracy retention by bit width:

Precision

Size Reduction

Speed Improvement

Accuracy Drop

Float32

1x (baseline)

1x (baseline)

0%

INT8

4x

2-4x

<1%

INT4

8x

3-6x

1-5%

INT2

16x

4-8x

5-15%

Note: Results vary by model and task.

8.2.9. Troubleshooting Accuracy Loss

If quantization hurts accuracy:

1. Try QAT instead of PTQ:

training:
  quantization: 2
  quantization_method: 'QAT'
  quantization_weight_bitwidth: 8
  quantization_activation_bitwidth: 8

2. Use higher bit widths:

If using 4-bit or 2-bit, try 8-bit first:

training:
  quantization_weight_bitwidth: 8
  quantization_activation_bitwidth: 8

3. Keep activations at higher precision:

Use higher activation bit width with lower weight bit width:

training:
  quantization_weight_bitwidth: 4
  quantization_activation_bitwidth: 8

4. Increase model size:

A larger model may tolerate quantization better.

8.2.10. Best Practices

  1. Start with INT8: Best balance of compression and accuracy

  2. Use QAT for critical applications: When accuracy is paramount

  3. Use TI optimised quantization for NPU: Set quantization: 2 for NPU targets

  4. Compare float vs quantized: Always measure accuracy drop

  5. Test on target device: Verify behavior matches simulation

8.2.11. Example: Full Quantization Workflow

common:
  task_type: 'generic_timeseries_classification'
  target_device: 'F28P55'

dataset:
  dataset_name: 'dc_arc_fault_example_dsk'

data_processing_feature_extraction:
  feature_extraction_name: 'FFT1024Input_256Feature_1Frame_Full_Bandwidth'
  variables: 1

training:
  model_name: 'CLS_4k_NPU'
  training_epochs: 30
  batch_size: 256
  quantization: 2
  quantization_method: 'QAT'
  quantization_weight_bitwidth: 8
  quantization_activation_bitwidth: 8

testing:
  enable: True

compilation:
  enable: True
  preset_name: 'compress_npu_layer_data'

Expected Results:

Float32 Model:
Accuracy: 99.2%
Size: 1.6 KB

INT8 Quantized Model:
Accuracy: 99.0%
Size: 0.4 KB
Speedup: 3.5x on NPU

8.2.12. Memory Savings

Quantization reduces memory at multiple levels:

Model Weights:

Float32: 4 bytes per parameter
INT8:    1 byte per parameter
INT4:    0.5 bytes per parameter

Example: 4000 parameter model
Float32: 16 KB
INT8:    4 KB
INT4:    2 KB

Activations:

Intermediate computations also benefit from reduced precision.

Total Memory:

For memory-constrained devices, quantization may be the difference between fitting and not fitting.

8.2.13. Performance Impact

NPU Performance:

Model: CLS_4k_NPU on F28P55

Float32 (CPU): ~5000 µs
INT8 (NPU):    ~300 µs
INT4 (NPU):    ~200 µs

CPU Performance:

Even without NPU, integer operations are faster:

Model: CLS_4k on F28P65 (no NPU)

Float32: ~5000 µs
INT8:    ~2000 µs

8.2.14. Quantization Wrapper Architecture

Under the hood, Tiny ML Tensorlab uses quantization wrapper classes from the tinyml-modeloptimization package. Understanding the wrapper architecture helps when customizing quantization or debugging.

Class Hierarchy:

TinyMLQuantFxBaseModule (base class)
    ├── TINPUTinyMLQuantFxModule
    │   ├── TINPUTinyMLQATFxModule   (quantization: 2, QAT)
    │   └── TINPUTinyMLPTQFxModule   (quantization: 2, PTQ)
    │
    └── GenericTinyMLQuantFxModule
        ├── GenericTinyMLQATFxModule  (quantization: 1, QAT)
        └── GenericTinyMLPTQFxModule  (quantization: 1, PTQ)

TINPUTinyML wrappers (quantization: 2) incorporate the constraints of TI NPU Hardware accelerator. They perform extensive graph transformations including 13+ layer pattern replacements to produce NPU-compatible integer operations. Key characteristics:

  • Enforces power-of-2 scale factors (mandatory for 8-bit quantization)

  • Transforms convolution, pooling, linear, and batch normalization layers to NPU-compatible patterns

  • Implements the NPU BNORM sequence: Add (bias) → Mul (scale) → Div (2^n, right shift) → Floor → Clip

  • All operations in integer domain, no dequantization step

GenericTinyML wrappers (quantization: 1) use standard PyTorch quantization APIs with minimal modifications, relying on ONNX Runtime for optimization. Key characteristics:

  • Flexible scaling (no power-of-2 constraint)

  • Only 1 pattern replacement (permute + unsqueeze)

  • Uses PyTorch’s native quantized operations

  • Relies on ONNX Runtime optimization for deployment

Note

When using the toolchain via YAML configs, you do not need to interact with these wrapper classes directly. Setting quantization: 1 or quantization: 2 in the config selects the appropriate wrapper automatically.

8.2.15. NPU Hardware Constraints

When using TI style optimised quantization (quantization: 2), the following hardware constraints are enforced automatically by the TINPU wrapper:

Channel Alignment:

Input and output channels must be multiples of 4. The NPU processes data in SIMD fashion with 4-channel vectors.

Layer Type

Channel Requirement

Notes

FCONV (First Conv)

Input: exactly 1, Output: multiple of 4

First layer in the network

GCONV (Generic Conv)

Input and Output: multiple of 4

General convolution layers

DWCONV (Depthwise Conv)

Input/Output: multiple of 4

Depthwise separable layers

PWCONV (Pointwise Conv)

Input/Output: multiple of 4

1x1 convolution layers

FC (Fully Connected)

Input: multiple of 4

Dense/linear layers

Power-of-2 Scaling:

For 8-bit quantization, scale factors must be powers of 2. This enables efficient implementation as bit shifts in hardware, avoiding expensive division operations. For sub-8-bit quantization (4-bit, 2-bit), non-power-of-2 scales are supported and may provide better accuracy.

Bitwidth Constraints:

Parameter

Allowed Values

Notes

Weight bitwidth

2, 4, or 8 bits (signed)

Determines model compression ratio

Activation bitwidth

8 bits (signed or unsigned)

Fixed at 8 bits for NPU acceleration

Bias

16-bit (2b/4b weights), 24-bit (8b weights)

Automatically computed

Scale

8-bit unsigned (2b/4b), power-of-2 shift (8b)

Automatically computed

Supported NPU Layer Patterns:

The NPU accelerates the following layer types: FCONV, GCONV, DWCONV, PWCONV, FC, AVGPOOL, MAXPOOL. Each layer includes a BNORM sequence (bias → scale → shift → floor → clip) that maps directly to NPU hardware units.

Warning

Models with layers that do not meet NPU constraints will fall back to CPU execution for those layers. Use quantization: 1 (Generic) for models that cannot satisfy these constraints.

8.2.16. Using Quantization Wrappers Directly

For advanced users who want to use the quantization wrappers outside the Tiny ML Tensorlab toolchain (e.g., in custom PyTorch training scripts), the wrappers can be imported and used directly.

TINPU QAT Example:

from tinyml_torchmodelopt.quantization import TINPUTinyMLQATFxModule

# Create and pretrain your model
model = MyNeuralNetwork()
model.load_state_dict(torch.load('pretrained.pth'))

# Wrap with TINPU quantization
model = TINPUTinyMLQATFxModule(model, total_epochs=epochs)

# Train the wrapped model (your usual training loop)
model.train()
for e in range(epochs):
    for images, target in train_loader:
        output = model(images)
        # loss, backward(), optimizer step as usual

model.eval()

# Convert to integer operations
model = model.convert()

# Export to ONNX
dummy_input = torch.rand((1, 1, 256, 1))
model.export(dummy_input, 'model_int8.onnx', input_names=['input'])

Generic QAT Example:

from tinyml_torchmodelopt.quantization import GenericTinyMLQATFxModule

# Create and pretrain your model
model = MyNeuralNetwork()
model.load_state_dict(torch.load('pretrained.pth'))

# Wrap with Generic quantization
model = GenericTinyMLQATFxModule(model, total_epochs=epochs)

# Train, convert, and export (same API as TINPU)
# ...
model = model.convert()
model.export(dummy_input, 'model_int8.onnx', input_names=['input'])

PTQ (Post-Training Quantization):

For PTQ, replace the QAT module with the PTQ variant. PTQ only requires a calibration pass (forward pass on representative data) instead of full retraining:

from tinyml_torchmodelopt.quantization import TINPUTinyMLPTQFxModule

model = TINPUTinyMLPTQFxModule(model, total_epochs=1)

# Calibration pass (no backward, no optimizer)
model.eval()
with torch.no_grad():
    for images, _ in calibration_loader:
        model(images)

model = model.convert()
model.export(dummy_input, 'model_int8.onnx', input_names=['input'])

Evaluating Exported ONNX Models:

After exporting, you can evaluate the quantized ONNX model using ONNX Runtime:

import onnxruntime as ort

ort_session_options = ort.SessionOptions()
ort_session_options.graph_optimization_level = (
    ort.GraphOptimizationLevel.ORT_ENABLE_EXTENDED
)

ort_session = ort.InferenceSession('model_int8.onnx', ort_session_options)
prediction = ort_session.run(None, {'input': example_input.numpy()})

8.2.17. Wrapper API Reference

All quantization wrappers inherit from TinyMLQuantFxBaseModule, which accepts the following parameters:

Parameter

Type

Description

model

nn.Module

The PyTorch model to quantize

qconfig_type

dict/None

QConfig mapping for quantization. None uses wrapper defaults.

example_inputs

Tensor

Example input with batch size 1

is_qat

bool

Toggle between QAT (True) and PTQ (False)

backend

str

Backend: 'qnnpack' (Linux) or 'fbgemm' (Windows). Automatically selected.

total_epochs

int

Total number of quantized training epochs

num_batch_norm_update_epochs

bool/int

BatchNorm freezing control (see below)

num_observer_update_epochs

bool/int

Observer freezing control (see below)

bias_calibration_factor

float

Bias calibration factor (0.0 = disabled)

verbose

bool

Enable verbose logging

float_ops

bool

Use float bias for Conv/Linear layers. Increases accuracy but disables BNORM on TINPU hardware.

BatchNorm Freezing (``num_batch_norm_update_epochs``):

  • None (default): Freezes BatchNorm statistics at the midpoint of training

  • False: Never freezes BatchNorm (may cause overfitting)

  • Integer value: Freezes after the specified epoch. Best results with half to 3/4 of total epochs.

Observer Freezing (``num_observer_update_epochs``):

  • False (default): Observers remain active throughout training

  • Integer value: Freezes observers after the specified epoch

8.2.18. Next Steps