8.4. Automatic Mixed Precision Quantization

Automatic Mixed Precision (AMP) is a Hessian-aware, fully automatic pipeline that assigns per-layer quantization bit widths using a greedy algorithm. It is enabled by setting auto_quantization: True in the training config and is the recommended approach when deploying quantized models, especially for regression tasks where uniform quantization can fail.

8.4.1. Overview

Standard uniform quantization applies the same bit width to every layer in the model. This is suboptimal because layers differ in their sensitivity to quantization error — some layers tolerate aggressive compression while others require higher precision to preserve accuracy.

Automatic Mixed Precision solves this by:

  • Estimating the sensitivity of each layer using the Hessian of the loss

  • Assigning bit widths layer-by-layer via a greedy algorithm that maximises accuracy improvement per bit spent

  • Automatically selecting the average bit width through binary search calibration — no manual tuning required

Layers assigned bit width 8, 4, or 2 execute on the NPU. Layers assigned 32 (float) run on the CPU. This CPU+NPU split applies across all task types.

The pipeline runs end-to-end without user intervention and is generalised across classification, regression, anomaly detection, and forecasting tasks.

Note

auto_quantization defaults to True for all task types (classification, regression, anomaly detection, forecasting). It has no effect when quantization: 0 (float training). It works with both quantization: 1 and quantization: 2

8.4.2. Algorithm

The pipeline consists of three sequential stages:

Stage 1 — Layer-wise Sensitivity Estimation

The sensitivity of a layer is defined as the largest eigenvalue (λmax) of the Hessian of the training loss with respect to that layer’s weights. A high eigenvalue indicates that small changes in the weights cause large changes in the loss — i.e. the layer is sensitive to quantization.

λmax is computed efficiently using power iteration:

  1. Start with a random normalised vector v

  2. Compute the first-order gradient g of the loss via backpropagation

  3. Form the scalar product gv

  4. Differentiate gv with respect to the weights to approximate the Hessian-vector product Hv

  5. Normalise Hv to obtain the new v

  6. Repeat until the Rayleigh quotient converges to λmax

This requires only a single batch of data and one forward-backward pass per iteration, making it computationally practical.

Stage 2 — Greedy Bit Width Assignment

Given a target average bit width budget for the model, the algorithm assigns bit widths from the set {2, 4, 8, 32} by maximising the following metric for each candidate upgrade:

Efficiency = Error Reduction / Bit Cost

where Error Reduction is the decrease in quantization error when a layer is upgraded from its current bit width to the next higher one, and Bit Cost is the increase in average model bit width from that upgrade.

Starting from the lowest bit width, the layer with the highest efficiency is upgraded at each step. This repeats until the total average bit width budget is exhausted.

Stage 3 — Automatic Average Bit Width via Calibration

Rather than requiring the user to specify the average bit width budget, the pipeline determines it automatically using binary search:

Task Type

Search Range

Metric

Default Tolerance

Config Key

Classification

[4, 8]

Accuracy

5% drop (0.05)

autoquant_tolerance_classification

Regression

[4, 12]

R²

5% drop (0.05)

autoquant_tolerance_regression

Forecasting

[4, 32]

SMAPE

3× float baseline (2.0)

autoquant_tolerance_forecasting

Anomaly Detection

[4, 8]

MSE

3× float baseline (2.0)

autoquant_tolerance_anomaly

At each candidate average bit width, a fast calibration pass (no full QAT retraining) is run and the metric is checked against the tolerance threshold. The lowest average bit width that still passes is selected. The binary search typically converges in two to three iterations.

If the Hessian estimation fails for any reason, the pipeline falls back to standard uniform 8-bit QAT automatically.

8.4.3. Tolerance Thresholds

The tolerance thresholds control how much metric degradation versus the float baseline is acceptable during the binary-search calibration. They are set in params.py and can be overridden per run in config.yaml under the training section.

For accuracy and R², higher values are better, so the tolerance is a fraction representing the maximum allowed drop from the float baseline. The quantized metric must stay above float_metric × (1 − tolerance).

For SMAPE and MSE, lower values are better, so the tolerance is a value added to 1.0 to form a ceiling multiplier. The quantized metric must stay below float_metric × (1 + tolerance).

Classification — autoquant_tolerance_classification (default: 0.05)

Accuracy is higher-is-better. 0.05 means the quantized model’s accuracy may drop by at most 5% relative to the float model. For example, if the float model achieves 90% accuracy, the threshold is 90% × (1 − 0.05) = 85.5%. Any candidate bit width that pushes accuracy below that threshold is rejected and the algorithm tries a higher bit width.

Regression — autoquant_tolerance_regression (default: 0.05)

R² is higher-is-better. 0.05 means the quantized model’s R² may drop by at most 5% relative to the float baseline. For example, a float R² of 0.95 sets a threshold of 0.95 × (1 − 0.05) = 0.9025. Regression metrics are highly sensitive to quantization, so keeping this tight ensures the selected bit width genuinely preserves model quality.

Forecasting — autoquant_tolerance_forecasting (default: 2.0)

SMAPE is lower-is-better. The tolerance is used as an additive factor to form a ceiling: threshold = float_SMAPE × (1 + 2.0) = 3 × float_SMAPE. So 2.0 means the quantized model’s SMAPE may be at most 3× the float baseline before the bit width is rejected. SMAPE is an unbounded ratio metric, so a multiplicative ceiling is more meaningful than a fixed fraction. The float SMAPE is recorded at the end of float training and used as the reference.

Anomaly Detection — autoquant_tolerance_anomaly (default: 2.0)

MSE is lower-is-better. The same formula applies: threshold = float_MSE × (1 + 2.0) = 3 × float_MSE. So 2.0 means the quantized model’s reconstruction MSE may be at most 3× the float baseline before the bit width is rejected. The absolute MSE value is dataset-dependent, which is why a multiplier is used rather than a fixed threshold.

8.4.4. Configuration

Since auto_quantization defaults to True, no explicit config change is needed — it is already active whenever quantization: 1 or quantization: 2 is set:

training:
  model_name: 'REGR_13k'
  training_epochs: 100
  quantization: 2

Note

Explicitly setting auto_quantization: True is not required. The above config is sufficient to enable automatic mixed precision.

To disable it and fall back to uniform quantization, explicitly set it to False:

training:
  training_epochs: 100
  quantization: 2
  auto_quantization: False

Note

When auto_quantization: True, the quantization_weight_bitwidth parameter is ignored. Bit widths are assigned per-layer by the greedy algorithm, not set uniformly.

Overriding tolerance thresholds

The tolerance thresholds have defaults set in params.py but can be overridden in config.yaml under the training key. Only the keys relevant to your task type need to be specified:

training:
  model_name: 'REGR_13k'
  training_epochs: 100
  quantization: 2
  auto_quantization: True
  # Tighten regression tolerance: allow at most 2% R² drop instead of 5%
  autoquant_tolerance_regression: 0.02
training:
  model_name: 'AD_17K'
  training_epochs: 100
  quantization: 2
  auto_quantization: True
  # Relax anomaly tolerance: allow up to 4x MSE increase
  autoquant_tolerance_anomaly: 3.0

All four keys and their defaults are:

training:
  autoquant_tolerance_classification: 0.05   # higher-is-better: max 5% accuracy drop vs float
  autoquant_tolerance_regression: 0.05        # higher-is-better: max 5% R² drop vs float
  autoquant_tolerance_forecasting: 2.0        # lower-is-better: SMAPE must stay below 3× float (1 + 2.0)
  autoquant_tolerance_anomaly: 2.0            # lower-is-better: MSE must stay below 3× float (1 + 2.0)

8.4.5. Task-Specific Behaviour

Classification and Anomaly Detection

The calibration search runs over [4, 8]. For most classification datasets the algorithm selects an average bit width in the range 4–6, giving better compression than uniform 8-bit with comparable accuracy.

Forecasting

The calibration search runs over [4, 32] using SMAPE as the metric. The wider range accounts for the sensitivity of sequence prediction models. The float SMAPE is recorded during the float training run and used as the reference for the binary search tolerance check.

Regression

Regression models are particularly sensitive to uniform quantization. Uniform 8-bit QAT can catastrophically degrade regression metrics (e.g. R² collapsing from 0.98 to −71 for some datasets). Automatic mixed precision addresses this by assigning higher bit widths to the sensitive layers (typically the first convolutional and last linear layers) while compressing less sensitive intermediate layers.

The calibration search range is extended to [4, 12] to allow higher average bit widths when the task demands it.

8.4.6. Example Configs

Regression (Washing Machine Load Weighing):

common:
  task_type: generic_timeseries_regression
  target_device: F28P55

dataset:
  dataset_name: washing_machine_load_weighing

data_processing_feature_extraction:
  stride_size: 0.1
  data_proc_transforms:
    - SimpleWindow
  frame_size: 512
  variables: 6

training:
  model_name: REGR_13k
  batch_size: 128
  training_epochs: 100
  quantization: 2
  auto_quantization: True

testing: {}
compilation: {}

Generic Timeseries Regression:

common:
  task_type: generic_timeseries_regression
  target_device: F28P55

training:
  model_name: REGR_13k
  quantization: 2
  auto_quantization: True

testing: {}
compilation: {}

8.4.7. Next Steps