5.21. RTDMA Module
5.21.1. Introduction
The F29H85-SDK RTDMA can be integrated with F29H85-MCAL for any RTDMA transfers according to the system requirements. This integration allows to initialize and use RTDMA channels based on the specific application.
CDD DMA driver will be provided in a future release. If customers have a need to use DMA in the meantime, they can use SDK RTDMA as described in this guide. However, please be aware that F29H85-SDK RTDMA is non-AUTOSAR and a Basic Quality driver. This integration is intended as a temporary solution to enable DMA use cases in the absence of CDD DMA. It is recommended to use AUTOSAR drivers on AUTOSAR core whenever possible.
The following example demonstrates a memory to memory data transfer in MCAL using the F29H85X-SDK RTDMA.
5.21.1.1. RTDMA Memory Transfer Example
5.21.1.1.1. Overview
Rtdma_Example_Mem_Transfer example demonstrates how to use the F29H85X-SDK RTDMA (Real-Time Direct Memory Access) module with the F29H85X-MCAL. The example performs a memory-to-memory transfer operation using one RTDMA channel.
The example demonstrates:
How to configure and initialize the RTDMA module.
How to set up a memory-to-memory transfer
How to trigger DMA transfers in software
How to use DMA interrupts to signal transfer completion
5.21.1.1.2. Software Version Used
F29H85X-SDK : 1.02.00.00
5.21.1.1.3. RTDMA Configuration
The example configures RTDMA1 Channel 1 with the following parameters:
Parameter |
Value |
Description |
|---|---|---|
Burst Size |
4 |
Number of words per burst |
Transfer Size |
16 |
Number of bursts in the transfer |
Source/Destination Width |
32-bit |
Data width for read/write operations |
Trigger Mode |
Software |
DMA transfers are triggered by software |
Interrupt Mode |
At End |
Interrupt generated at the end of the transfer |
5.21.1.1.4. Example logs
RTDMA Sample Application - Starts!!!
---------------------------------------------------------------
Data at source before transfer:
0 1 2 3 4 5 6 7 8 9 10 11 12 13 14 15
Data at destination before transfer:
0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
Data at source after transfer:
0 1 2 3 4 5 6 7 8 9 10 11 12 13 14 15
Data at destination after transfer:
0 1 2 3 4 5 6 7 8 9 10 11 12 13 14 15
===============================================
Transfer successful
5.21.2. References
F29H85X-SDK RTDMA documentation
RTDMA example ‘rtdma_ex1_mem_transfer’ in F29H85X-SDK