5.20. RTDMA Module

5.20.1. Introduction

The F29H85-SDK RTDMA can be integrated with F29H85-MCAL for any RTDMA transfers according to the system requirements. This integration allows to initialize and use RTDMA channels based on the specific application.

CDD DMA driver will be provided in a future release. If customers have a need to use DMA in the meantime, they can use SDK RTDMA as described in this guide. However, please be aware that F29H85-SDK RTDMA is non-AUTOSAR and a Basic Quality driver. This integration is intended as a temporary solution to enable DMA use cases in the absence of CDD DMA. It is recommended to use AUTOSAR drivers on AUTOSAR core whenever possible.

The following example demonstrates a memory to memory data transfer in MCAL using the F29H85X-SDK RTDMA.

5.20.1.1. RTDMA Memory Transfer Example

5.20.1.1.1. Overview

Rtdma_Example_Mem_Transfer example demonstrates how to use the F29H85X-SDK RTDMA (Real-Time Direct Memory Access) module with the F29H85X-MCAL. The example performs a memory-to-memory transfer operation using one RTDMA channel.

The example demonstrates:

  • How to configure and initialize the RTDMA module.

  • How to set up a memory-to-memory transfer

  • How to trigger DMA transfers in software

  • How to use DMA interrupts to signal transfer completion

5.20.1.1.2. Software Version Used

  • F29H85X-SDK : 1.02.00.00

5.20.1.1.3. RTDMA Configuration

The example configures RTDMA1 Channel 1 with the following parameters:

Parameter

Value

Description

Burst Size

4

Number of words per burst

Transfer Size

16

Number of bursts in the transfer

Source/Destination Width

32-bit

Data width for read/write operations

Trigger Mode

Software

DMA transfers are triggered by software

Interrupt Mode

At End

Interrupt generated at the end of the transfer

5.20.1.1.4. Example logs

RTDMA Sample Application - Starts!!!
---------------------------------------------------------------
Data at source before transfer:
0 1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 
Data at destination before transfer:
0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 
Data at source after transfer:
0 1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 
Data at destination after transfer:
0 1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 
===============================================

Transfer successful

5.20.2. References