5.3. DIO Module

5.3.1. Acronyms and Definitions

Abbreviation/Term

Explanation

AUTOSAR

Automotive Open System Architecture

RTE

Runtime Environment

BSW

Basic Software

GPIO

General Purpose Input Output

MCAL

Micro controller Abstraction Layer

API

Application Programming Interface

DET

Default Error Tracer

HW

Hardware

SW

Software

DIO

Digital Input Output

I/O

Input/Output

ID

Identifier

5.3.2. Introduction

The DIO module provides interfaces to external peripherals by abstracting the input and output pins on the micro controller device, Following sections highlight key aspects of this implementation which would be of interest to an integrator.

DIO MCAL AUTOSAR

Fig. 5.5 DIO MCAL AUTOSAR

This document details AUTOSAR BSW DIO module implementation

Supported AUTOSAR Release

4.3.1

Supported Configuration Variants

Pre-Compile & Link Time

Vendor ID

DIO_VENDOR_ID (44)

Module ID

DIO_MODULE_ID (120)

5.3.3. Functional Overview

The DIO Driver abstracts the access to the micro controller’s hardware pins. Furthermore, it allows the grouping of those pins. This module works on pins and ports which are configured by the PORT driver for this purpose. For this reason, there is no configuration and initialization of this port structure in the DIO Driver.

The DIO Modules expects that pin mux is set correctly to configure the GPIO pins for GPIO mode. This is done by the PORT driver. The pin direction shall also be set by the PORT driver.

The DIO Driver provides services for reading and writing to/from

  • DIO Channels - Represents a single general-purpose digital input/output pin.

  • DIO Ports - Represents several DIO channels that are grouped by hardware (typically controlled by one hardware register).

  • DIO Channel Groups - A channel group is a formal logical combination of several adjoining DIO channels within a DIO port. A DIO channel group shall belong to one DIO port. Below picture describes this.

The basic behavior of this driver is synchronous.

Schematic description of a ChannelGroup

Fig. 5.6 Schematic description of a ChannelGroup

5.3.4. Hardware Features

5.3.4.1. Hardware Features supported

Features Supported at a high level are:

  • Un-Buffered Read & Write of GPIO Pin Levels

  • Un-Buffered Read & Write of internal general purpose I/O ports

  • Un-Buffered Read & Write of subset of internal general purpose I/O ports

  • Flipping GPIO Pin Levels

For the device there are up to 8 Possible I/O Ports.

Port

ChannelId

Port ID

Port A

0 - 31

0

Port B

32 - 63

1

Port C

64 - 95

2

Port D

96 - 127

3

Port E

128 - 159

4

Port F

160 - 191

5

Port G

192 - 223

6

Port H

224 - 255

7

Note

The number of pins shown above may vary depending on the specific device being used. For accurate and up-to-date information, please consult the device’s datasheet.

5.3.4.2. Not supported Features

None

5.3.4.3. Non compliance

DIO Channel validity will be checked against maximum allowed DIO channels which is 256

Below AUTOSAR design requirement is not supported for Dio Driver :
SWS_Dio_00084 : If the micro-controller does not support the direct read-back of a pin value, the Dio module’s read functions shall provide the value of the output register, when they are used on a channel which is configured as an output channel

Rejection Reason : Direct read back of a pin value is achieved using GPyDAT register, Hence this requirement is rejected.

5.3.5. Source files

📦f29h85x_mcal
┣ 📂build
┣ 📂docs
┣ 📂drivers
┃ ┣ 📂BSW_Stubs
┃ ┣ 📂Can
┃ ┣ 📂Dio
┃ ┃ ┣ 📂include
┃ ┃ ┃ ┣ 📜Dio.h : Contains the API declarations of the DIO driver to be used by upper layers.
┃ ┃ ┃ ┗ 📜Dio_Priv.h : contains the private functions declarations
┃ ┃ ┣ 📂src
┃ ┃ ┃ ┣ 📜Dio.c : contains the implementation of the API’s for DIO driver.
┃ ┃ ┃ ┗ 📜Dio_Priv.c : contains the implementation for DIO private functions which will directly interact with hardware registers.
┃ ┃ ┗ 📜CMakeLists.txt
┃ ┣ 📂Gpt
┃ ┣ 📂hw_include
┃ ┣ 📂Mcal_Lib
┃ ┣ 📂Mcu
┃ ┗ 📂Port
┣ 📂examples
┣ 📂plugins
┣ 📜CMakeLists.txt
┗ 📜CMakePresets.json

Dio Header File Structure

Fig. 5.7 Dio Header File Structure

5.3.6. Module requirements

5.3.6.1. Memory Mapping

The driver follows the AUTOSAR memory mapping strategy. All memory sections should be stored in memory as per AUTOSAR specifications, considering initialization policy, alignment requirements, safety classification, and core scope where applicable.

Reference memory map files can be found at:

{MCAL_INSTALL_PATH}\drivers\BSW_Stubs\MemMap\include

The memory sections are organized according to AUTOSAR specifications to ensure proper placement of code and data in different memory regions based on their usage and access patterns.

5.3.6.2. Scheduling

There is no scheduling functions in Dio

5.3.6.3. Error handling

5.3.6.3.1. Development Error Reporting

Development errors are reported to the DET using the service Det_ReportError(), when enabled. The driver interface contains the MACRO declaration of the error codes to be returned.

5.3.6.4. Error codes

Type of Error

Related Error code

Value (Hex)

API parameter checking: Invalid channel requested

DIO_E_PARAM_INVALID_CHANNEL_ID

0x0A

API parameter checking: Invalid port requested

DIO_E_PARAM_INVALID_PORT_ID

0x14

API parameter checking: Invalid channel group requested

DIO_E_PARAM_INVALID_GROUP

0x1F

API service called with a NULL pointer

DIO_E_PARAM_POINTER

0x20

5.3.7. Used resources

5.3.7.1. Interrupt Handling

There are no Interrupts in Dio

5.3.7.2. Instance support

CPU instances

supported

CPU 1

YES

CPU 2

NO

CPU 3

NO

5.3.7.3. Hardware-Software Mapping

Below image shows Dio driver Hardware-Software mapping. For more information related to HW/SW mapping, refer the F29x Reference Manual.

Dio HW/SW Mapping

Fig. 5.8 Dio HW/SW Mapping

5.3.8. Integration description

5.3.8.1. Dependent modules

5.3.8.1.1. DET

This implementation depends on the DET in order to report development errors The detection of development errors is configurable (ON / OFF), The switch DIO_DEV_ERROR_DETECT will activate or deactivate the detection of all development errors.

5.3.8.1.2. PORT

PORT Module is required to initialize Pin configurations like MUX mode, Pin direction and more

5.3.8.1.3. MCU

MCU Module is required to initialize all the clock to be used by different peripherals

5.3.8.2. Multi-core and Resource allocator

The DIO module is not managed by the Resource Allocator. GPIO pin core allocation on F29H85x is controlled through the Port module’s PortPinCoreSelect parameter. The DIO module only operates on GPIO pins that are allocated to CPU1 (the MCAL/AUTOSAR core). No Resource Allocator instance allocation is needed for the DIO module.

5.3.9. Configuration

The Dio Driver implementation supports multiple configuration variants, namely Dio Pre-Compile config and Link-Time config. the driver expects generated Dio_Cfg.h to be present as input file. The associated dio driver configuration generated files are Dio_Cfg.c or Dio_Lcfg.c

The generated configuration files should not be modified manually. The config tool Elektrobit Tresos should be used to modify the configuration files.

5.3.9.1. Configuration Parameters

5.3.9.1.1. DioConfig

This container contains the configuration parameters and sub containers of the AUTOSAR DIO module.

5.3.9.1.1.1. DioPort

Configuration of individual DIO ports, consisting of channels and possible channel groups.

5.3.9.1.1.2. DioPortId

Item

Name

DioPortId

Description

Numeric identifier of the DIO port. Not all MCU ports may be used for DIO, thus there may be “gaps” in the list of all IDs. This value will be

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Link-Time

VARIANT-LINK-TIME

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

7

Min-value

0

5.3.9.1.1.3. DioChannel

Configuration of an individual DIO channel.

5.3.9.1.1.4. DioChannelId

Item

Name

DioChannelId

Description

Channel Id of the DIO channel. This value will be assigned to the symbolic names.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Link-Time

VARIANT-LINK-TIME

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

255

Min-value

0

5.3.9.1.1.5. DioPinNumRef

Item

Name

DioPinNumRef

Description

Reference to the Port Pin configuration, which is set in the PORT driver configuration

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Link-Time

VARIANT-LINK-TIME

Pre-Compile-Time

VARIANT-PRE-COMPILE

5.3.9.1.1.6. DioChannelGroup

Definition and configuration of DIO channel groups. A channel group represents several adjoining DIO channels represented by a logical group.

5.3.9.1.1.7. DioChannelGroupIdentification

Item

Name

DioChannelGroupIdentification

Description

The DIO channel group is identified in DIO API by a pointer to a data structure (of type Dio_ChannelGroupType). That data structure contains the channel group information.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Link-Time

VARIANT-LINK-TIME

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

Dio_ChannelGroup

5.3.9.1.1.8. DioPortMask

Item

Name

DioPortMask

Description

This shall be the mask which defines the positions of the channel

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Link-Time

VARIANT-LINK-TIME

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

4294967295

Max-value

4294967295

Min-value

0

5.3.9.1.1.9. DioPortOffset

Item

Name

DioPortOffset

Description

The position of the Channel Group on the port, counted

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Link-Time

VARIANT-LINK-TIME

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

31

Min-value

0

5.3.9.1.2. DioGeneral

General DIO module configuration parameters.

5.3.9.1.2.1. DioDevErrorDetect

Item

Name

DioDevErrorDetect

Description

Switches the development error detection and notification on or off.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Link-Time

VARIANT-LINK-TIME

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

5.3.9.1.2.2. DioFlipChannelApi

Item

Name

DioFlipChannelApi

Description

Adds / removes the service Dio_FlipChannel() from the code.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Link-Time

VARIANT-LINK-TIME

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

5.3.9.1.2.3. DioVersionInfoApi

Item

Name

DioVersionInfoApi

Description

Adds / removes the service Dio_ GetVersionInfo() from the code.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Link-Time

VARIANT-LINK-TIME

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

5.3.9.2. Steps To Configure Dio Module

  1. Open EB Tresos configurator tool and load Port and Dio modules

  2. Open PORT module plugin and configure required pins as GPIO’s

  3. Open DIO module plugin, Select the Config Variant (Pre-compile/Link-Time)

  4. In DIO module plugin, Create port container, add Channels by referring port pins configured in port plugin

  5. Add channel groups

  6. Save the configuration and generate the configuration.

5.3.10. Examples

The example application demonstrates use of Dio module, the list below identifies key steps performed the example.

5.3.10.1. Overview

  • Dio_Example_Read_Write_All

    • EcuM_Init()

      • Initializes clock to 200 MHz using Mcu_Init()

      • Initializes pins as GPIO Outputs and GPIO Inputs using Port_Init()

    • Perform channel read/write on initialized channels

    • Perform channel group read/write on initialized channel group

    • Perform port read/write on initialized ports

    • Perform flip channel on initialized channel

5.3.10.2. Setup required to run example

5.3.10.3. How to run examples

  • Open CCS and Import Dio example

  • Connect the hardware and power up

  • Build project then debug project

  • Connect the UART set up to check the log on serial console

5.3.10.3.1. Sample Log of Dio_Example_Read_Write_All

Sample Application - STARTS !!!
DIO MCAL Version Info
---------------------
Vendor ID           : 44
Module ID           : 120
SW Major Version    : 1
SW Minor Version    : 0
SW Patch Version    : 3

Test A. Write and Read Channel
-------------------------------
Reading channel 4
Writing High to channel 4
Reading channel 4
Writing Low to channel 4
Reading channel 4
DIO Test A :Service API: Write/Read Channel completed

Test B. Write/Read Port
----------------------------
Writing on to Port 0
Reading from Port 0
Test B. Write/Read Port completed

Test C. Write/Read Channel group
----------------------------
Writing on to channel group 0
Reding from channel group 0
DIO Test C :Service API: Write/Read Channel group completed

Test D. Flip Channel
---------------------
Reading from channel 8
Fliping channel 8 level
PASS: channel 8 level fliped
DIO Test D :Service API: Flip Channel completed

Dio_Example_Read_Write_All: Sample Application - Completes successfully !!!

5.3.10.4. File Structure

📦f29h85x_mcal
┣ 📂build
┣ 📂docs
┣ 📂drivers
┣ 📂examples
┃ ┣ 📂AppUtils
┃ ┣ 📂Can
┃ ┣ 📂DeviceSupport
┃ ┣ 📂Dio
┃ ┃ ┗ 📂Dio_Example_Read_Write_All
┃ ┃ ┃ ┣ 📂CCS
┃ ┃ ┃ ┃ ┗ 📜Dio_Example_Read_Write_All.projectspec
┃ ┃ ┃ ┣ 📂Dio_Example_Read_Write_Config
┃ ┃ ┃ ┃ ┣ 📂config
┃ ┃ ┃ ┃ ┃ ┣ 📜Dem.xdm
┃ ┃ ┃ ┃ ┃ ┣ 📜Dio.xdm: Generated EB Tresos config file in .xdm format
┃ ┃ ┃ ┃ ┃ ┣ 📜EcuM.xdm
┃ ┃ ┃ ┃ ┃ ┣ 📜Mcu.xdm
┃ ┃ ┃ ┃ ┃ ┣ 📜Os.xdm
┃ ┃ ┃ ┃ ┃ ┗ 📜Port.xdm
┃ ┃ ┃ ┃ ┣ 📂include
┃ ┃ ┃ ┃ ┃ ┣ 📜Dem_Cfg.h
┃ ┃ ┃ ┃ ┃ ┣ 📜Dio_Cfg.h : Contains the generated pre-compiler configuration.
┃ ┃ ┃ ┃ ┃ ┣ 📜EcuM_Cfg.h
┃ ┃ ┃ ┃ ┃ ┣ 📜Mcu_Cfg.h
┃ ┃ ┃ ┃ ┃ ┣ 📜Os_Cfg.h
┃ ┃ ┃ ┃ ┃ ┗ 📜Port_Cfg.h
┃ ┃ ┃ ┃ ┣ 📂src
┃ ┃ ┃ ┃ ┃ ┣ 📜Dem_Cfg.c
┃ ┃ ┃ ┃ ┃ ┣ 📜Dio_Lcfg.c : Contains the pre-build configuration parameters.
┃ ┃ ┃ ┃ ┃ ┣ 📜EcuM_Cfg.c
┃ ┃ ┃ ┃ ┃ ┣ 📜Mcu_PBcfg.c
┃ ┃ ┃ ┃ ┃ ┣ 📜Os_Cfg.c
┃ ┃ ┃ ┃ ┃ ┗ 📜Port_PBcfg.c
┃ ┃ ┃ ┃ ┗ 📜CMakeLists.txt
┃ ┃ ┃ ┣ 📜CMakeLists.txt
┃ ┃ ┃ ┗ 📜Dio_Example_Read_Write_All.c
┃ ┣ 📂Gpt
┃ ┣ 📂Mcu
┃ ┣ 📂Port
┣ 📂plugins
┣ 📜CMakeLists.txt
┗ 📜CMakePresets.json

Note

Either Dio_Lcfg.c OR Dio_Cfg.c will be present based on selected config variant by user