4.7. PORT Module

4.7.1. Acronyms and Definitions

Abbreviation/Term

Explanation

AUTOSAR

Automotive Open System Architecture

RTE

Runtime Environment

BSW

Basic Software

GPIO

General Purpose Input Output

MCAL

Micro Controller Abstraction Layer

API

Application Programming Interface

DET

Default Error Tracer

HW

Hardware

SW

Software

I/O

Input/Output

4.7.2. Introduction

The Port driver module is an I/O driver in AUTOSAR Basic Software (BSW) layer. PORT driver provide the services for initializing the whole PORT structure of the microcontroller. It is used to assign various functionalities to Port and port pins (e.g. GPIOs, ADC, SPI and other peripheral modes)

PORT MCAL AUTOSAR

Fig. 4.24 PORT MCAL AUTOSAR

This document details AUTOSAR BSW PORT module implementation

Supported AUTOSAR Release

4.3.1

Supported Configuration Variants

Pre-Compile & Post Build

Vendor ID

PORT_VENDOR_ID (44)

Module ID

PORT_MODULE_ID (124)

4.7.3. Functional Overview

The Port module shall provide the service for initializing the whole PORT structure of the microcontroller. Many ports and port pins can be assigned to various functionalities, For e.g.

  • General purpose I/O

  • CAN

  • SPI

  • ADC

  • LIN etc

Up to twelve independent peripheral signals are multiplexed on a single GPIO-enabled pin in addition to the CPU-controlled I/O capability. Each pin output can be controlled by either a peripheral or one of the CPU controllers. PORT driver module shall complete the overall configuration and initialization of the port structure which is used in other dependent driver modules. Therefore, other dependent modules driver works on pins and ports which are configured by the PORT driver. Hence PORT driver shall be initialized prior to use of other driver modules functions. Otherwise those functions might exhibit undefined behavior.

4.7.4. Hardware Features

4.7.4.1. Hardware Features supported

Features Supported at a high level are:

  • Configure each port and port pin (Input/Output, Pin driver characteristics).

  • Set pins to an initial default value.

  • Refresh the direction of the initial configuration.

  • Switch the port pin configuration during runtime.

  • Pin direction changeable during runtime.

  • Port mode changeable during runtime.

4.7.4.1.1. Port Structure

For the device there are up to 8 Possible I/O Ports. Up to twelve independent peripheral signals are multiplexed on a single GPIO-enabled pin in addition to the CPU-controlled I/O capability.

Each pin output can be controlled by either a peripheral or one of the CPU controllers.

Port

GPIO Number

Port ID

Port A

0 - 31

0

Port B

32 - 63

1

Port C

64 - 95

2

Port D

96 - 127

3

Port E

128 - 159

4

Port F

160 - 191

5

Port G

192 - 223

6

Port H

224 - 255

7

4.7.4.1.2. AIOs

Some GPIOs are multiplexed with analog pins and only have digital input functionality. These are also referred to as AIOs. Pins with only an AIO option on this port can only function in input mode. See the device data sheet for list of AIO signals. By default, these pins function as analog pins and the GPIOs are in a high-impedance state.

4.7.4.1.3. AGPIOs

Some GPIOs are multiplexed with analog pins and have digital input and output functionality. These are also referred to as AGPIOs. Unlike AIOs, AGPIOs have full input and output capability. By default, the AGPIOs are not connected and must be configured.

4.7.4.1.4. Input Qualification

The input qualification scheme has been designed to be very flexible. Input qualification can be configured by user using the configurator tool. In the case of a GPIO input pin, the qualification can be specified as only synchronized to SYSCLKOUT or qualification by a sampling window. For pins that are configured as peripheral inputs, the input can also be asynchronous in addition to synchronized to SYSCLKOUT or qualified by a sampling window. The remainder of this section describes the options available.

  • No Synchronization (Asynchronous Input) : This mode is used for peripherals where input synchronization is not required or the peripheral itself performs the synchronization. Examples include communication ports McBSP, SCI, SPI, and I2C. In addition, the ePWM trip zone (TZn) signals can function independent of the presence of SYSCLKOUT

  • Synchronization to SYSCLKOUT Only : This is the default qualification mode of all the pins at reset. In this mode, the input signal is only synchronized to the system clock (SYSCLKOUT). Because the incoming signal is asynchronous, a SYSCLKOUT period of delay is needed for the input to the device to be changed. No further qualification is performed on the signal.

  • Qualification Using a Sampling Window : In this mode, the signal is first synchronized to the system clock (SYSCLKOUT) and then qualified by a specified number of cycles before the input is allowed to change. Two parameters are specified by the user for this type of qualification: (1) the sampling period, or how often the signal is sampled, and (2) the number of samples to be taken.

Note

Using input synchronization when the peripheral itself performs the synchronization can cause unexpected results. The user must make sure that the GPIO pin is configured for asynchronous in this case.

4.7.4.1.5. GPIO and Peripheral Muxing

Up to twelve different peripheral functions are multiplexed to each pin along with a general-purpose input/output (GPIO) function. This allows user to choose the peripheral mix and pinout that works best for your particular application.

Note

Available Pin Packages: Port Driver needs to be initialized as per the available pin package. Refer Device Data Sheet for details about available pin packages.

4.7.4.2. Not supported Features

  • Out of total number of available pins for a particular pin package, there are few reserved/not configurable pins.

Note

Refer Device Data Sheet for details about reserved/non-configurable pins for the respective pin package.

  • Lock Configuration and Lock Commit configuration as not supported for the module

4.7.4.3. Non compliance

Below AUTOSAR design requirements are not supported/partially supported for Port Driver :
SWS_Port_00205 : Port_Lcfg.c shall include Port_MemMap.h and Port.h

Rejection Reason : Port Driver doesn’t have any Link Time configuration input file, it only supports Pre-Compile and Port-Build configurations.

ECUC_Port_00127 : Pin Id of the port pin. Range : 1 .. 65535

Partial Non Compliance Reason : In current implementation, Pin Id range starts from 0 instead of 1 as mapping of Pin Id to GPIOs starts from 0. Therefore Port Pin Id Range is 0 to Number of Pins in Pin package. i.e for 256 pin package , range will be 0-255.

SWS_BSW_00042 : Detection of Development Errors: The detection and reporting of Development errors shall be performed only if the configuration parameter for detection of Development errors is set

Partial Non Compliance Reason : Few Null pointer input parameter checks are needed irrespective of Development errors is set, to handle MISRA requirement.

For more details, Refer AUTOSAR_SWS_PortDriver : Section: 5.1.2 : Header File Structure

4.7.5. Source files

📦f29h85x_mcal
┣ 📂build
┣ 📂docs
┣ 📂drivers
┃ ┣ 📂BSW_Stubs
┃ ┣ 📂Can
┃ ┣ 📂Dio
┃ ┣ 📂Gpt
┃ ┣ 📂hw_include
┃ ┣ 📂Mcal_Lib
┃ ┣ 📂Mcu
┃ ┗ 📂Port
┃ ┃ ┣ 📂include
┃ ┃ ┃ ┣ 📜Port.h : Contains the API declarations of the Port driver to be used by upper layers.
┃ ┃ ┃ ┣ 📜Port_Pin_Map.h : Contains the MACROs to define GPIO MUX values.
┃ ┃ ┃ ┗ 📜Port_Priv.h : Contains data structures and Internal function declarations.
┃ ┃ ┣ 📂src
┃ ┃ ┃ ┣ 📜Port.c : Contains the implementation of the API for Port driver.
┃ ┃ ┃ ┗ 📜Port_Priv.c : Contains Functions that support the API for Port driver
┃ ┃ ┗ 📜CMakeLists.txt
┣ 📂examples
┣ 📂plugins
┣ 📜CMakeLists.txt
┗ 📜CMakePresets.json

Port Header File Structure

Fig. 4.25 Port Header File Structure

4.7.6. Module requirements

4.7.6.1. Memory Mapping

Will be added in later release

4.7.6.2. Scheduling

None

4.7.6.3. Error handling

4.7.6.3.1. Development Error Reporting

Development errors are reported to the DET using the service Det_ReportError(), when enabled. The driver interface contains the MACRO declaration of the error codes to be returned.

4.7.6.4. Error codes

Type of Error

Related Error code

Value (Hex)

Invalid Port Pin ID requested.

PORT_E_PARAM_PIN

0x0A

Port Pin not configured as changeable.

PORT_E_DIRECTION_UNCHANGEABLE

0x0B

API Port_Init service called with wrong parameter.

PORT_E_INIT_FAILED

0x0C

API Port_SetPinMode service called when mode is unchangeable. Invalid Mode Passed

PORT_E_PARAM_INVALID_MODE

0x0D

API Port_SetPinMode service called when mode is unchangeable.

PORT_E_MODE_UNCHANGEABLE

0x0E

API service called without module initialization.

PORT_E_UNINIT

0x0F

API called with a Null Pointer.

PORT_E_PARAM_POINTER

0x10

4.7.7. Safety Mechanism

TI Diagnostic Unique Identifier

Summary

Description

GPIO1

Lock Mechanism for Control Registers

Port Pins Pad control register configuration can be locked and locked configurations can be committed. If user calls Port_Init or Port_SetPinMode APIs after committing the locked configuration, it will result in DET error PORT_E_INIT_FAILED or PORT_PIN_MODE_UNCHANGEABLE respectively

Note

Locked Configurations can be committed by user during runtime. After committing the configurations, user won’t be able to change the configurations during runtime. To change the configuration after committing, hard reset will be required. More details of Safety Mechanisms can be found in Safety Manual.

4.7.8. Used resources

4.7.8.1. Interrupt Handling

There are no Interrupts in Port

4.7.8.2. Instance support

CPU instances

supported

CPU 1

YES

CPU 2

NO

CPU 3

NO

4.7.8.3. Hardware-Software Mapping

Below image shows Port driver Hardware-Software mapping. For more information related to HW/SW mapping, refer the F29x Reference Manual.

Port HW/SW Mapping

Fig. 4.26 Port HW/SW Mapping

4.7.9. Integration description

4.7.9.1. Dependent modules

4.7.9.1.1. DET

This implementation depends on the DET in order to report development errors The detection of development errors is configurable (ON / OFF), The switch PORT_DEV_ERROR_DETECT will activate or deactivate the detection of all development errors.

4.7.9.1.2. SchM

If multiple AUTOSAR runnables have access to the same Data Store Memory block, the exported AUTOSAR specification enforces data consistency by using an AUTOSAR exclusive area. With this specification, the runnables have mutually exclusive access to the per-instance memory global data, which prevents data corruption. Beside the OS, the BSW Scheduler provides functions that PORT module calls at begin and end of critical sections. This implementation requires 1 level of exclusive access to guard critical sections.

The data consistency mechanism that has to be applied to an ExclusiveArea might be domain, ECU or even project specific. The decision which mechanism has to be applied by RTE / Basic Software Scheduler is taken during ECU integration by setting the Exclusive Area configuration parameter RteExclusiveAreaImplMechanism. This parameter is an input for RTE generator.
For Port Module, data consistency and exclusive access to critical sections are required for the following sections as shown in the table below:

Exclusive Area Functions used

Port Function calling Exclusive Area

Need for Exclusive Area

Recommended Exclusive Area Mapping

PORT_EXCLUSIVE_AREA_0

Port_SetPinDirection
Port_RefreshPortDirection
Port_SetPinMode

To protect against multiple access for shared resources, i.e. GPIO Data and Mode Registers, which can lead to race condition

OS_RESOURCE : If the Port APIs are only called from pre-emptible task context, its recommended to use this mechanism as it takes care of resource access protection and task priority management.
None: If Port APIs are only called from non pre-emptible task context or during init, its recommended to use this mechanism as multiple access protection to shared resource is not needed.

4.7.9.1.3. MCU

MCU Module is required to initialize all the clock to be used by different peripherals

4.7.9.2. Multi-core and Resource allocator

Not Supported

4.7.10. Configuration

The Port Driver implementation supports multiple configuration variants, namely Port Post-Build config and Pre-Compile config. The driver expects generated Port_cfg.h to be present as input file. The associated Port driver configuration generated source files are Port_Cfg.c or Port_PBcfg.c

The generated configuration files should not be modified manually. The config tool Elektrobit Tresos should be used to modify the configuration files.

Note

Refer section Getting Started with EB Tresos of Chapter MCAL Configuration and EB Tresos for more information on how to load plugin and generate the configuration files.

4.7.10.1. Configuration Precautions

  • For any peripheral pin configuration, make sure to set correct pad configurations or else it will result in unexpected behavior of the module.

  • Similarly in case of Pin Mode Changeable support, make sure to set proper pad configurations for the supported pins.

Note

More details related to Configuration precautions can be found in Safety Manual.

4.7.10.2. PortConfigSet

This container contains the configuration parameters and sub containers of the AUTOSAR Port module.

4.7.10.2.1. PortContainer

Container collecting the PortPins.

4.7.10.2.1.1. PortNumberOfPortPins

Item

Name

PortNumberOfPortPins

Description

The number of specified PortPins in this PortContainer.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

1

Max-value

1

Min-value

1

4.7.10.2.2. PortPin

Configuration of the individual port pins.

4.7.10.2.2.1. PortPinPeripheral

Item

Name

PortPinPeripheral

Description

Available Peripherals for the pin package

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

GPIO

4.7.10.2.2.2. PortPinPeripheralInstance

Item

Name

PortPinPeripheralInstance

Description

Available instances for the Peripheral selected

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

GPIO0

4.7.10.2.2.3. PortPinPeripheralSignal

Item

Name

PortPinPeripheralSignal

Description

Select specific type of peripheral signal pin of interest

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

GPIO0

4.7.10.2.2.4. PortPhysicalPinId

Item

Name

PortPhysicalPinId

Description

Identifying The physical Pin Number on the selected Pin Package.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

A8

4.7.10.2.2.5. PortPinName

Item

Name

PortPinName

Description

Device Pin Name for reference.

Origin

Texas Instruments

Post-Build-Variant-Value

true

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

GPIO0

4.7.10.2.2.6. PortPinId

Item

Name

PortPinId

Description

Pin Id of the port pin. This value will be assigned to the symbolic name derived from the port pin container short name.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

9223372036854775807

Min-value

-9223372036854775808

4.7.10.2.2.7. PortAnalogMode

Item

Name

PortAnalogMode

Description

Select whether the pin operates in Analog Mode.

Origin

Texas Instruments

Post-Build-Variant-Value

true

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

PORT_ANALOG_ENABLED

Range

PORT_ANALOG_DISABLED
PORT_ANALOG_ENABLED

4.7.10.2.2.8. PortPinInitialMode

Item

Name

PortPinInitialMode

Description

Port pin mode from mode list for use with Port_Init() function.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

true

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

PORT_MUXMODE_NA

Range

PORT_MUXMODE_NA

4.7.10.2.2.9. PortPinDirection

Item

Name

PortPinDirection

Description

The initial direction of the pin (IN or OUT). If the direction is not changeable, the value configured here is fixed.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

true

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

PORT_PIN_IN

Range

PORT_PIN_NA

4.7.10.2.2.10. PortPinDirectionChangeable

Item

Name

PortPinDirectionChangeable

Description

Parameter to indicate if the direction is changeable on a port pin during runtime.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

true

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

False

4.7.10.2.2.11. PortPinPadConfig

Item

Name

PortPinPadConfig

Description

Enable Push-Pull or Open Drain functionality.

Origin

Texas Instruments

Post-Build-Variant-Value

true

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

PORT_PIN_TYPE_STD

Range

PORT_PIN_TYPE_STD
PORT_PIN_TYPE_OPEN_DRAIN
PORT_PIN_TYPE_NA

4.7.10.2.2.12. PortPinPullUpConfig

Item

Name

PortPinPullUpConfig

Description

Enable Pull Up.

Origin

Texas Instruments

Post-Build-Variant-Value

true

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.7.10.2.2.13. PortPinQualificationMode

Item

Name

PortPinQualificationMode

Description

Synchronization mode of the peripheral signals.

Origin

Texas Instruments

Post-Build-Variant-Value

true

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

PORT_QUAL_SYNC

Range

PORT_QUAL_SYNC
PORT_QUAL_3SAMPLE
PORT_QUAL_6SAMPLE
PORT_QUAL_ASYNC
PORT_QUAL_NA

4.7.10.2.2.14. PortPinQualificationPeriod

Item

Name

PortPinQualificationPeriod

Description

Qualification period of the peripheral signals. NOTE: Qualification period can be set for the pair of 8 GPIOs For Instance: Qualification sampling period for GPIO0 to GPIO7: 0x00,QUALPRDx = PLLSYSCLK 0x01,QUALPRDx = PLLSYSCLK/2 0x02,QUALPRDx = PLLSYSCLK/4 …. 0xFF,QUALPRDx = PLLSYSCLK/510 Reset type: SYSRSn

Origin

Texas Instruments

Post-Build-Variant-Value

true

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

1

Max-value

9223372036854775807

Min-value

-9223372036854775808

4.7.10.2.2.15. PortPinLevelValue

Item

Name

PortPinLevelValue

Description

Port Pin Level value from Port pin list.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

true

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

PORT_PIN_LEVEL_LOW

Range

PORT_PIN_LEVEL_HIGH
PORT_PIN_LEVEL_LOW
PORT_PIN_LEVEL_NA

4.7.10.2.2.16. PortPinCoreSelect

Item

Name

PortPinCoreSelect

Description

Selection of core to which pin is to be mapped.

Origin

Texas Instruments

Post-Build-Variant-Value

true

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

PORT_CORE_CPU1

Range

PORT_CORE_CPU1
PORT_CORE_CPU2
PORT_CORE_CPU3

4.7.10.2.2.17. PortEnableWakeUpPinLPM

Item

Name

PortEnableWakeUpPinLPM

Description

Use/Don’t use the GPIO Pin as a wakeup source for the low power modes - standby/halt.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.7.10.2.2.18. PortPinMode

Item

Name

PortPinMode

Description

Port pin mode from mode list.

Multiplicity-Configuration-Class

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

true

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

PORT_MUXMODE_NA

Range

PORT_MUXMODE_NA

4.7.10.2.2.19. PortPinModeChangeable

Item

Name

PortPinModeChangeable

Description

Parameter to indicate if the mode is changeable on a port pin during runtime. True: Port Pin mode changeable allowed. False: Port Pin mode changeable not permitted.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

true

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.7.10.3. PortGeneral

Module wide configuration parameters of the PORT driver.

4.7.10.3.1. PortDevErrorDetect

Item

Name

PortDevErrorDetect

Description

Switches the development error detection and notification on or off.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.7.10.3.2. PortSetPinDirectionApi

Item

Name

PortSetPinDirectionApi

Description

Pre-processor switch to enable / disable the use of the function Port_SetPinDirection().

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.7.10.3.3. PortSetPinModeApi

Item

Name

PortSetPinModeApi

Description

Pre-processor switch to enable / disable the use of the function Port_SetPinMode().

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.7.10.3.4. PortVersionInfoApi

Item

Name

PortVersionInfoApi

Description

Pre-processor switch to enable / disable the API to read out the modules version information.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.7.10.3.5. PortLockConfiguration

Item

Name

PortLockConfiguration

Description

Lock All pins configuration.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

Refer AUTOSAR_SWS_PortDriver section: 10 Configuration specification for more configuration parameters details

Note

The analog signals on this device are multiplexed with digital inputs and outputs. Some of these analog IO (AIO) pins do not have digital output capability. Others of these pins are analog pins capable of full digital input and output capability (AGPIO). Analog pins with AIO (digital input only) capability contain “AIO” signals in the Pin Attributes table of the device data sheet. Analog pins with full input and output capability (AGPIO pins) contain “GPIO” signals in the Pin Attributes table of the device data sheet. AGPIO pins also have pin names with both analog signals and GPIO in the name.

4.7.10.4. Steps To Configure Port Module

  1. Open EB Tresos configurator tool and Select the Config Variant ( Precompile/Post-Build) and Device Variant ( Pin Package ) parameters

  2. Go to Port Container tab and create a new container

  3. Open the created container and go to PortPin container to create a portPin configuration. ( Multiple PortPin configurations can be created )

  4. Open the created Port pin, and configure the pin parameters

  5. Select the Port pin peripheral instance ( Mode ) which needs to be configured and accordingly select the Peripheral Signal. As per selected Signal, physical pin ID needs to be selected from the list

  6. Configure the other parameters as per pin usage.

  7. Open Port pin Mode tab and add the default port pin mode ( at least one mode is required for this field ). Other supported modes for that pin can also be configured if user needs to change the mode for the pin afterwards.

  8. Configure the number of port pins in port container general tab

  9. Save the configuration and generate the configuration.

4.7.11. Examples

The example application demonstrates use of Port module, the list below identifies key steps performed in the example.

4.7.11.1. Overview

  • Port_Example_Init

    • EcuM_Init()

      • Initializes clock to 200 MHz using Mcu_Init()

      • Initializes one pin from each port as GPIO Output using Port_Init()

    • Port_SetPinDirection Changes the direction of GPIO0 pin to Input ( LED can be connected to GPIO0 to observe the behavior )

    • Port_RefreshPinDirection will refresh the direction of the pins where direction changeable is FALSE

    • Port_SetPinMode will change the Mode from GPIO to CAND_TX of the GPIO0 pin

    • Port_GetVersionInfo will get the software version info details

4.7.11.2. Setup required to run example

  • Install Code Composer Studio(CCS) latest version

  • Install latest C29 compiler

4.7.11.3. How to run examples

  • Open CCS and import Port Example

  • Build project and start debug project

4.7.11.4. Sample Log

PORT Driver Sample Application - Starts!!!
---------------------------------------------------------------------------

Test 1: Initialize Port Driver
Initializing Port Driver...
API Port_Init executed successfully

---------------------------------------------------------------------------

Test 2: Change direction for PortPin_0
Direction changed to INPUT for PortPin_0
API Port_SetPinDirection executed successfully

---------------------------------------------------------------------------

Test 3: Change Mode for PortPin_0
Mode changed to MCAND_TX for PortPin_0
API Port_SetPinMode executed successfully

---------------------------------------------------------------------------

Test 4: Refresh Pin direction for direction unchangeable pins
API Port_RefreshPortDirection executed successfully

---------------------------------------------------------------------------

Test 5: Get Version info for Port
 API Port_GetVersionInfo executed successfully
 PORT MCAL Version Info
 ---------------------
 Vendor ID           : 44
 Module ID           : 124
 SW Major Version    : 1
 SW Minor Version    : 0
 SW Patch Version    : 0
 
---------------------------------------------------------------------------

Port Example App run is Completed
Result - PASS!!

4.7.11.5. File Structure

📦f29h85x_mcal
┣ 📂build
┣ 📂docs
┣ 📂drivers
┣ 📂examples
┃ ┣ 📂AppUtils
┃ ┣ 📂Can
┃ ┣ 📂DeviceSupport
┃ ┣ 📂Dio
┃ ┣ 📂Gpt
┃ ┣ 📂Mcu
┃ ┣ 📂Port
┃ ┃ ┗ 📂 Port_Example_Init
┃ ┃ ┃ ┣ 📂ccs
┃ ┃ ┃ ┃ ┗ 📜Port_Example_Init.projectspec
┃ ┃ ┃ ┣ 📂Port_Example_Init_Config
┃ ┃ ┃ ┃ ┣ 📂config
┃ ┃ ┃ ┃ ┃ ┣ 📜Dem.xdm
┃ ┃ ┃ ┃ ┃ ┣ 📜EcuM.xdm
┃ ┃ ┃ ┃ ┃ ┣ 📜Mcu.xdm
┃ ┃ ┃ ┃ ┃ ┣ 📜Os.xdm
┃ ┃ ┃ ┃ ┃ ┗ 📜Port.xdm : Generated EB Tresos config file in .xdm format
┃ ┃ ┃ ┃ ┣ 📂include
┃ ┃ ┃ ┃ ┃ ┣ 📜Dem_Cfg.h
┃ ┃ ┃ ┃ ┃ ┣ 📜EcuM_Cfg.h
┃ ┃ ┃ ┃ ┃ ┣ 📜Mcu_Cfg.h
┃ ┃ ┃ ┃ ┃ ┣ 📜Os_Cfg.h
┃ ┃ ┃ ┃ ┃ ┗ 📜Port_Cfg.h : Contains the generated pre-compiler configuration header.*
┃ ┃ ┃ ┃ ┣ 📂src
┃ ┃ ┃ ┃ ┃ ┣ 📜Dem_Cfg.c
┃ ┃ ┃ ┃ ┃ ┣ 📜EcuM_Cfg.c
┃ ┃ ┃ ┃ ┃ ┣ 📜Mcu_PBcfg.c
┃ ┃ ┃ ┃ ┃ ┣ 📜Os_Cfg.c
┃ ┃ ┃ ┃ ┃ ┗ 📜Port_PBcfg.c : Contains the Post build configuration parameters.
┃ ┃ ┃ ┃ ┗ 📜CMakeLists.txt
┃ ┃ ┃ ┣ 📜CMakeLists.txt
┃ ┃ ┗ ┗ 📜📂Port_Example_Init.c : Example application for Port
┃ ┗ 📜CMakeLists.txt
┣ 📂plugins
┣ 📜CMakeLists.txt
┗ 📜CMakePresets.json

Note

Either Port_PBcfg.c OR Port_Cfg.c will be present based on selected config variant by user