F29H85x-SDK  1.02.00.00
 
EMIF 16bit ASRAM

Introduction

This example configures EMIF1 in 16bit ASYNC mode and uses CS2 as chip enable

Clock source configuration

Watch Variables

  • g_errCnt

External Connections

  • Custom setup with External ASRAM memory (CY7C1041CV33 -10ZSXA) daughter card
  • Modify pinmux based on the setup under test

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see CCS Build Project).
  • When using makefiles to build, note the required combination and build using make command (see Makefile based Build)
  • Establish connections as mentioned in External Connections section.
  • Launch a CCS debug session and run the executable, see Build, Load and Run
  • Wait for transmissions to complete, check the PEAK application on the PC for received message

See Also

EMIF