F29H85x-SDK
26.00.00
CCS Build Project
Table of Contents
Build Program
Note
The steps on this page need to be done once on a given host machine
Build Program
Following are the options to build and load an example program
Build and Load together in a single click
Righ click on the project and select 'Debug Project (F5)' option
Debug CCS project
It performs the following sequence
Builds the project
Executes the 'Post build sequence for FLASH configuration'
Launches the Target Configuration based on the 'F29H850TU9.ccxml' included in projectspec
Prompts user to select the core to load the program
Select core to load program
Connects to the target core selected in above step
Loads the program onto the selected core
Build and Load separately
Build
Right click on the project and select either 'Build Project(s)' or 'Rebuild Project(s)' option
Build CCS project
Upon successful build, example program is generated 'C:\Users\user_id\workspace_ccstheia\timer_ex2_cputimers_syscfg\RAM\' folder
Executes the 'Post build sequence for FLASH configuration'
generated by
1.11.0