Introduction

TI 15.4-Stack

TI 15.4-Stack is part of the SimpleLink CC13x0 SDK. TI 15.4-Stack is a software stack from Texas Instruments that implements the standard IEEE 802.15.4e and 802.15.4g specification. TI 15.4-Stack also implements a frequency-hopping scheme adopted from Wi-SUN® field area network (FAN) specification. The SimpleLink CC13x0 SDK also provides the required tools, real-time operating system (RTOS), and example applications for TI 15.4-Stack to help developers quickly get started developing their own star- topology-basedwireless network products. The purpose of this document is to give an overview of TI 15.4-Stack to help developers run the out-of-box example applications and enable creation of custom TI 15.4-Stack based wireless star-topology networking solutions. This document introduces the essential need-to-know technology details for developing a wireless network based on the IEEE™ 802.15.4 and Wi-SUN FAN specification supported by TI 15.4-Stack.

Note

Do not use this document as a substitute for the complete specification. For more details, see the IEEE 802.15.4 specification and Wi-SUN FAN specification.

SimpleLink CC13x0 SDK

The SimpleLink CC13x0 SDK is part of TI’s SimpleLink MCU platform, offering a single development environment that delivers flexible hardware, software and tool options for customers developing wired and wireless applications. For more information about the SimpleLink MCU platform, visit (https://www.ti.com/simplelink).

The Institute of Electrical and Electronics Engineers IEEE 802.15.4 standard defines the physical PHY and media access control MAC layers of the Open Systems Interconnection OSI model of network operations. The PHY defines the wireless link conditions like modulation, frequency, and power, while the MAC defines the format of the data.

TI implementation of this standard combines the following:

  • The basic standard (802.15.4-2006) with the most recent updates
  • The 802.15.4e for industrial applications and 802.15.4g for the smart utility networks SUN
  • An implementation of Wi-SUN frequency hopping

Disclaimer

  • SimpleLink, TI-RTOS, Code Composer Studio, Sensor Controller Studio, SmartRF, BoosterPack are trademarks of Texas Instruments.
  • ARM, Cortex are registered trademarks of ARM Ltd.
  • Wireshark is a trademark of CACE Technologies, LLC.
  • IEEE is a trademark of International Electrical and Electronics Engineers.
  • Node.js is a registered trademark of Joyent, Inc.
  • Linux is a registered trademark of Linus Torvalds.
  • Windows is a registered trademark of Microsoft Corporation.
  • Wi-SUN is a registered trademark of Wi-SUN Alliance.
  • All other trademarks are the property of their respective owners.