EMACMSP432E4 Hardware attributes. More...
#include <EMACMSP432E4.h>
Data Fields | |
uint32_t | baseAddr |
Base address of the EMAC peripheral. More... | |
uint32_t | intNum |
The EMAC peripheral's interrupt number. More... | |
uint32_t | intPriority |
The EMAC peripheral's interrupt priority. More... | |
uint32_t | led0Pin |
Pin connected to an LED used to indicate the Ethernet link is nominal. More... | |
uint32_t | led1Pin |
Pin connected to an LED used to indicate the Ethernet transmit (TX) and receive (RX) activity. More... | |
uint8_t * | macAddress |
Pointer to a MAC address. More... | |
EMACMSP432E4 Hardware attributes.
uint32_t EMACMSP432E4_HWAttrs::baseAddr |
Base address of the EMAC peripheral.
uint32_t EMACMSP432E4_HWAttrs::intNum |
The EMAC peripheral's interrupt number.
uint32_t EMACMSP432E4_HWAttrs::intPriority |
The EMAC peripheral's interrupt priority.
The interrupt priority is operating system dependent. This value is passed unmodified to the underlying interrupt handler creation code.
uint32_t EMACMSP432E4_HWAttrs::led0Pin |
Pin connected to an LED used to indicate the Ethernet link is nominal.
uint32_t EMACMSP432E4_HWAttrs::led1Pin |
Pin connected to an LED used to indicate the Ethernet transmit (TX) and receive (RX) activity.
uint8_t* EMACMSP432E4_HWAttrs::macAddress |
Pointer to a MAC address.
If this points to a value of ff:ff:ff:ff:ff:ff
, the driver reads the MAC address stored in flash. Otherwise, the value pointed to is used. An example declaration is provided below.