EMACMSP432E4.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2017-2019, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 /*!****************************************************************************
33  * @file EMACMSP432E4.h
34  * @brief Ethernet Media Access Control (EMAC) MSP432E4 Driver
35  *
36  ******************************************************************************
37  */
38 
39 #ifndef ti_drivers_emac_EMACMSP432E4__include
40 #define ti_drivers_emac_EMACMSP432E4__include
41 
42 /* @cond */
46 #ifndef __MSP432E411Y__
47 #define __MSP432E411Y__ 1
48 #endif
49 
50 #include <stdint.h>
51 #include <ti/devices/msp432e4/inc/msp432.h>
52 #include <ti/devices/msp432e4/driverlib/pin_map.h>
53 /* @endcond */
54 
55 #include <ti/ndk/inc/stkmain.h>
57 
58 #ifdef __cplusplus
59 extern "C" {
60 #endif
61 
65 #define EMACMSP432E4_PF0_EN0LED0 GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTF, 0, GPIO_PF0_EN0LED0)
66 
70 #define EMACMSP432E4_PK4_EN0LED0 GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTK, 4, GPIO_PK4_EN0LED0)
71 
75 #define EMACMSP432E4_PF4_EN0LED1 GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTF, 4, GPIO_PF4_EN0LED1)
76 
80 #define EMACMSP432E4_PK6_EN0LED1 GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTK, 6, GPIO_PK6_EN0LED1)
81 
85 #define EMACMSP432E4_PF1_EN0LED2 GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTF, 1, GPIO_PF1_EN0LED2)
86 
90 #define EMACMSP432E4_PK5_EN0LED2 GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTK, 5, GPIO_PK5_EN0LED2)
91 
95 #define EMACMSP432E4_ETHERNET_NAME "eth0"
96 
101 typedef struct {
103  uint32_t baseAddr;
104 
108  uint32_t intNum;
109 
117  uint32_t intPriority;
118 
123  uint32_t led0Pin;
124 
129  uint32_t led1Pin;
130 
143  uint8_t *macAddress;
144 
146 
153 extern bool EMACMSP432E4_isLinkUp();
154 
163 extern int EMACMSP432E4_NIMUInit(STKEVENT_Handle hEvent);
164 
165 #ifdef __cplusplus
166 }
167 #endif
168 
169 #endif /* ti_drivers_emac_EMACMSP432E4__include */
uint32_t intPriority
The EMAC peripheral&#39;s interrupt priority.
Definition: EMACMSP432E4.h:117
EMACMSP432E4 Hardware attributes.
Definition: EMACMSP432E4.h:101
uint32_t led1Pin
Pin connected to an LED used to indicate the Ethernet transmit (TX) and receive (RX) activity...
Definition: EMACMSP432E4.h:129
int EMACMSP432E4_NIMUInit(STKEVENT_Handle hEvent)
This function is included in the NIMUDeviceTable that is used by the NDK to initialize and register t...
uint8_t * macAddress
Pointer to a MAC address.
Definition: EMACMSP432E4.h:143
uint32_t baseAddr
Base address of the EMAC peripheral.
Definition: EMACMSP432E4.h:103
bool EMACMSP432E4_isLinkUp()
This function returns the link state of the EMACMSP432E4 driver.
MSP432E4 GPIO driver.
uint32_t led0Pin
Pin connected to an LED used to indicate the Ethernet link is nominal.
Definition: EMACMSP432E4.h:123
uint32_t intNum
The EMAC peripheral&#39;s interrupt number.
Definition: EMACMSP432E4.h:108
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale