USBLib API Guide  1.00.00.01
Data Structures | Macros | Enumerations | Functions | Variables
Hid_mouse_device_class_api
Collaboration diagram for Hid_mouse_device_class_api:

Data Structures

struct  tHIDMouseInstance
 
struct  tUSBDHIDMouseDevice
 
struct  PACKED
 USB_CDC_GET/SET_LINE_CODING request-specific data. More...
 

Macros

#define NUM_HID_SECTIONS
 
#define HID_REPORT_BUTTONS   0
 
#define HID_REPORT_X   1
 
#define HID_REPORT_Y   2
 
#define MOUSE_REPORT_SIZE   3
 
#define MOUSE_SUCCESS   0
 This return code from USBDHIDMouseStateChange() indicates success. More...
 
#define MOUSE_ERR_TX_ERROR   2
 
#define MOUSE_ERR_NOT_CONFIGURED   4
 
#define MOUSE_REPORT_BUTTON_1   0x01
 
#define MOUSE_REPORT_BUTTON_2   0x02
 
#define MOUSE_REPORT_BUTTON_3   0x04
 

Enumerations

enum  tMouseState { eHIDMouseStateUnconfigured, eHIDMouseStateIdle, eHIDMouseStateWaitData, eHIDMouseStateSend }
 

Functions

void * USBDHIDMouseInit (uint32_t ui32Index, tUSBDHIDMouseDevice *psMouseDevice)
 
void * USBDHIDMouseCompositeInit (uint32_t ui32Index, tUSBDHIDMouseDevice *psMouseDevice, tCompositeEntry *psCompEntry)
 
void USBDHIDMouseTerm (void *pvMouseDevice)
 
void * USBDHIDMouseSetCBData (void *pvMouseDevice, void *pvCBData)
 
uint32_t USBDHIDMouseStateChange (void *pvMouseDevice, int8_t i8DeltaX, int8_t i8DeltaY, uint8_t ui8Buttons)
 
void USBDHIDMousePowerStatusSet (void *pvMouseDevice, uint8_t ui8Power)
 
bool USBDHIDMouseRemoteWakeupRequest (void *pvMouseDevice)
 

Variables

uint8_t g_pui8MouseDescriptor []
 
uint8_t g_pui8HIDInterface [HIDINTERFACE_SIZE]
 
const uint8_t g_pui8HIDInEndpoint [HIDINENDPOINT_SIZE]
 
const tConfigSection g_sHIDConfigSection
 
const tConfigSection g_sHIDInterfaceSection
 
const tConfigSection g_sHIDInEndpointSection
 
tConfigSection g_sHIDDescriptorSection
 
const tConfigSectiong_psHIDSections []
 
tConfigHeader g_sHIDConfigHeader
 
const tConfigHeader *const g_ppsHIDConfigDescriptors []
 

Detailed Description

Macro Definition Documentation

§ NUM_HID_SECTIONS

#define NUM_HID_SECTIONS
Value:
(sizeof(g_psHIDSections) / \
sizeof(g_psHIDSections[0]))
const tConfigSection * g_psHIDSections[]
Definition: usbdhidmouse.c:237

§ HID_REPORT_BUTTONS

#define HID_REPORT_BUTTONS   0

Referenced by USBDHIDMouseStateChange().

§ HID_REPORT_X

#define HID_REPORT_X   1

Referenced by USBDHIDMouseStateChange().

§ HID_REPORT_Y

#define HID_REPORT_Y   2

Referenced by USBDHIDMouseStateChange().

§ MOUSE_REPORT_SIZE

#define MOUSE_REPORT_SIZE   3

Referenced by USBDHIDMouseStateChange().

§ MOUSE_SUCCESS

#define MOUSE_SUCCESS   0

This return code from USBDHIDMouseStateChange() indicates success.

Referenced by USBDHIDMouseStateChange().

§ MOUSE_ERR_TX_ERROR

#define MOUSE_ERR_TX_ERROR   2

This return code from USBDHIDMouseStateChange() indicates that an error was reported while attempting to send a report to the host. A client should assume that the host has disconnected if this return code is seen.

Referenced by USBDHIDMouseStateChange().

§ MOUSE_ERR_NOT_CONFIGURED

#define MOUSE_ERR_NOT_CONFIGURED   4

USBDHIDMouseStateChange() returns this value if it is called before the USB host has connected and configured the device. All mouse state information passed on the call is been ignored.

Referenced by USBDHIDMouseStateChange().

§ MOUSE_REPORT_BUTTON_1

#define MOUSE_REPORT_BUTTON_1   0x01

Setting this bit in the ui8Buttons parameter to USBDHIDMouseStateChange() indicates to the USB host that button 1 on the mouse is pressed.

§ MOUSE_REPORT_BUTTON_2

#define MOUSE_REPORT_BUTTON_2   0x02

Setting this bit in the ui8Buttons parameter to USBDHIDMouseStateChange() indicates to the USB host that button 2 on the mouse is pressed.

§ MOUSE_REPORT_BUTTON_3

#define MOUSE_REPORT_BUTTON_3   0x04

Setting this bit in the ui8Buttons parameter to USBDHIDMouseStateChange() indicates to the USB host that button 3 on the mouse is pressed.

Enumeration Type Documentation

§ tMouseState

Enumerator
eHIDMouseStateUnconfigured 
eHIDMouseStateIdle 
eHIDMouseStateWaitData 
eHIDMouseStateSend 

Function Documentation

§ USBDHIDMouseInit()

void * USBDHIDMouseInit ( uint32_t  ui32Index,
tUSBDHIDMouseDevice psMouseDevice 
)

Initializes HID mouse device operation for a given USB controller.

Parameters
ui32Indexis the index of the USB controller which is to be initialized for HID mouse device operation.
psMouseDevicepoints to a structure containing parameters customizing the operation of the HID mouse device.

An application wishing to offer a USB HID mouse interface to a USB host must call this function to initialize the USB controller and attach the mouse device to the USB bus. This function performs all required USB initialization.

On successful completion, this function returns the psMouseDevice pointer passed to it. This must be passed on all future calls to the HID mouse device driver.

When a host connects and configures the device, the application callback receives USB_EVENT_CONNECTED after which calls can be made to USBDHIDMouseStateChange() to report pointer movement and button presses to the host.

Note
The application must not make any calls to the lower level USB device interfaces if interacting with USB via the USB HID mouse device API. Doing so causes unpredictable (though almost certainly unpleasant) behavior.
Returns
Returns NULL on failure or the psMouseDevice pointer on success.

References g_pui8MouseDescriptor, tUSBDHIDMouseDevice::pfnCallback, tUSBDHIDMouseDevice::ppui8StringDescriptors, tHIDMouseInstance::sHIDDevice, tUSBDHIDMouseDevice::sPrivateData, tUSBDHIDMouseDevice::ui16MaxPowermA, tUSBDHIDMouseDevice::ui8PwrAttributes, USBDHIDInit(), and USBDHIDMouseCompositeInit().

§ USBDHIDMouseCompositeInit()

void * USBDHIDMouseCompositeInit ( uint32_t  ui32Index,
tUSBDHIDMouseDevice psMouseDevice,
tCompositeEntry psCompEntry 
)

Initializes HID mouse device operation for a given USB controller.

Parameters
ui32Indexis the index of the USB controller which is to be initialized for HID mouse device operation.
psMouseDevicepoints to a structure containing parameters customizing the operation of the HID mouse device.
psCompEntryis the composite device entry to initialize when creating a composite device.

This call is very similar to USBDHIDMouseInit() except that it is used for initializing an instance of the HID mouse device for use in a composite device. If this HID mouse is part of a composite device, then the psCompEntry should point to the composite device entry to initialize. This is part of the array that is passed to the USBDCompositeInit() function.

Returns
Returns zero on failure or a non-zero instance value that should be used with the remaining USB HID Mouse APIs.

References eHIDMouseStateUnconfigured, tHIDMouseInstance::iMouseState, tUSBDHIDMouseDevice::pfnCallback, tUSBDHIDDevice::pfnRxCallback, tUSBDHIDMouseDevice::ppui8StringDescriptors, tUSBDHIDDevice::psReportIdle, tHIDMouseInstance::sHIDDevice, tUSBDHIDMouseDevice::sPrivateData, tHIDMouseInstance::sReportIdle, tUSBDHIDMouseDevice::ui16MaxPowermA, tUSBDHIDDevice::ui16MaxPowermA, tUSBDHIDMouseDevice::ui16PID, tUSBDHIDDevice::ui16PID, tHIDReportIdle::ui16TimeTillNextmS, tUSBDHIDMouseDevice::ui16VID, tUSBDHIDDevice::ui16VID, tHIDReportIdle::ui32TimeSinceReportmS, tHIDReportIdle::ui8Duration4mS, tUSBDHIDDevice::ui8NumInputReports, tHIDMouseInstance::ui8Protocol, tUSBDHIDDevice::ui8Protocol, tUSBDHIDMouseDevice::ui8PwrAttributes, tUSBDHIDDevice::ui8PwrAttributes, tHIDReportIdle::ui8ReportID, tUSBDHIDDevice::ui8Subclass, tHIDMouseInstance::ui8USBConfigured, USB_HID_PROTOCOL_MOUSE, USB_HID_PROTOCOL_REPORT, and USB_HID_SCLASS_BOOT.

Referenced by USBDHIDMouseInit().

§ USBDHIDMouseTerm()

void USBDHIDMouseTerm ( void *  pvMouseDevice)

Shuts down the HID mouse device.

Parameters
pvMouseDeviceis the pointer to the device instance structure.

This function terminates HID mouse operation for the instance supplied and removes the device from the USB bus. Following this call, the pvMouseDevice instance may not me used in any other call to the HID mouse device other than USBDHIDMouseInit().

Returns
None.

References tHIDMouseInstance::sHIDDevice, tUSBDHIDMouseDevice::sPrivateData, tHIDMouseInstance::ui8USBConfigured, and USBDHIDTerm().

§ USBDHIDMouseSetCBData()

void * USBDHIDMouseSetCBData ( void *  pvMouseDevice,
void *  pvCBData 
)

Sets the client-specific pointer parameter for the mouse callback.

Parameters
pvMouseDeviceis the pointer to the mouse device instance structure.
pvCBDatais the pointer that client wishes to be provided on each event sent to the mouse callback function.

The client uses this function to change the callback pointer passed in the first parameter on all callbacks to the pfnCallback function passed on USBDHIDMouseInit().

If a client wants to make runtime changes in the callback pointer, it must ensure that the pvMouseDevice structure passed to USBDHIDMouseInit() resides in RAM. If this structure is in flash, callback data changes are not possible.

Returns
Returns the previous callback pointer that was set for this instance.

References tUSBDHIDMouseDevice::pvCBData.

§ USBDHIDMouseStateChange()

uint32_t USBDHIDMouseStateChange ( void *  pvMouseDevice,
int8_t  i8DeltaX,
int8_t  i8DeltaY,
uint8_t  ui8Buttons 
)

Reports a mouse state change, pointer movement or button press, to the USB host.

Parameters
pvMouseDeviceis the pointer to the mouse device instance structure.
i8DeltaXis the relative horizontal pointer movement that the application wishes to report. Valid values are in the range [-127, 127] with positive values indicating movement to the right.
i8DeltaYis the relative vertical pointer movement that the application wishes to report. Valid values are in the range [-127, 127] with positive values indicating downward movement.
ui8Buttonsis a bit mask indicating which (if any) of the three mouse buttons is pressed. Valid values are logical OR combinations of MOUSE_REPORT_BUTTON_1, MOUSE_REPORT_BUTTON_2 and MOUSE_REPORT_BUTTON_3.

This function is called to report changes in the mouse state to the USB host. These changes can be movement of the pointer, reported relative to its previous position, or changes in the states of up to 3 buttons that the mouse may support. The return code indicates whether or not the mouse report could be sent to the host. In cases where a previous report is still being transmitted, MOUSE_ERR_TX_ERROR is returned and the state change is ignored.

Returns
Returns MOUSE_SUCCESS on success, MOUSE_ERR_TX_ERROR if an error occurred while attempting to schedule transmission of the mouse report to the host (typically due to a previous report which has not yet completed transmission or due to disconnection of the host) or MOUSE_ERR_NOT_CONFIGURED if called before a host has connected to and configured the device.

References eHIDMouseStateSend, HID_REPORT_BUTTONS, HID_REPORT_X, HID_REPORT_Y, tHIDMouseInstance::iMouseState, MOUSE_ERR_NOT_CONFIGURED, MOUSE_ERR_TX_ERROR, MOUSE_REPORT_SIZE, MOUSE_SUCCESS, tHIDMouseInstance::pui8Report, tHIDMouseInstance::sHIDDevice, tUSBDHIDMouseDevice::sPrivateData, tHIDMouseInstance::ui8USBConfigured, USBDHIDReportWrite(), and USBDHIDTxPacketAvailable().

§ USBDHIDMousePowerStatusSet()

void USBDHIDMousePowerStatusSet ( void *  pvMouseDevice,
uint8_t  ui8Power 
)

Reports the device power status (bus- or self-powered) to the USB library.

Parameters
pvMouseDeviceis the pointer to the mouse device instance structure.
ui8Powerindicates the current power status, either USB_STATUS_SELF_PWR or USB_STATUS_BUS_PWR.

Applications which support switching between bus- or self-powered operation should call this function whenever the power source changes to indicate the current power status to the USB library. This information is required by the USB library to allow correct responses to be provided when the host requests status from the device.

Returns
None.

References tHIDMouseInstance::sHIDDevice, tUSBDHIDMouseDevice::sPrivateData, and USBDHIDPowerStatusSet().

§ USBDHIDMouseRemoteWakeupRequest()

bool USBDHIDMouseRemoteWakeupRequest ( void *  pvMouseDevice)

Requests a remote wake up to resume communication when in suspended state.

Parameters
pvMouseDeviceis the pointer to the mouse device instance structure.

When the bus is suspended, an application which supports remote wake up (advertised to the host via the configuration descriptor) may call this function to initiate remote wake up signaling to the host. If the remote wake up feature has not been disabled by the host, this causes the bus to resume operation within 20mS. If the host has disabled remote wake up, false is returned to indicate that the wake up request was not successful.

Returns
Returns true if the remote wake up is not disabled and the signaling was started or false if remote wake up is disabled or if signaling is currently ongoing following a previous call to this function.

References tHIDMouseInstance::sHIDDevice, tUSBDHIDMouseDevice::sPrivateData, and USBDHIDRemoteWakeupRequest().

Variable Documentation

§ g_pui8MouseDescriptor

uint8_t g_pui8MouseDescriptor[]
Initial value:
=
{
9,
USBShort(34),
1,
1,
5,
250,
}
#define USB_DTYPE_CONFIGURATION
Definition: usblib.h:281
#define USBShort(ui16Value)
Definition: usblib.h:834
#define USB_CONF_ATTR_SELF_PWR
Definition: usblib.h:602

Referenced by USBDHIDMouseInit().

§ g_pui8HIDInterface

uint8_t g_pui8HIDInterface[HIDINTERFACE_SIZE]
Initial value:
=
{
9,
0,
0,
1,
4,
}
#define USB_CLASS_HID
Definition: usblib.h:422
#define USB_DTYPE_INTERFACE
Definition: usblib.h:283
#define USB_HID_SCLASS_BOOT
Definition: usbhid.h:50
#define USB_HID_PROTOCOL_MOUSE
Definition: usbhid.h:59

§ g_pui8HIDInEndpoint

const uint8_t g_pui8HIDInEndpoint[HIDINENDPOINT_SIZE]
Initial value:
=
{
7,
USB_EP_DESC_IN | USBEPToIndex(USB_EP_1),
USBShort(USBFIFOSizeToBytes(USB_FIFO_SZ_64)),
16,
}
#define USB_EP_ATTR_INT
Definition: usblib.h:743
#define USB_DTYPE_ENDPOINT
Definition: usblib.h:284
#define USBShort(ui16Value)
Definition: usblib.h:834
#define USB_EP_DESC_IN
Definition: usblib.h:723

§ g_sHIDConfigSection

const tConfigSection g_sHIDConfigSection
Initial value:
=
{
}
uint8_t g_pui8MouseDescriptor[]
Definition: usbdhidmouse.c:54

§ g_sHIDInterfaceSection

const tConfigSection g_sHIDInterfaceSection
Initial value:
=
{
}
uint8_t g_pui8HIDInterface[HIDINTERFACE_SIZE]
Definition: usbdhidmouse.c:77

§ g_sHIDInEndpointSection

const tConfigSection g_sHIDInEndpointSection
Initial value:
=
{
}
const uint8_t g_pui8HIDInEndpoint[HIDINENDPOINT_SIZE]
Definition: usbdhidmouse.c:95

§ g_sHIDDescriptorSection

tConfigSection g_sHIDDescriptorSection
Initial value:
=
{
sizeof(g_sMouseHIDDescriptor),
(const uint8_t *)&g_sMouseHIDDescriptor
}

§ g_psHIDSections

const tConfigSection* g_psHIDSections[]
Initial value:
=
{
}
const tConfigSection g_sHIDConfigSection
Definition: usbdhidmouse.c:202
const tConfigSection g_sHIDInEndpointSection
Definition: usbdhidmouse.c:214
const tConfigSection g_sHIDInterfaceSection
Definition: usbdhidmouse.c:208
tConfigSection g_sHIDDescriptorSection
Definition: usbdhidmouse.c:225

§ g_sHIDConfigHeader

tConfigHeader g_sHIDConfigHeader
Initial value:
=
{
}
#define NUM_HID_SECTIONS
Definition: usbdhidmouse.c:245
const tConfigSection * g_psHIDSections[]
Definition: usbdhidmouse.c:237

§ g_ppsHIDConfigDescriptors

const tConfigHeader* const g_ppsHIDConfigDescriptors[]
Initial value:
=
{
}
tConfigHeader g_sHIDConfigHeader
Definition: usbdhidmouse.c:257
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale