USBLib API Guide  1.00.00.01
Data Structures | Macros
Usbchap9_src
Collaboration diagram for Usbchap9_src:

Data Structures

struct  PACKED
 USB_CDC_GET/SET_LINE_CODING request-specific data. More...
 

Macros

#define USB_RTYPE_DIR_IN   0x80
 
#define USB_RTYPE_DIR_OUT   0x00
 
#define USB_RTYPE_TYPE_M   0x60
 
#define USB_RTYPE_VENDOR   0x40
 
#define USB_RTYPE_CLASS   0x20
 
#define USB_RTYPE_STANDARD   0x00
 
#define USB_RTYPE_RECIPIENT_M   0x1f
 
#define USB_RTYPE_OTHER   0x03
 
#define USB_RTYPE_ENDPOINT   0x02
 
#define USB_RTYPE_INTERFACE   0x01
 
#define USB_RTYPE_DEVICE   0x00
 
#define USBREQ_GET_STATUS   0x00
 
#define USBREQ_CLEAR_FEATURE   0x01
 
#define USBREQ_SET_FEATURE   0x03
 
#define USBREQ_SET_ADDRESS   0x05
 
#define USBREQ_GET_DESCRIPTOR   0x06
 
#define USBREQ_SET_DESCRIPTOR   0x07
 
#define USBREQ_GET_CONFIG   0x08
 
#define USBREQ_SET_CONFIG   0x09
 
#define USBREQ_GET_INTERFACE   0x0a
 
#define USBREQ_SET_INTERFACE   0x0b
 
#define USBREQ_SYNC_FRAME   0x0c
 
#define USB_STATUS_SELF_PWR   0x0001
 
#define USB_STATUS_BUS_PWR   0x0000
 
#define USB_STATUS_PWR_M   0x0001
 
#define USB_STATUS_REMOTE_WAKE   0x0002
 
#define USB_FEATURE_EP_HALT   0x0000
 
#define USB_FEATURE_REMOTE_WAKE   0x0001
 
#define USB_FEATURE_TEST_MODE   0x0002
 
#define USB_REQ_EP_NUM_M   0x007F
 
#define USB_REQ_EP_DIR_M   0x0080
 
#define USB_REQ_EP_DIR_IN   0x0080
 
#define USB_REQ_EP_DIR_OUT   0x0000
 
#define USB_DTYPE_DEVICE   1
 
#define USB_DTYPE_CONFIGURATION   2
 
#define USB_DTYPE_STRING   3
 
#define USB_DTYPE_INTERFACE   4
 
#define USB_DTYPE_ENDPOINT   5
 
#define USB_DTYPE_DEVICE_QUAL   6
 
#define USB_DTYPE_OSPEED_CONF   7
 
#define USB_DTYPE_INTERFACE_PWR   8
 
#define USB_DTYPE_OTG   9
 
#define USB_DTYPE_INTERFACE_ASC   11
 
#define USB_DTYPE_CS_INTERFACE   36
 
#define USB_DTYPE_HUB   41
 
#define USB_CLASS_DEVICE   0x00
 
#define USB_CLASS_AUDIO   0x01
 
#define USB_CLASS_CDC   0x02
 
#define USB_CLASS_HID   0x03
 
#define USB_CLASS_PHYSICAL   0x05
 
#define USB_CLASS_IMAGE   0x06
 
#define USB_CLASS_PRINTER   0x07
 
#define USB_CLASS_MASS_STORAGE   0x08
 
#define USB_CLASS_HUB   0x09
 
#define USB_CLASS_CDC_DATA   0x0a
 
#define USB_CLASS_SMART_CARD   0x0b
 
#define USB_CLASS_SECURITY   0x0d
 
#define USB_CLASS_VIDEO   0x0e
 
#define USB_CLASS_HEALTHCARE   0x0f
 
#define USB_CLASS_DIAG_DEVICE   0xdc
 
#define USB_CLASS_WIRELESS   0xe0
 
#define USB_CLASS_MISC   0xef
 
#define USB_CLASS_APP_SPECIFIC   0xfe
 
#define USB_CLASS_VEND_SPECIFIC   0xff
 
#define USB_CLASS_EVENTS   0xffffffff
 
#define USB_SUBCLASS_UNDEFINED   0x00
 
#define USB_PROTOCOL_UNDEFINED   0x00
 
#define USB_MISC_SUBCLASS_SYNC   0x01
 
#define USB_MISC_SUBCLASS_COMMON   0x02
 
#define USB_MISC_PROTOCOL_IAD   0x01
 
#define USB_HUB_PROTOCOL_FS   0x00
 
#define USB_HUB_PROTOCOL_SINGLE   0x01
 
#define USB_HUB_PROTOCOL_MULTI   0x02
 
#define USB_CONF_ATTR_PWR_M   0xC0
 
#define USB_CONF_ATTR_SELF_PWR   0xC0
 
#define USB_CONF_ATTR_BUS_PWR   0x80
 
#define USB_CONF_ATTR_RWAKE   0xA0
 
#define USB_EP_DESC_OUT   0x00
 
#define USB_EP_DESC_IN   0x80
 
#define USB_EP_DESC_NUM_M   0x0f
 
#define USB_EP_MAX_PACKET_COUNT_M   0x07FF
 
#define USB_EP_ATTR_CONTROL   0x00
 
#define USB_EP_ATTR_ISOC   0x01
 
#define USB_EP_ATTR_BULK   0x02
 
#define USB_EP_ATTR_INT   0x03
 
#define USB_EP_ATTR_TYPE_M   0x03
 
#define USB_EP_ATTR_ISOC_M   0x0c
 
#define USB_EP_ATTR_ISOC_NOSYNC   0x00
 
#define USB_EP_ATTR_ISOC_ASYNC   0x04
 
#define USB_EP_ATTR_ISOC_ADAPT   0x08
 
#define USB_EP_ATTR_ISOC_SYNC   0x0c
 
#define USB_EP_ATTR_USAGE_M   0x30
 
#define USB_EP_ATTR_USAGE_DATA   0x00
 
#define USB_EP_ATTR_USAGE_FEEDBACK   0x10
 
#define USB_EP_ATTR_USAGE_IMPFEEDBACK   0x20
 
#define USBShort(ui16Value)   (ui16Value & 0xff), (ui16Value >> 8)
 
#define USB3Byte(ui32Value)
 
#define USBLong(ui32Value)
 
#define NEXT_USB_DESCRIPTOR(ptr)
 

Detailed Description

Macro Definition Documentation

§ USB_RTYPE_DIR_IN

#define USB_RTYPE_DIR_IN   0x80

§ USB_RTYPE_DIR_OUT

#define USB_RTYPE_DIR_OUT   0x00

§ USB_RTYPE_TYPE_M

#define USB_RTYPE_TYPE_M   0x60

§ USB_RTYPE_VENDOR

#define USB_RTYPE_VENDOR   0x40

§ USB_RTYPE_CLASS

#define USB_RTYPE_CLASS   0x20

§ USB_RTYPE_STANDARD

#define USB_RTYPE_STANDARD   0x00

§ USB_RTYPE_RECIPIENT_M

#define USB_RTYPE_RECIPIENT_M   0x1f

§ USB_RTYPE_OTHER

#define USB_RTYPE_OTHER   0x03

§ USB_RTYPE_ENDPOINT

#define USB_RTYPE_ENDPOINT   0x02

§ USB_RTYPE_INTERFACE

#define USB_RTYPE_INTERFACE   0x01

§ USB_RTYPE_DEVICE

#define USB_RTYPE_DEVICE   0x00

§ USBREQ_GET_STATUS

#define USBREQ_GET_STATUS   0x00

§ USBREQ_CLEAR_FEATURE

#define USBREQ_CLEAR_FEATURE   0x01

§ USBREQ_SET_FEATURE

#define USBREQ_SET_FEATURE   0x03

§ USBREQ_SET_ADDRESS

#define USBREQ_SET_ADDRESS   0x05

Referenced by USBHCDSetAddress().

§ USBREQ_GET_DESCRIPTOR

#define USBREQ_GET_DESCRIPTOR   0x06

§ USBREQ_SET_DESCRIPTOR

#define USBREQ_SET_DESCRIPTOR   0x07

§ USBREQ_GET_CONFIG

#define USBREQ_GET_CONFIG   0x08

§ USBREQ_SET_CONFIG

#define USBREQ_SET_CONFIG   0x09

Referenced by USBHCDSetConfig().

§ USBREQ_GET_INTERFACE

#define USBREQ_GET_INTERFACE   0x0a

§ USBREQ_SET_INTERFACE

#define USBREQ_SET_INTERFACE   0x0b

Referenced by USBHCDSetInterface().

§ USBREQ_SYNC_FRAME

#define USBREQ_SYNC_FRAME   0x0c

§ USB_STATUS_SELF_PWR

#define USB_STATUS_SELF_PWR   0x0001

Referenced by USBDCDPowerStatusSet().

§ USB_STATUS_BUS_PWR

#define USB_STATUS_BUS_PWR   0x0000

Referenced by USBDCDPowerStatusSet().

§ USB_STATUS_PWR_M

#define USB_STATUS_PWR_M   0x0001

Referenced by USBDCDPowerStatusSet().

§ USB_STATUS_REMOTE_WAKE

#define USB_STATUS_REMOTE_WAKE   0x0002

§ USB_FEATURE_EP_HALT

#define USB_FEATURE_EP_HALT   0x0000

§ USB_FEATURE_REMOTE_WAKE

#define USB_FEATURE_REMOTE_WAKE   0x0001

§ USB_FEATURE_TEST_MODE

#define USB_FEATURE_TEST_MODE   0x0002

§ USB_REQ_EP_NUM_M

#define USB_REQ_EP_NUM_M   0x007F

§ USB_REQ_EP_DIR_M

#define USB_REQ_EP_DIR_M   0x0080

§ USB_REQ_EP_DIR_IN

#define USB_REQ_EP_DIR_IN   0x0080

§ USB_REQ_EP_DIR_OUT

#define USB_REQ_EP_DIR_OUT   0x0000

§ USB_DTYPE_DEVICE

#define USB_DTYPE_DEVICE   1

§ USB_DTYPE_CONFIGURATION

#define USB_DTYPE_CONFIGURATION   2

§ USB_DTYPE_STRING

#define USB_DTYPE_STRING   3

§ USB_DTYPE_INTERFACE

#define USB_DTYPE_INTERFACE   4

§ USB_DTYPE_ENDPOINT

#define USB_DTYPE_ENDPOINT   5

§ USB_DTYPE_DEVICE_QUAL

#define USB_DTYPE_DEVICE_QUAL   6

§ USB_DTYPE_OSPEED_CONF

#define USB_DTYPE_OSPEED_CONF   7

§ USB_DTYPE_INTERFACE_PWR

#define USB_DTYPE_INTERFACE_PWR   8

§ USB_DTYPE_OTG

#define USB_DTYPE_OTG   9

§ USB_DTYPE_INTERFACE_ASC

#define USB_DTYPE_INTERFACE_ASC   11

§ USB_DTYPE_CS_INTERFACE

#define USB_DTYPE_CS_INTERFACE   36

§ USB_DTYPE_HUB

#define USB_DTYPE_HUB   41

§ USB_CLASS_DEVICE

#define USB_CLASS_DEVICE   0x00

§ USB_CLASS_AUDIO

#define USB_CLASS_AUDIO   0x01

§ USB_CLASS_CDC

#define USB_CLASS_CDC   0x02

§ USB_CLASS_HID

#define USB_CLASS_HID   0x03

§ USB_CLASS_PHYSICAL

#define USB_CLASS_PHYSICAL   0x05

§ USB_CLASS_IMAGE

#define USB_CLASS_IMAGE   0x06

§ USB_CLASS_PRINTER

#define USB_CLASS_PRINTER   0x07

§ USB_CLASS_MASS_STORAGE

#define USB_CLASS_MASS_STORAGE   0x08

§ USB_CLASS_HUB

#define USB_CLASS_HUB   0x09

§ USB_CLASS_CDC_DATA

#define USB_CLASS_CDC_DATA   0x0a

§ USB_CLASS_SMART_CARD

#define USB_CLASS_SMART_CARD   0x0b

§ USB_CLASS_SECURITY

#define USB_CLASS_SECURITY   0x0d

§ USB_CLASS_VIDEO

#define USB_CLASS_VIDEO   0x0e

§ USB_CLASS_HEALTHCARE

#define USB_CLASS_HEALTHCARE   0x0f

§ USB_CLASS_DIAG_DEVICE

#define USB_CLASS_DIAG_DEVICE   0xdc

§ USB_CLASS_WIRELESS

#define USB_CLASS_WIRELESS   0xe0

§ USB_CLASS_MISC

#define USB_CLASS_MISC   0xef

§ USB_CLASS_APP_SPECIFIC

#define USB_CLASS_APP_SPECIFIC   0xfe

§ USB_CLASS_VEND_SPECIFIC

#define USB_CLASS_VEND_SPECIFIC   0xff

§ USB_CLASS_EVENTS

#define USB_CLASS_EVENTS   0xffffffff

§ USB_SUBCLASS_UNDEFINED

#define USB_SUBCLASS_UNDEFINED   0x00

§ USB_PROTOCOL_UNDEFINED

#define USB_PROTOCOL_UNDEFINED   0x00

§ USB_MISC_SUBCLASS_SYNC

#define USB_MISC_SUBCLASS_SYNC   0x01

§ USB_MISC_SUBCLASS_COMMON

#define USB_MISC_SUBCLASS_COMMON   0x02

§ USB_MISC_PROTOCOL_IAD

#define USB_MISC_PROTOCOL_IAD   0x01

§ USB_HUB_PROTOCOL_FS

#define USB_HUB_PROTOCOL_FS   0x00

§ USB_HUB_PROTOCOL_SINGLE

#define USB_HUB_PROTOCOL_SINGLE   0x01

§ USB_HUB_PROTOCOL_MULTI

#define USB_HUB_PROTOCOL_MULTI   0x02

§ USB_CONF_ATTR_PWR_M

#define USB_CONF_ATTR_PWR_M   0xC0

§ USB_CONF_ATTR_SELF_PWR

#define USB_CONF_ATTR_SELF_PWR   0xC0

§ USB_CONF_ATTR_BUS_PWR

#define USB_CONF_ATTR_BUS_PWR   0x80

§ USB_CONF_ATTR_RWAKE

#define USB_CONF_ATTR_RWAKE   0xA0

§ USB_EP_DESC_OUT

#define USB_EP_DESC_OUT   0x00

§ USB_EP_DESC_IN

#define USB_EP_DESC_IN   0x80

Referenced by USBDeviceConfig().

§ USB_EP_DESC_NUM_M

#define USB_EP_DESC_NUM_M   0x0f

Referenced by USBDeviceConfig().

§ USB_EP_MAX_PACKET_COUNT_M

#define USB_EP_MAX_PACKET_COUNT_M   0x07FF

§ USB_EP_ATTR_CONTROL

#define USB_EP_ATTR_CONTROL   0x00

§ USB_EP_ATTR_ISOC

#define USB_EP_ATTR_ISOC   0x01

§ USB_EP_ATTR_BULK

#define USB_EP_ATTR_BULK   0x02

§ USB_EP_ATTR_INT

#define USB_EP_ATTR_INT   0x03

§ USB_EP_ATTR_TYPE_M

#define USB_EP_ATTR_TYPE_M   0x03

§ USB_EP_ATTR_ISOC_M

#define USB_EP_ATTR_ISOC_M   0x0c

§ USB_EP_ATTR_ISOC_NOSYNC

#define USB_EP_ATTR_ISOC_NOSYNC   0x00

§ USB_EP_ATTR_ISOC_ASYNC

#define USB_EP_ATTR_ISOC_ASYNC   0x04

§ USB_EP_ATTR_ISOC_ADAPT

#define USB_EP_ATTR_ISOC_ADAPT   0x08

§ USB_EP_ATTR_ISOC_SYNC

#define USB_EP_ATTR_ISOC_SYNC   0x0c

§ USB_EP_ATTR_USAGE_M

#define USB_EP_ATTR_USAGE_M   0x30

§ USB_EP_ATTR_USAGE_DATA

#define USB_EP_ATTR_USAGE_DATA   0x00

§ USB_EP_ATTR_USAGE_FEEDBACK

#define USB_EP_ATTR_USAGE_FEEDBACK   0x10

§ USB_EP_ATTR_USAGE_IMPFEEDBACK

#define USB_EP_ATTR_USAGE_IMPFEEDBACK   0x20

§ USBShort

#define USBShort (   ui16Value)    (ui16Value & 0xff), (ui16Value >> 8)

Write a 16-bit value to a USB descriptor block.

Parameters
ui16Valueis the 16-bit value to write to the descriptor.

This helper macro is used in descriptor definitions to write two-byte values. Since the configuration descriptor contains all interface and endpoint descriptors in a contiguous block of memory, these descriptors are typically defined using an array of bytes rather than as packed structures.

Returns
Not a function.

§ USB3Byte

#define USB3Byte (   ui32Value)
Value:
(ui32Value & 0xff), \
((ui32Value >> 8) & 0xff), \
((ui32Value >> 16) & 0xff)

Write a 24-bit value to a USB descriptor block.

Parameters
ui32Valueis the 24-bit value that to write to the descriptor.

This helper macro is used in descriptor definitions to write three-byte values. Since the configuration descriptor contains all interface and endpoint descriptors in a contiguous block of memory, these descriptors are typically defined using an array of bytes rather than as packed structures.

Returns
Not a function.

§ USBLong

#define USBLong (   ui32Value)
Value:
(ui32Value & 0xff), \
((ui32Value >> 8) & 0xff), \
((ui32Value >> 16) & 0xff), \
((ui32Value >> 24) & 0xff)

Write a 32-bit value to a USB descriptor block.

Parameters
ui32Valueis the 32-bit value that to write to the descriptor.

This helper macro is used in descriptor definitions to write four-byte values. Since the configuration descriptor contains all interface and endpoint descriptors in a contiguous block of memory, these descriptors are typically defined using an array of bytes rather than as packed structures.

Returns
Not a function.

§ NEXT_USB_DESCRIPTOR

#define NEXT_USB_DESCRIPTOR (   ptr)
Value:
(tDescriptorHeader *)(((uint8_t *)(ptr)) + \
*((uint8_t *)(ptr)))

Traverse to the next USB descriptor in a block.

Parameters
ptrpoints to the first byte of a descriptor in a block of USB descriptors.

This macro aids in traversing lists of descriptors by returning a pointer to the next descriptor in the list given a pointer to the current one.

Returns
Returns a pointer to the next descriptor in the block following ptr.

Referenced by USBDescGet(), USBDescGetNum(), and USBDescGetNumAlternateInterfaces().

© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale