#include <usbdhid.h>
Data Fields | |
uint16_t | ui16VID |
The vendor ID that this device is to present in the device descriptor. More... | |
uint16_t | ui16PID |
The product ID that this device is to present in the device descriptor. More... | |
uint16_t | ui16MaxPowermA |
The maximum power consumption of the device, expressed in milliamps. More... | |
uint8_t | ui8PwrAttributes |
uint8_t | ui8Subclass |
The interface subclass to publish to the server for this HID device. More... | |
uint8_t | ui8Protocol |
The interface protocol to publish to the server for this HID device. More... | |
uint8_t | ui8NumInputReports |
tHIDReportIdle * | psReportIdle |
tUSBCallback | pfnRxCallback |
void * | pvRxCBData |
tUSBCallback | pfnTxCallback |
void * | pvTxCBData |
bool | bUseOutEndpoint |
const tHIDDescriptor * | psHIDDescriptor |
const uint8_t *const * | ppui8ClassDescriptors |
const uint8_t *const * | ppui8StringDescriptors |
uint32_t | ui32NumStringDescriptors |
const tConfigHeader *const * | ppsConfigDescriptor |
tHIDInstance | sPrivateData |
The structure used by the application to define operating parameters for the HID device.
uint16_t tUSBDHIDDevice::ui16VID |
The vendor ID that this device is to present in the device descriptor.
Referenced by USBDHIDGamepadCompositeInit(), USBDHIDInit(), USBDHIDKeyboardCompositeInit(), USBDHIDMouseCompositeInit(), and USBDHIDSensorCompositeInit().
uint16_t tUSBDHIDDevice::ui16PID |
The product ID that this device is to present in the device descriptor.
Referenced by USBDHIDGamepadCompositeInit(), USBDHIDInit(), USBDHIDKeyboardCompositeInit(), USBDHIDMouseCompositeInit(), and USBDHIDSensorCompositeInit().
uint16_t tUSBDHIDDevice::ui16MaxPowermA |
The maximum power consumption of the device, expressed in milliamps.
Referenced by USBDHIDGamepadCompositeInit(), USBDHIDKeyboardCompositeInit(), USBDHIDMouseCompositeInit(), and USBDHIDSensorCompositeInit().
uint8_t tUSBDHIDDevice::ui8PwrAttributes |
Indicates whether the device is self- or bus-powered and whether or not it supports remote wakeup. Valid values are USB_CONF_ATTR_SELF_PWR or USB_CONF_ATTR_BUS_PWR, optionally ORed with USB_CONF_ATTR_RWAKE.
Referenced by USBDHIDGamepadCompositeInit(), USBDHIDKeyboardCompositeInit(), USBDHIDMouseCompositeInit(), and USBDHIDSensorCompositeInit().
uint8_t tUSBDHIDDevice::ui8Subclass |
The interface subclass to publish to the server for this HID device.
Referenced by USBDHIDGamepadCompositeInit(), USBDHIDKeyboardCompositeInit(), USBDHIDMouseCompositeInit(), and USBDHIDSensorCompositeInit().
uint8_t tUSBDHIDDevice::ui8Protocol |
The interface protocol to publish to the server for this HID device.
Referenced by USBDHIDGamepadCompositeInit(), USBDHIDKeyboardCompositeInit(), USBDHIDMouseCompositeInit(), and USBDHIDSensorCompositeInit().
uint8_t tUSBDHIDDevice::ui8NumInputReports |
The number of Input reports that this device supports. This field must equal the number of reports published in the HID class descriptors for the device and also the number of entries in the array whose first element is pointed to by field pi16ReportIdle below.
Referenced by USBDHIDCompositeInit(), USBDHIDGamepadCompositeInit(), USBDHIDInit(), USBDHIDKeyboardCompositeInit(), USBDHIDMouseCompositeInit(), and USBDHIDSensorCompositeInit().
tHIDReportIdle* tUSBDHIDDevice::psReportIdle |
A pointer to the first element in an array of structures used to track idle time for each Input report. When USBDHIDInit() is called, the ui8Duration4mS and ui8ReportID fields of each of these array members should be initialized to indicate the default idle timeout for each input report. This array must be in RAM since the HID device class driver updates values in it in response to requests from the host and to track elapsed time. The number of elements in the array must match the number supplied in the ui8NumInputReports field above.
Referenced by USBDHIDCompositeInit(), USBDHIDGamepadCompositeInit(), USBDHIDInit(), USBDHIDKeyboardCompositeInit(), USBDHIDMouseCompositeInit(), and USBDHIDSensorCompositeInit().
tUSBCallback tUSBDHIDDevice::pfnRxCallback |
A pointer to the callback function which is called to notify the application of general events, events related to report transfers on endpoint zero and events related to reception of Output and Feature reports via the (optional) interrupt OUT endpoint.
Referenced by USBDHIDCompositeInit(), USBDHIDInit(), USBDHIDKeyboardCompositeInit(), USBDHIDMouseCompositeInit(), and USBDHIDSensorCompositeInit().
void* tUSBDHIDDevice::pvRxCBData |
A client-supplied pointer which is sent as the first parameter in all calls made to the receive channel callback, pfnRxCallback.
tUSBCallback tUSBDHIDDevice::pfnTxCallback |
A pointer to the callback function which is called to notify the application of events related to transmission of Input reports via the interrupt IN endpoint.
Referenced by USBDHIDCompositeInit(), USBDHIDGamepadCompositeInit(), and USBDHIDInit().
void* tUSBDHIDDevice::pvTxCBData |
A client-supplied pointer which is sent as the first parameter in all calls made to the transmit channel callback, pfnTxCallback.
bool tUSBDHIDDevice::bUseOutEndpoint |
If set to true, this field indicates that the device should use a dedicated interrupt OUT endpoint to receive reports from the host. In this case, reports from the host are passed to the application via the receive callback using USB_EVENT_RX_AVAILABLE events. If false, reports from the host are received via endpoint zero and passed to the application via USBD_HID_EVENT_REPORT_SENT events.
const tHIDDescriptor* tUSBDHIDDevice::psHIDDescriptor |
The HID descriptor that the device is to publish (following the standard interface descriptor and prior to the endpoint descriptors for the interface).
Referenced by USBDHIDCompositeInit(), and USBDHIDInit().
const uint8_t* const* tUSBDHIDDevice::ppui8ClassDescriptors |
The HID class descriptors offered by the device are defined in an array of byte pointers and this field points to that array. The order and number of elements in the array must match the associated information provided in the HID descriptor in field by pi16HIDDescriptor.
Referenced by USBDHIDCompositeInit(), and USBDHIDInit().
const uint8_t* const* tUSBDHIDDevice::ppui8StringDescriptors |
A pointer to the string descriptor array for this device. This array must contain the following string descriptor pointers in this order. Language descriptor, Manufacturer name string (language 1), Product name string (language 1), Serial number string (language 1),HID Interface description string (language 1), Configuration description string (language 1), (optionally) First HID device-specific string (language 1), (optionally) Second HID device-specific string (language 1), etc.
If supporting more than 1 language, the descriptor block (except for string descriptor 0) must be repeated for each language defined in the language descriptor.
The number of HID device-specific strings is dependent upon the content of the report descriptor passed to the interface and is, thus, application controlled.
Referenced by USBDHIDCompositeInit(), and USBDHIDInit().
uint32_t tUSBDHIDDevice::ui32NumStringDescriptors |
The number of descriptors provided in the ppStringDescriptors array. This must be 1 + ((5 + (num HID strings)) * (num languages)).
Referenced by USBDHIDCompositeInit().
const tConfigHeader* const* tUSBDHIDDevice::ppsConfigDescriptor |
Referenced by USBDHIDCompositeInit().
tHIDInstance tUSBDHIDDevice::sPrivateData |
The private instance data for this device instance. This memory must remain accessible for as long as the HID device is in use and must not be modified by any code outside the HID class driver.
Referenced by USBDHIDCompositeInit(), and USBDHIDInit().