Data Structures | |
struct | tHIDMouseInstance |
struct | tUSBDHIDMouseDevice |
struct | PACKED |
USB_CDC_GET/SET_LINE_CODING request-specific data. More... | |
Macros | |
#define | NUM_HID_SECTIONS |
#define | HID_REPORT_BUTTONS 0 |
#define | HID_REPORT_X 1 |
#define | HID_REPORT_Y 2 |
#define | MOUSE_REPORT_SIZE 3 |
#define | MOUSE_SUCCESS 0 |
This return code from USBDHIDMouseStateChange() indicates success. More... | |
#define | MOUSE_ERR_TX_ERROR 2 |
#define | MOUSE_ERR_NOT_CONFIGURED 4 |
#define | MOUSE_REPORT_BUTTON_1 0x01 |
#define | MOUSE_REPORT_BUTTON_2 0x02 |
#define | MOUSE_REPORT_BUTTON_3 0x04 |
Enumerations | |
enum | tMouseState { eHIDMouseStateUnconfigured, eHIDMouseStateIdle, eHIDMouseStateWaitData, eHIDMouseStateSend } |
Functions | |
void * | USBDHIDMouseInit (uint32_t ui32Index, tUSBDHIDMouseDevice *psMouseDevice) |
void * | USBDHIDMouseCompositeInit (uint32_t ui32Index, tUSBDHIDMouseDevice *psMouseDevice, tCompositeEntry *psCompEntry) |
void | USBDHIDMouseTerm (void *pvMouseDevice) |
void * | USBDHIDMouseSetCBData (void *pvMouseDevice, void *pvCBData) |
uint32_t | USBDHIDMouseStateChange (void *pvMouseDevice, int8_t i8DeltaX, int8_t i8DeltaY, uint8_t ui8Buttons) |
void | USBDHIDMousePowerStatusSet (void *pvMouseDevice, uint8_t ui8Power) |
bool | USBDHIDMouseRemoteWakeupRequest (void *pvMouseDevice) |
Variables | |
uint8_t | g_pui8MouseDescriptor [] |
uint8_t | g_pui8HIDInterface [HIDINTERFACE_SIZE] |
const uint8_t | g_pui8HIDInEndpoint [HIDINENDPOINT_SIZE] |
const tConfigSection | g_sHIDConfigSection |
const tConfigSection | g_sHIDInterfaceSection |
const tConfigSection | g_sHIDInEndpointSection |
tConfigSection | g_sHIDDescriptorSection |
const tConfigSection * | g_psHIDSections [] |
tConfigHeader | g_sHIDConfigHeader |
const tConfigHeader *const | g_ppsHIDConfigDescriptors [] |
#define NUM_HID_SECTIONS |
#define HID_REPORT_BUTTONS 0 |
Referenced by USBDHIDMouseStateChange().
#define HID_REPORT_X 1 |
Referenced by USBDHIDMouseStateChange().
#define HID_REPORT_Y 2 |
Referenced by USBDHIDMouseStateChange().
#define MOUSE_REPORT_SIZE 3 |
Referenced by USBDHIDMouseStateChange().
#define MOUSE_SUCCESS 0 |
This return code from USBDHIDMouseStateChange() indicates success.
Referenced by USBDHIDMouseStateChange().
#define MOUSE_ERR_TX_ERROR 2 |
This return code from USBDHIDMouseStateChange() indicates that an error was reported while attempting to send a report to the host. A client should assume that the host has disconnected if this return code is seen.
Referenced by USBDHIDMouseStateChange().
#define MOUSE_ERR_NOT_CONFIGURED 4 |
USBDHIDMouseStateChange() returns this value if it is called before the USB host has connected and configured the device. All mouse state information passed on the call is been ignored.
Referenced by USBDHIDMouseStateChange().
#define MOUSE_REPORT_BUTTON_1 0x01 |
Setting this bit in the ui8Buttons parameter to USBDHIDMouseStateChange() indicates to the USB host that button 1 on the mouse is pressed.
#define MOUSE_REPORT_BUTTON_2 0x02 |
Setting this bit in the ui8Buttons parameter to USBDHIDMouseStateChange() indicates to the USB host that button 2 on the mouse is pressed.
#define MOUSE_REPORT_BUTTON_3 0x04 |
Setting this bit in the ui8Buttons parameter to USBDHIDMouseStateChange() indicates to the USB host that button 3 on the mouse is pressed.
enum tMouseState |
void * USBDHIDMouseInit | ( | uint32_t | ui32Index, |
tUSBDHIDMouseDevice * | psMouseDevice | ||
) |
Initializes HID mouse device operation for a given USB controller.
ui32Index | is the index of the USB controller which is to be initialized for HID mouse device operation. |
psMouseDevice | points to a structure containing parameters customizing the operation of the HID mouse device. |
An application wishing to offer a USB HID mouse interface to a USB host must call this function to initialize the USB controller and attach the mouse device to the USB bus. This function performs all required USB initialization.
On successful completion, this function returns the psMouseDevice pointer passed to it. This must be passed on all future calls to the HID mouse device driver.
When a host connects and configures the device, the application callback receives USB_EVENT_CONNECTED after which calls can be made to USBDHIDMouseStateChange() to report pointer movement and button presses to the host.
References g_pui8MouseDescriptor, tUSBDHIDMouseDevice::pfnCallback, tUSBDHIDMouseDevice::ppui8StringDescriptors, tHIDMouseInstance::sHIDDevice, tUSBDHIDMouseDevice::sPrivateData, tUSBDHIDMouseDevice::ui16MaxPowermA, tUSBDHIDMouseDevice::ui8PwrAttributes, USBDHIDInit(), and USBDHIDMouseCompositeInit().
void * USBDHIDMouseCompositeInit | ( | uint32_t | ui32Index, |
tUSBDHIDMouseDevice * | psMouseDevice, | ||
tCompositeEntry * | psCompEntry | ||
) |
Initializes HID mouse device operation for a given USB controller.
ui32Index | is the index of the USB controller which is to be initialized for HID mouse device operation. |
psMouseDevice | points to a structure containing parameters customizing the operation of the HID mouse device. |
psCompEntry | is the composite device entry to initialize when creating a composite device. |
This call is very similar to USBDHIDMouseInit() except that it is used for initializing an instance of the HID mouse device for use in a composite device. If this HID mouse is part of a composite device, then the psCompEntry should point to the composite device entry to initialize. This is part of the array that is passed to the USBDCompositeInit() function.
References eHIDMouseStateUnconfigured, tHIDMouseInstance::iMouseState, tUSBDHIDMouseDevice::pfnCallback, tUSBDHIDDevice::pfnRxCallback, tUSBDHIDMouseDevice::ppui8StringDescriptors, tUSBDHIDDevice::psReportIdle, tHIDMouseInstance::sHIDDevice, tUSBDHIDMouseDevice::sPrivateData, tHIDMouseInstance::sReportIdle, tUSBDHIDMouseDevice::ui16MaxPowermA, tUSBDHIDDevice::ui16MaxPowermA, tUSBDHIDMouseDevice::ui16PID, tUSBDHIDDevice::ui16PID, tHIDReportIdle::ui16TimeTillNextmS, tUSBDHIDMouseDevice::ui16VID, tUSBDHIDDevice::ui16VID, tHIDReportIdle::ui32TimeSinceReportmS, tHIDReportIdle::ui8Duration4mS, tUSBDHIDDevice::ui8NumInputReports, tHIDMouseInstance::ui8Protocol, tUSBDHIDDevice::ui8Protocol, tUSBDHIDMouseDevice::ui8PwrAttributes, tUSBDHIDDevice::ui8PwrAttributes, tHIDReportIdle::ui8ReportID, tUSBDHIDDevice::ui8Subclass, tHIDMouseInstance::ui8USBConfigured, USB_HID_PROTOCOL_MOUSE, USB_HID_PROTOCOL_REPORT, and USB_HID_SCLASS_BOOT.
Referenced by USBDHIDMouseInit().
void USBDHIDMouseTerm | ( | void * | pvMouseDevice | ) |
Shuts down the HID mouse device.
pvMouseDevice | is the pointer to the device instance structure. |
This function terminates HID mouse operation for the instance supplied and removes the device from the USB bus. Following this call, the pvMouseDevice instance may not me used in any other call to the HID mouse device other than USBDHIDMouseInit().
References tHIDMouseInstance::sHIDDevice, tUSBDHIDMouseDevice::sPrivateData, tHIDMouseInstance::ui8USBConfigured, and USBDHIDTerm().
void * USBDHIDMouseSetCBData | ( | void * | pvMouseDevice, |
void * | pvCBData | ||
) |
Sets the client-specific pointer parameter for the mouse callback.
pvMouseDevice | is the pointer to the mouse device instance structure. |
pvCBData | is the pointer that client wishes to be provided on each event sent to the mouse callback function. |
The client uses this function to change the callback pointer passed in the first parameter on all callbacks to the pfnCallback function passed on USBDHIDMouseInit().
If a client wants to make runtime changes in the callback pointer, it must ensure that the pvMouseDevice structure passed to USBDHIDMouseInit() resides in RAM. If this structure is in flash, callback data changes are not possible.
References tUSBDHIDMouseDevice::pvCBData.
uint32_t USBDHIDMouseStateChange | ( | void * | pvMouseDevice, |
int8_t | i8DeltaX, | ||
int8_t | i8DeltaY, | ||
uint8_t | ui8Buttons | ||
) |
Reports a mouse state change, pointer movement or button press, to the USB host.
pvMouseDevice | is the pointer to the mouse device instance structure. |
i8DeltaX | is the relative horizontal pointer movement that the application wishes to report. Valid values are in the range [-127, 127] with positive values indicating movement to the right. |
i8DeltaY | is the relative vertical pointer movement that the application wishes to report. Valid values are in the range [-127, 127] with positive values indicating downward movement. |
ui8Buttons | is a bit mask indicating which (if any) of the three mouse buttons is pressed. Valid values are logical OR combinations of MOUSE_REPORT_BUTTON_1, MOUSE_REPORT_BUTTON_2 and MOUSE_REPORT_BUTTON_3. |
This function is called to report changes in the mouse state to the USB host. These changes can be movement of the pointer, reported relative to its previous position, or changes in the states of up to 3 buttons that the mouse may support. The return code indicates whether or not the mouse report could be sent to the host. In cases where a previous report is still being transmitted, MOUSE_ERR_TX_ERROR is returned and the state change is ignored.
References eHIDMouseStateSend, HID_REPORT_BUTTONS, HID_REPORT_X, HID_REPORT_Y, tHIDMouseInstance::iMouseState, MOUSE_ERR_NOT_CONFIGURED, MOUSE_ERR_TX_ERROR, MOUSE_REPORT_SIZE, MOUSE_SUCCESS, tHIDMouseInstance::pui8Report, tHIDMouseInstance::sHIDDevice, tUSBDHIDMouseDevice::sPrivateData, tHIDMouseInstance::ui8USBConfigured, USBDHIDReportWrite(), and USBDHIDTxPacketAvailable().
void USBDHIDMousePowerStatusSet | ( | void * | pvMouseDevice, |
uint8_t | ui8Power | ||
) |
Reports the device power status (bus- or self-powered) to the USB library.
pvMouseDevice | is the pointer to the mouse device instance structure. |
ui8Power | indicates the current power status, either USB_STATUS_SELF_PWR or USB_STATUS_BUS_PWR. |
Applications which support switching between bus- or self-powered operation should call this function whenever the power source changes to indicate the current power status to the USB library. This information is required by the USB library to allow correct responses to be provided when the host requests status from the device.
References tHIDMouseInstance::sHIDDevice, tUSBDHIDMouseDevice::sPrivateData, and USBDHIDPowerStatusSet().
bool USBDHIDMouseRemoteWakeupRequest | ( | void * | pvMouseDevice | ) |
Requests a remote wake up to resume communication when in suspended state.
pvMouseDevice | is the pointer to the mouse device instance structure. |
When the bus is suspended, an application which supports remote wake up (advertised to the host via the configuration descriptor) may call this function to initiate remote wake up signaling to the host. If the remote wake up feature has not been disabled by the host, this causes the bus to resume operation within 20mS. If the host has disabled remote wake up, false is returned to indicate that the wake up request was not successful.
References tHIDMouseInstance::sHIDDevice, tUSBDHIDMouseDevice::sPrivateData, and USBDHIDRemoteWakeupRequest().
uint8_t g_pui8MouseDescriptor[] |
Referenced by USBDHIDMouseInit().
uint8_t g_pui8HIDInterface[HIDINTERFACE_SIZE] |
const uint8_t g_pui8HIDInEndpoint[HIDINENDPOINT_SIZE] |
const tConfigSection g_sHIDConfigSection |
const tConfigSection g_sHIDInterfaceSection |
const tConfigSection g_sHIDInEndpointSection |
tConfigSection g_sHIDDescriptorSection |
const tConfigSection* g_psHIDSections[] |
tConfigHeader g_sHIDConfigHeader |
const tConfigHeader* const g_ppsHIDConfigDescriptors[] |