uDMA driver implementation for MSP432E4.
============================================================================
This driver is intended for use only by TI-RTOS drivers that use the uDMA peripheral (e.g., SPI). This driver is mainly used for management of the control table base address of the UDMA peripheral, and to create the DMA error Hwi.
The application should only define the memory for the control table and set up the UDMAMSP432E4_HWAttrs and UDMAMSP432E4_Config structures.
The UDMAMSP432E4 header file should be included in an application as follows:
#include <stdbool.h>
#include <stdint.h>
#include <ti/drivers/dpl/HwiP.h>
Go to the source code of this file.
Data Structures | |
struct | UDMAMSP432E4_HWAttrs |
UDMAMSP432E4 Hardware attributes. More... | |
struct | UDMAMSP432E4_Config |
UDMAMSP432E4 Global configuration. More... | |
struct | UDMAMSP432E4_Object |
UDMAMSP432E4 object. More... | |
Typedefs | |
typedef void(* | UDMAMSP432E4_ErrorFxn) (uintptr_t arg) |
UDMA error function pointer. More... | |
typedef struct UDMAMSP432E4_HWAttrs | UDMAMSP432E4_HWAttrs |
UDMAMSP432E4 Hardware attributes. More... | |
typedef struct UDMAMSP432E4_Config | UDMAMSP432E4_Config |
UDMAMSP432E4 Global configuration. More... | |
typedef struct UDMAMSP432E4_Config * | UDMAMSP432E4_Handle |
A handle that is returned from a UDMAMSP432E4_open() call. More... | |
typedef struct UDMAMSP432E4_Object | UDMAMSP432E4_Object |
UDMAMSP432E4 object. More... | |
Functions | |
void | UDMAMSP432E4_close (UDMAMSP432E4_Handle handle) |
Function to close the DMA driver. More... | |
void | UDMAMSP432E4_init () |
Function to initialize the MSP432E4 DMA driver. More... | |
UDMAMSP432E4_Handle | UDMAMSP432E4_open () |
Function to initialize the MSP432E4 DMA peripheral. More... | |
typedef void(* UDMAMSP432E4_ErrorFxn) (uintptr_t arg) |
UDMA error function pointer.
typedef struct UDMAMSP432E4_HWAttrs UDMAMSP432E4_HWAttrs |
UDMAMSP432E4 Hardware attributes.
This structure contains the base address of the uDMA control table, and uDMA error interrupt attributes.
The control table is used by the uDMA controller to store channel control structures. The control table can be located anywhere in system memory, but must be contiguous and aligned on a 1024-byte boundary.
dmaErrorFxn is the uDMA peripheral's error interrupt handler.
intPriority is priority of the uDMA peripheral's error interrupt, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. If the driver uses the ti.dpl interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create().
A sample structure is shown below:
typedef struct UDMAMSP432E4_Config UDMAMSP432E4_Config |
UDMAMSP432E4 Global configuration.
The UDMAMSP432E4_Config structure contains pointers used by the UDMAMSP432E4 driver.
This structure needs to be defined before calling UDMAMSP432E4_init() and it must not be changed thereafter.
typedef struct UDMAMSP432E4_Config* UDMAMSP432E4_Handle |
A handle that is returned from a UDMAMSP432E4_open() call.
typedef struct UDMAMSP432E4_Object UDMAMSP432E4_Object |
UDMAMSP432E4 object.
The application must not access any member variables of this structure!
void UDMAMSP432E4_close | ( | UDMAMSP432E4_Handle | handle | ) |
Function to close the DMA driver.
Close a DMA handle returned from UDMAMSP432E4_open().
handle | A UDMAMSP432E4_Handle returned from UDMAMSP432E4_open() |
void UDMAMSP432E4_init | ( | ) |
Function to initialize the MSP432E4 DMA driver.
The function should be called prior to opening the DMA driver.
UDMAMSP432E4_Handle UDMAMSP432E4_open | ( | ) |
Function to initialize the MSP432E4 DMA peripheral.
UDMAMSP432E4_open() can be called multiple times. *