Network Services API
2.00.00.16
|
Controls standard stack/interface options and capabilities. More...
Data Structures | |
struct | _SlNetIf_Config_t |
SlNetIf_Config_t structure contains all the function callbacks that are expected to be filled by the relevant network stack interface Each interface has different capabilities, so not all the API's must be supported therefore an API's can be defined as: . More... | |
struct | _SlNetIf_t |
The SlNetIf_t structure holds the configuration of the interface Its ID, name, flags and the configuration list - SlNetIf_Config_t. More... | |
Typedefs | |
typedef struct _SlNetIf_Config_t | SlNetIf_Config_t |
SlNetIf_Config_t structure contains all the function callbacks that are expected to be filled by the relevant network stack interface Each interface has different capabilities, so not all the API's must be supported therefore an API's can be defined as: . More... | |
typedef struct _SlNetIf_t | SlNetIf_t |
The SlNetIf_t structure holds the configuration of the interface Its ID, name, flags and the configuration list - SlNetIf_Config_t. More... | |
Enumerations | |
enum | SlNetIfState_e { SLNETIF_STATE_DISABLE = 0, SLNETIF_STATE_ENABLE = 1 } |
Interface state bit pool to be used in set interface state function. More... | |
enum | SlNetIfAddressType_e { SLNETIF_IPV4_ADDR = 0, SLNETIF_IPV6_ADDR_LOCAL = 1, SLNETIF_IPV6_ADDR_GLOBAL = 2 } |
Address type enum to be used in get ip address function. More... | |
Functions | |
int32_t | SlNetIf_init (int32_t flags) |
Initialize the SlNetIf module. More... | |
int32_t | SlNetIf_add (uint16_t ifID, char *ifName, const SlNetIf_Config_t *ifConf, uint8_t priority) |
Adding new interface. More... | |
SlNetIf_t * | SlNetIf_getIfByID (uint16_t ifID) |
Get interface configuration from interface ID. More... | |
SlNetIf_t * | SlNetIf_queryIf (uint32_t ifBitmap, uint32_t queryBitmap) |
Get highest priority interface configuration using interface bitmap. More... | |
const char * | SlNetIf_getNameByID (uint16_t ifID) |
Get interface Name from interface ID. More... | |
int32_t | SlNetIf_getIDByName (char *ifName) |
Get interface ID from interface name. More... | |
int32_t | SlNetIf_getPriority (uint16_t ifID) |
Get interface priority. More... | |
int32_t | SlNetIf_setPriority (uint16_t ifID, uint8_t priority) |
Set interface priority. More... | |
int32_t | SlNetIf_setState (uint16_t ifID, SlNetIfState_e ifState) |
Set interface state. More... | |
int32_t | SlNetIf_getState (uint16_t ifID) |
Get interface state. More... | |
int32_t | SlNetIf_getConnectionStatus (uint16_t ifID) |
Get interface connection status. More... | |
int32_t | SlNetIf_getIPAddr (uint16_t ifID, SlNetIfAddressType_e addrType, uint16_t *addrConfig, uint32_t *ipAddr) |
Get IP Address of specific interface. More... | |
int32_t | SlNetIf_loadSecObj (uint16_t objType, char *objName, int16_t objNameLen, uint8_t *objBuff, int16_t objBuffLen, uint32_t ifBitmap) |
Load secured buffer to the network stack. More... | |
Controls standard stack/interface options and capabilities.
#define SLNETIF_ID_1 (1 << 0) |
#define SLNETIF_ID_2 (1 << 1) |
#define SLNETIF_ID_3 (1 << 2) |
#define SLNETIF_ID_4 (1 << 3) |
#define SLNETIF_ID_5 (1 << 4) |
#define SLNETIF_ID_6 (1 << 5) |
#define SLNETIF_ID_7 (1 << 6) |
#define SLNETIF_ID_8 (1 << 7) |
#define SLNETIF_ID_9 (1 << 8) |
#define SLNETIF_ID_10 (1 << 9) |
#define SLNETIF_ID_11 (1 << 10) |
#define SLNETIF_ID_12 (1 << 11) |
#define SLNETIF_ID_13 (1 << 12) |
#define SLNETIF_ID_14 (1 << 13) |
#define SLNETIF_ID_15 (1 << 14) |
#define SLNETIF_ID_16 (1 << 15) |
#define SLNETIF_MAX_IF (16) |
#define ONLY_ONE_BIT_IS_SET | ( | x | ) | (((x > 0) && ((x & (x - 1)) == 0))?true:false) |
#define SLNETIF_STATUS_DISCONNECTED (0) |
#define SLNETIF_STATUS_CONNECTED (1) |
#define SLNETIF_ADDR_CFG_UNKNOWN (0) |
#define SLNETIF_ADDR_CFG_DHCP (1) |
#define SLNETIF_ADDR_CFG_DHCP_LLA (2) |
#define SLNETIF_ADDR_CFG_STATIC (4) |
#define SLNETIF_ADDR_CFG_STATELESS (5) |
#define SLNETIF_ADDR_CFG_STATEFUL (6) |
#define SLNETIF_SEC_OBJ_TYPE_RSA_PRIVATE_KEY (1) |
#define SLNETIF_SEC_OBJ_TYPE_CERTIFICATE (2) |
#define SLNETIF_SEC_OBJ_TYPE_DH_KEY (3) |
#define SLNETIF_QUERY_IF_STATE_BIT (1 << 0) |
#define SLNETIF_QUERY_IF_CONNECTION_STATUS_BIT (1 << 1) |
#define SLNETIF_QUERY_IF_ALLOW_PARTIAL_MATCH_BIT (1 << 2) |
typedef struct _SlNetIf_Config_t SlNetIf_Config_t |
SlNetIf_Config_t structure contains all the function callbacks that are expected to be filled by the relevant network stack interface
Each interface has different capabilities, so not all the API's must be supported therefore an API's can be defined as:
.
typedef struct _SlNetIf_t SlNetIf_t |
The SlNetIf_t structure holds the configuration of the interface Its ID, name, flags and the configuration list - SlNetIf_Config_t.
enum SlNetIfState_e |
enum SlNetIfAddressType_e |
int32_t SlNetIf_init | ( | int32_t | flags | ) |
Initialize the SlNetIf module.
The SlNetIf_init function Initialize the SlNetIf module.
[in] | flags | For future usage, The value 0 may be used in order to run the default flags |
int32_t SlNetIf_add | ( | uint16_t | ifID, |
char * | ifName, | ||
const SlNetIf_Config_t * | ifConf, | ||
uint8_t | priority | ||
) |
Adding new interface.
The SlNetIf_add function allows the application to add specific interfaces with their priorities and function list.
This function gives full control to the application on the interfaces.
[in] | ifID | Specifies the interface which needs to be added. The values of the interface identifier is defined with the prefix SLNETIF_ID_ which defined in slnetif.h |
[in] | ifName | Specifies the name of the interface, Note: Can be set to NULL, but when set to NULL cannot be used with SlNetIf_getIDByName |
[in] | ifConf | Specifies the function list for the interface |
[in] | priority | Specifies the priority needs to be set (In ascending order). Note: maximum priority is 15 |
SlNetIf_t* SlNetIf_getIfByID | ( | uint16_t | ifID | ) |
Get interface configuration from interface ID.
The SlNetIf_getIfByID function retrieves the configuration of the requested interface.
[in] | ifID | Specifies the interface which its configuration needs to be retrieved. The values of the interface identifier is defined with the prefix SLNETIF_ID_ which defined in slnetif.h |
SlNetIf_t* SlNetIf_queryIf | ( | uint32_t | ifBitmap, |
uint32_t | queryBitmap | ||
) |
Get highest priority interface configuration using interface bitmap.
The SlNetIf_getIfByID function retrieves highest priority interface configuration that can be found in the interface bitmap, or the highest exists when ifBitmap is zero.
[in,out] | ifBitmap | Specifies the interface that needs to be checked according to the queryBitmap and return the interface with the highest priority. The values of the interface Bitmap is a combination of the interface identifiers defined with the prefix SLNETIF_ID_ which defined in slnetif.h Note: Zero is not a valid parameter, an error will be returned |
[in] | queryBitmap | Specifies the additional criterias for the query that will be use along the interface priority and interface ID. queryBitmap bits:
|
const char* SlNetIf_getNameByID | ( | uint16_t | ifID | ) |
Get interface Name from interface ID.
The SlNetIf_getNameByID function retrieves the name of the requested interface.
[in] | ifID | Specifies the interface which its name needs to be retrieved. The values of the interface identifier is defined with the prefix SLNETIF_ID_ which defined in slnetif.h |
int32_t SlNetIf_getIDByName | ( | char * | ifName | ) |
Get interface ID from interface name.
The SlNetIf_getIDByName function retrieves the interface identifier of the requested interface name.
[in] | ifName | Specifies the interface which its interface identifier needs to be retrieved. |
int32_t SlNetIf_getPriority | ( | uint16_t | ifID | ) |
Get interface priority.
The SlNetIf_getPriority function retrieves the priority of the interface.
[in] | ifID | Specifies the interface which its priority needs to be retrieved. The values of the interface identifier is defined with the prefix SLNETIF_ID_ which defined in slnetif.h |
int32_t SlNetIf_setPriority | ( | uint16_t | ifID, |
uint8_t | priority | ||
) |
Set interface priority.
The SlNetIf_setPriority function sets new priority to the requested interface.
[in] | ifID | Specifies the interface which its priority needs to be changed. The values of the interface identifier is defined with the prefix SLNETIF_ID_ which defined in slnetif.h |
[in] | priority | Specifies the priority needs to be set. (In ascending order) Note: maximum priority is 15 |
int32_t SlNetIf_setState | ( | uint16_t | ifID, |
SlNetIfState_e | ifState | ||
) |
Set interface state.
The SlNetIf_setState function sets the state of the interface (Enable or Disable).
[in] | ifID | Specifies the interface which its state needs to be changed. The values of the interface identifier is defined with the prefix SLNETIF_ID_ which defined in slnetif.h |
[in] | ifState | Specifies the interface state. The values of the interface state are defined with the prefix SLNETIF_INTERFACE_ which defined in slnetif.h |
int32_t SlNetIf_getState | ( | uint16_t | ifID | ) |
Get interface state.
The SlNetIf_getState function gets the state of the interface (Enable or Disable).
[in] | ifID | Specifies the interface which its state needs to be retrieved. The values of the interface identifier is defined with the prefix SLNETIF_ID_ which defined in slnetif.h |
int32_t SlNetIf_getConnectionStatus | ( | uint16_t | ifID | ) |
Get interface connection status.
The SlNetIf_getConnectionStatus function gets the connection status of the interface (connected Or disconnected).
[in] | ifID | Specifies the interface which its connection status needs to be retrieved. The values of the interface identifier is defined with the prefix SLNETIF_ID_ which defined in slnetif.h |
int32_t SlNetIf_getIPAddr | ( | uint16_t | ifID, |
SlNetIfAddressType_e | addrType, | ||
uint16_t * | addrConfig, | ||
uint32_t * | ipAddr | ||
) |
Get IP Address of specific interface.
The SlNetIf_getIPAddr function retrieve the IP address of a specific interface according to the Address Type, IPv4, IPv6 LOCAL or IPv6 GLOBAL.
[in] | ifID | Specifies the interface which its connection state needs to be retrieved. The values of the interface identifier is defined with the prefix SLNETIF_ID_ which defined in slnetif.h |
[in] | addrType | Address type:
|
[out] | addrConfig | Address config:
|
[out] | ipAddr | IP Address according to the Address Type |
int32_t SlNetIf_loadSecObj | ( | uint16_t | objType, |
char * | objName, | ||
int16_t | objNameLen, | ||
uint8_t * | objBuff, | ||
int16_t | objBuffLen, | ||
uint32_t | ifBitmap | ||
) |
Load secured buffer to the network stack.
The SlNetSock_secLoadObj function loads buffer/files into the inputted network stack for future usage of the socket SSL/TLS connection. This option is relevant for network stacks with file system and also for network stacks that lack file system that can store the secured files.
[in] | objType | Specifies the security object type which could be one of the following:
|
[in] | objName | Specifies the name/input identifier of the secured buffer loaded for file systems - this can be the file name for plain text buffer loading this can be the name of the object |
[in] | objNameLen | Specifies the buffer name length to be loaded. |
[in] | objBuff | Specifies the pointer to the secured buffer to be loaded. |
[in] | objBuffLen | Specifies the buffer length to be loaded. |
[in] | ifBitmap | Specifies the interfaces which the security objects needs to be added to. The values of the interface identifiers is defined with the prefix SLNETIF_ID_ which defined in slnetif.h |