TI BLE Stack API Documentation
2.03.08
|
LE Enhanced Connection Complete Event. More...
#include <hci.h>
Public Attributes | |
osal_event_hdr_t | hdr |
osal event header | |
uint8 | BLEEventCode |
BLE Event Code. | |
uint8 | status |
status of event | |
uint16 | connectionHandle |
connection handle | |
uint8 | role |
role of connection | |
uint8 | peerAddrType |
peer address type | |
uint8 | peerAddr [6] |
peer address | |
uint16 | connInterval |
connection interval | |
uint16 | connLatency |
connection latency | |
uint16 | connTimeout |
connection supervision timeout | |
uint8 | clockAccuracy |
connection clock accuracy | |
uint8 | localRPA [6] |
local resolvable private address | |
uint8 | peerRPA [6] |
peer resolvable private address | |
LE Enhanced Connection Complete Event.