TI BLE Stack API Documentation
2.03.08
|
This module implements the Host Controller Interface. For a detailed usage section describing how to send these commands and receive events, see the HCI Section of the User's Guide. More...
Modules | |
HCI Function Maps | |
HCI Constants | |
HCI Events | |
Files | |
file | hci.h |
HCI layer interface. | |
Functions | |
uint8 | HCI_ValidConnTimeParams (uint16 connIntervalMin, uint16 connIntervalMax, uint16 connLatency, uint16 connTimeout) |
This API is used to check that the connection time parameter ranges are valid, and that the connection time parameter combination is valid. It also checks if the min/max CI range is valid. More... | |
void | HCI_TestAppTaskRegister (uint8 taskID) |
HCI vendor specific registration for HCI Test Application. More... | |
void | HCI_GAPTaskRegister (uint8 taskID) |
HCI vendor specific registration for Host GAP. More... | |
void | HCI_L2CAPTaskRegister (uint8 taskID) |
HCI vendor specific registration for Host L2CAP. More... | |
void | HCI_SMPTaskRegister (uint8 taskID) |
HCI vendor specific registration for Host SMP. More... | |
void | HCI_ExtTaskRegister (uint8 taskID) |
HCI vendor specific registration for Host extended commands. More... | |
hciStatus_t | HCI_SendDataPkt (uint16 connHandle, uint8 pbFlag, uint16 pktLen, uint8 *pData) |
This API is used to send a ACL data packet over a connection. More... | |
hciStatus_t | HCI_DisconnectCmd (uint16 connHandle, uint8 reason) |
This BT API is used to terminate a connection. More... | |
hciStatus_t | HCI_ReadRemoteVersionInfoCmd (uint16 connHandle) |
This BT API is used to request version information from the the remote device in a connection. More... | |
hciStatus_t | HCI_SetEventMaskCmd (uint8 *pMask) |
This BT API is used to set the HCI event mask, which is used to determine which events are supported. More... | |
hciStatus_t | HCI_SetEventMaskPage2Cmd (uint8 *pMask) |
This BT API is used to set the HCI event mask page 2, which is used to determine which events are supported. More... | |
hciStatus_t | HCI_ResetCmd (void) |
Reset the Link Layer. More... | |
hciStatus_t | HCI_ReadTransmitPowerLevelCmd (uint16 connHandle, uint8 txPwrType) |
Read the transmit power level. More... | |
hciStatus_t | HCI_SetControllerToHostFlowCtrlCmd (uint8 flowControlEnable) |
This BT API is used by the Host to turn flow control on or off for data sent from the Controller to Host. Related Events: HCI_CommandCompleteEvent. More... | |
hciStatus_t | HCI_HostBufferSizeCmd (uint16 hostAclPktLen, uint8 hostSyncPktLen, uint16 hostTotalNumAclPkts, uint16 hostTotalNumSyncPkts) |
This BT API is used by the Host to notify the Controller of the maximum size ACL buffer size the Controller can send to the Host. More... | |
hciStatus_t | HCI_HostNumCompletedPktCmd (uint8 numHandles, uint16 *connHandles, uint16 *numCompletedPkts) |
This BT API is used by the Host to notify the Controller of the number of HCI data packets that have been completed for each connection handle since this command was previously sent to the controller. More... | |
hciStatus_t | HCI_ReadAuthPayloadTimeoutCmd (uint16 connHandle, uint16 *aptoValue) |
Read the connection's Authenticated Payload Timeout value. More... | |
hciStatus_t | HCI_WriteAuthPayloadTimeoutCmd (uint16 connHandle, uint16 aptoValue) |
Used to write the connection's Authenticated Payload Timeout value. More... | |
hciStatus_t | HCI_ReadLocalVersionInfoCmd (void) |
Read the local version information. More... | |
hciStatus_t | HCI_ReadLocalSupportedCommandsCmd (void) |
Read the locally supported commands. More... | |
hciStatus_t | HCI_ReadLocalSupportedFeaturesCmd (void) |
Read the locally supported features. More... | |
hciStatus_t | HCI_ReadBDADDRCmd (void) |
Read this device's BLE address (BDADDR). More... | |
hciStatus_t | HCI_ReadRssiCmd (uint16 connHandle) |
Read RSSI of last packet. More... | |
hciStatus_t | HCI_LE_SetEventMaskCmd (uint8 *pEventMask) |
This LE API is used to set the HCI LE event mask, which is used to determine which LE events are supported. More... | |
hciStatus_t | HCI_LE_ReadBufSizeCmd (void) |
This LE API is used by the Host to determine the maximum ACL data packet size allowed by the Controller. More... | |
hciStatus_t | HCI_LE_ReadLocalSupportedFeaturesCmd (void) |
Read the LE locally supported features. More... | |
hciStatus_t | HCI_LE_SetRandomAddressCmd (uint8 *pRandAddr) |
Set this device's Random address. More... | |
hciStatus_t | HCI_LE_SetAdvParamCmd (uint16 advIntervalMin, uint16 advIntervalMax, uint8 advType, uint8 ownAddrType, uint8 directAddrType, uint8 *directAddr, uint8 advChannelMap, uint8 advFilterPolicy) |
Set the Advertising parameters. More... | |
hciStatus_t | HCI_LE_SetAdvDataCmd (uint8 dataLen, uint8 *pData) |
Set the Advertising data. More... | |
hciStatus_t | HCI_LE_SetScanRspDataCmd (uint8 dataLen, uint8 *pData) |
Set the Advertising Scan Response data. More... | |
hciStatus_t | HCI_LE_SetAdvEnableCmd (uint8 advEnable) |
Turn Advertising on or off. More... | |
hciStatus_t | HCI_LE_ReadAdvChanTxPowerCmd (void) |
Read transmit power when Advertising. More... | |
hciStatus_t | HCI_LE_SetScanParamCmd (uint8 scanType, uint16 scanInterval, uint16 scanWindow, uint8 ownAddrType, uint8 filterPolicy) |
Set the Scan parameters. More... | |
hciStatus_t | HCI_LE_SetScanEnableCmd (uint8 scanEnable, uint8 filterDuplicates) |
Turn Scanning on or off. More... | |
hciStatus_t | HCI_LE_CreateConnCmd (uint16 scanInterval, uint16 scanWindow, uint8 initFilterPolicy, uint8 addrTypePeer, uint8 *peerAddr, uint8 ownAddrType, uint16 connIntervalMin, uint16 connIntervalMax, uint16 connLatency, uint16 connTimeout, uint16 minLen, uint16 maxLen) |
Create a connection. More... | |
hciStatus_t | HCI_LE_CreateConnCancelCmd (void) |
Cancel connection. More... | |
hciStatus_t | HCI_LE_ReadWhiteListSizeCmd (void) |
Read the white list. More... | |
hciStatus_t | HCI_LE_ClearWhiteListCmd (void) |
Clear the white list. More... | |
hciStatus_t | HCI_LE_AddWhiteListCmd (uint8 addrType, uint8 *devAddr) |
Add a white list entry. More... | |
hciStatus_t | HCI_LE_RemoveWhiteListCmd (uint8 addrType, uint8 *devAddr) |
Remove a white list entry. More... | |
hciStatus_t | HCI_LE_ConnUpdateCmd (uint16 connHandle, uint16 connIntervalMin, uint16 connIntervalMax, uint16 connLatency, uint16 connTimeout, uint16 minLen, uint16 maxLen) |
Update the connection parameters. More... | |
hciStatus_t | HCI_LE_SetHostChanClassificationCmd (uint8 *chanMap) |
Update the current data channel map. More... | |
hciStatus_t | HCI_LE_ReadChannelMapCmd (uint16 connHandle) |
Read a connection's data channel map. More... | |
hciStatus_t | HCI_LE_ReadRemoteUsedFeaturesCmd (uint16 connHandle) |
Read the remote device's used features. More... | |
hciStatus_t | HCI_LE_EncryptCmd (uint8 *key, uint8 *plainText) |
Perform an encryption using AES128. More... | |
hciStatus_t | HCI_LE_RandCmd (void) |
Generate a random number. More... | |
hciStatus_t | HCI_LE_StartEncyptCmd (uint16 connHandle, uint8 *random, uint8 *encDiv, uint8 *ltk) |
Start encryption in a connection. More... | |
hciStatus_t | HCI_LE_LtkReqReplyCmd (uint16 connHandle, uint8 *ltk) |
This LE API is used by the Host to send to the Controller a positive LTK reply. More... | |
hciStatus_t | HCI_LE_LtkReqNegReplyCmd (uint16 connHandle) |
This LE API is used by the Host to send to the Controller a negative LTK reply. More... | |
hciStatus_t | HCI_LE_ReadSupportedStatesCmd (void) |
Read the Controller's supported states. More... | |
hciStatus_t | HCI_LE_ReceiverTestCmd (uint8 rxChan) |
Start the receiver Direct Test Mode test. More... | |
hciStatus_t | HCI_LE_TransmitterTestCmd (uint8 txChan, uint8 dataLen, uint8 pktPayload) |
This LE API is used to start the transmit Direct Test Mode test. More... | |
hciStatus_t | HCI_LE_TestEndCmd (void) |
End the Direct Test Mode test. More... | |
hciStatus_t | HCI_LE_RemoteConnParamReqReplyCmd (uint16 connHandle, uint16 connIntervalMin, uint16 connIntervalMax, uint16 connLatency, uint16 connTimeout, uint16 minLen, uint16 maxLen) |
This LE API is used to positively reply to the HCI LE Remote Connection Parameter Request event from the Controller. This command indicates that the Host has accepted the remote device's request to change connection parameters. More... | |
hciStatus_t | HCI_LE_RemoteConnParamReqNegReplyCmd (uint16 connHandle, uint8 reason) |
Negatively reply to the Conneciton Parameter Update Request. More... | |
hciStatus_t | HCI_LE_SetDataLenCmd (uint16 connHandle, uint16 txOctets, uint16 txTime) |
Set Data Length. More... | |
hciStatus_t | HCI_LE_ReadSuggestedDefaultDataLenCmd (void) |
Read Suggested Default Data Length. More... | |
hciStatus_t | HCI_LE_WriteSuggestedDefaultDataLenCmd (uint16 txOctets, uint16 txTime) |
Write Suggested Default Data Length. More... | |
hciStatus_t | HCI_LE_ReadMaxDataLenCmd (void) |
Read max data length. More... | |
hciStatus_t | HCI_LE_AddDeviceToResolvingListCmd (uint8 peerIdAddrType, uint8 *peerIdAddr, uint8 *peerIRK, uint8 *localIRK) |
Add a device to the resolving list. More... | |
hciStatus_t | HCI_LE_RemoveDeviceFromResolvingListCmd (uint8 peerIdAddrType, uint8 *peerIdAddr) |
Remove a device from the whitelist. More... | |
hciStatus_t | HCI_LE_ClearResolvingListCmd (void) |
Remove all devices from the whitelist. More... | |
hciStatus_t | HCI_LE_ReadResolvingListSizeCmd (void) |
Read Resolving List Size. More... | |
hciStatus_t | HCI_LE_ReadPeerResolvableAddressCmd (uint8 peerIdAddrType, uint8 *peerIdAddr) |
Read the Peer Resolvable Address. More... | |
hciStatus_t | HCI_LE_ReadLocalResolvableAddressCmd (uint8 localIdAddrType, uint8 *localIdAddr) |
Read Local Resolvable Private Address. More... | |
hciStatus_t | HCI_LE_SetAddressResolutionEnableCmd (uint8 addrResolutionEnable) |
Disable / Enable Address Resolution. More... | |
hciStatus_t | HCI_LE_SetResolvablePrivateAddressTimeoutCmd (uint16 rpaTimeout) |
Set Resolvable Private Address Timeout. More... | |
hciStatus_t | HCI_LE_ReadLocalP256PublicKeyCmd (void) |
Read local P-256 Public Key. More... | |
hciStatus_t | HCI_LE_GenerateDHKeyCmd (uint8 *publicKey) |
Generate Diffie-Hellman Key. More... | |
hciStatus_t | HCI_LE_ReadPhyCmd (uint16 connHandle) |
Read the current transmitter and receiver PHY. More... | |
hciStatus_t | HCI_LE_SetDefaultPhyCmd (uint8 allPhys, uint8 txPhy, uint8 rxPhy) |
Set Default PHY. More... | |
hciStatus_t | HCI_LE_SetPhyCmd (uint16 connHandle, uint8 allPhys, uint8 txPhy, uint8 rxPhy) |
This LE API is used to request a change to the transmitter and receiver PHY for a connection. More... | |
hciStatus_t | HCI_LE_EnhancedRxTestCmd (uint8 rxChan, uint8 rxPhy, uint8 modIndex) |
Start Enhanced RX Test. More... | |
hciStatus_t | HCI_LE_EnhancedTxTestCmd (uint8 txChan, uint8 payloadLen, uint8 payloadType, uint8 txPhy) |
Start Enhanced TX Test. More... | |
hciStatus_t | HCI_EXT_SetRxGainCmd (uint8 rxGain) |
Set the receiver gain. More... | |
hciStatus_t | HCI_EXT_SetTxPowerCmd (uint8 txPower) |
Set the transmit power. More... | |
hciStatus_t | HCI_EXT_OnePktPerEvtCmd (uint8 control) |
This HCI Extension API is used to set whether a connection will be limited to one packet per event. More... | |
hciStatus_t | HCI_EXT_ClkDivOnHaltCmd (uint8 control) |
Set whether the system clock will be divided when the MCU is halted. More... | |
hciStatus_t | HCI_EXT_DeclareNvUsageCmd (uint8 mode) |
This HCI Extension API is used to indicate to the Controller whether or not the Host will be using the NV memory during BLE operations. More... | |
hciStatus_t | HCI_EXT_DecryptCmd (uint8 *key, uint8 *encText) |
This HCI Extension API is used to decrypt encrypted data using AES128. More... | |
hciStatus_t | HCI_EXT_SetLocalSupportedFeaturesCmd (uint8 *localFeatures) |
This HCI Extension API is used to write this device's supported features. More... | |
hciStatus_t | HCI_EXT_SetFastTxResponseTimeCmd (uint8 control) |
This HCI Extension API is used to set whether transmit data is sent as soon as possible even when slave latency is used. More... | |
hciStatus_t | HCI_EXT_SetSlaveLatencyOverrideCmd (uint8 control) |
This HCI Extension API is used to to enable or disable suspending slave latency. More... | |
hciStatus_t | HCI_EXT_ModemTestTxCmd (uint8 cwMode, uint8 txChan) |
This API is used start a continuous transmitter modem test, using either a modulated or unmodulated carrier wave tone, at the frequency that corresponds to the specified RF channel. Use HCI_EXT_EndModemTest command to end the test. More... | |
hciStatus_t | HCI_EXT_ModemHopTestTxCmd (void) |
Start Modem Hop Tx Test. More... | |
hciStatus_t | HCI_EXT_ModemTestRxCmd (uint8 rxChan) |
Start Modem Hop RX Test. More... | |
hciStatus_t | HCI_EXT_EndModemTestCmd (void) |
This API is used to shutdown a modem test. A complete Controller reset will take place. More... | |
hciStatus_t | HCI_EXT_SetBDADDRCmd (uint8 *bdAddr) |
This API is used to set this device's BLE address (BDADDR). More... | |
hciStatus_t | HCI_EXT_SetSCACmd (uint16 scaInPPM) |
This API is used to set this device's Sleep Clock Accuracy. More... | |
hciStatus_t | HCI_EXT_EnablePTMCmd (void) |
This HCI Extension API is used to enable Production Test Mode. More... | |
hciStatus_t | HCI_EXT_SetFreqTuneCmd (uint8 step) |
This HCI Extension API is used to set the frequency tuning up or down. Setting the mode up/down decreases/increases the amount of capacitance on the external crystal oscillator. More... | |
hciStatus_t | HCI_EXT_SaveFreqTuneCmd (void) |
This HCI Extension API is used to save the frequency tuning value to flash. More... | |
hciStatus_t | HCI_EXT_SetMaxDtmTxPowerCmd (uint8 txPower) |
This HCI Extension API is used to set the maximum transmit output power for Direct Test Mode. More... | |
hciStatus_t | HCI_EXT_MapPmIoPortCmd (uint8 ioPort, uint8 ioPin) |
This HCI Extension API is used to configure and map a CC254x I/O Port as a General Purpose I/O (GPIO) output signal that reflects the Power Management (PM) state of the CC254x device. The GPIO output will be High on Wake, and Low upon entering Sleep. This feature can be disabled by specifying HCI_EXT_PM_IO_PORT_NONE for the ioPort (ioPin is then ignored). The system default value upon hardware reset is disabled. This command can be used to control an external DC-DC Converter (its actual intent) such has the TI TPS62730 (or any similar converter that works the same way). This command should be used with extreme care as it will override how the Port/Pin was previously configured! This includes the mapping of Port 0 pins to 32kHz clock output, Analog I/O, UART, Timers; Port 1 pins to Observables, Digital Regulator status, UART, Timers; Port 2 pins to an external 32kHz XOSC. The selected Port/Pin will be configured as an output GPIO with interrupts masked. Careless use can result in a reconfiguration that could disrupt the system. It is therefore the user's responsibility to ensure the selected Port/Pin does not cause any conflicts in the system. More... | |
hciStatus_t | HCI_EXT_DisconnectImmedCmd (uint16 connHandle) |
This HCI Extension API is used to disconnect the connection immediately. More... | |
hciStatus_t | HCI_EXT_PacketErrorRateCmd (uint16 connHandle, uint8 command) |
This function is used to Reset or Read the Packet Error Rate counters for a connection. More... | |
hciStatus_t | HCI_EXT_PERbyChanCmd (uint16 connHandle, perByChan_t *perByChan) |
This HCI Extension API is used to start or end Packet Error Rate by Channel counter accumulation for a connection. If the pointer is not NULL, it is assumed there is sufficient memory for the PER data, per the type perByChan_t. If NULL, then the operation is considered disabled. More... | |
hciStatus_t | HCI_EXT_ExtendRfRangeCmd (void) |
This HCI Extension API is used to Extend Rf Range using the TI CC2590 2.4 GHz RF Front End device. More... | |
hciStatus_t | HCI_EXT_HaltDuringRfCmd (uint8 mode) |
Halt During RF Command. More... | |
hciStatus_t | HCI_EXT_AdvEventNoticeCmd (uint8 taskID, uint16 taskEvent) |
This HCI Extension API is used to enable or disable a notification to the specified task using the specified task event whenever a Adv event ends. A non-zero taskEvent value is taken to be "enable", while a zero valued taskEvent is taken to be "disable". More... | |
hciStatus_t | HCI_EXT_ScanEventNoticeCmd (uint8 taskID, uint16 taskEvent) |
Scan Event Notice Command. More... | |
hciStatus_t | HCI_EXT_ConnEventNoticeCmd (uint16 connHandle, uint8 taskID, uint16 taskEvent) |
This HCI Extension API is used to enable or disable a notification to the specified task using the specified task event whenever a Connection event ends. A non-zero taskEvent value is taken to be "enable", while a zero valued taskEvent taken to be "disable". More... | |
hciStatus_t | HCI_EXT_BuildRevisionCmd (uint8 mode, uint16 userRevNum) |
This HCI Extension API is used set a user revision number or read the build revision number. More... | |
hciStatus_t | HCI_EXT_DelaySleepCmd (uint16 delay) |
This HCI Extension API is used set the sleep delay. More... | |
hciStatus_t | HCI_EXT_ResetSystemCmd (uint8 mode) |
This HCI Extension API is used to issue a soft or hard system reset. More... | |
hciStatus_t | HCI_EXT_LLTestModeCmd (uint8 testCase) |
This HCI Extension API is used to send a LL Test Mode test case. More... | |
hciStatus_t | HCI_EXT_OverlappedProcessingCmd (uint8 mode) |
This HCI Extension API is used to enable or disable overlapped processing. More... | |
hciStatus_t | HCI_EXT_NumComplPktsLimitCmd (uint8 limit, uint8 flushOnEvt) |
This HCI Extension API is used to set the minimum number of completed packets which must be met before a Number of Completed Packets event is returned. If the limit is not reach by the end of the connection event, then a Number of Completed Packets event will be returned (if non-zero) based on the flushOnEvt flag. More... | |
hciStatus_t | HCI_EXT_GetConnInfoCmd (uint8 *numAllocConns, uint8 *numActiveConns, hciConnInfo_t *activeConnInfo) |
Get Connection Info. More... | |
hciStatus_t | HCI_EXT_SetMaxDataLenCmd (uint16 txOctets, uint16 txTime, uint16 rxOctets, uint16 rxTime) |
This LE API is used to set the maximum supported Rx and Tx Octets (in bytes) and Time (in us). More... | |
hciStatus_t | HCI_EXT_ScanReqRptCmd (uint8 mode) |
This LE API is used to enable/disable Scan Request Reports. More... | |
This module implements the Host Controller Interface. For a detailed usage section describing how to send these commands and receive events, see the HCI Section of the User's Guide.
hciStatus_t HCI_DisconnectCmd | ( | uint16 | connHandle, |
uint8 | reason | ||
) |
This BT API is used to terminate a connection.
connHandle | - Connection handle. |
reason | - Reason for disconnection: HCI_DISCONNECT_AUTH_FAILURE, HCI_DISCONNECT_REMOTE_USER_TERM, HCI_DISCONNECT_REMOTE_DEV_POWER_OFF, HCI_DISCONNECT_UNSUPPORTED_REMOTE_FEATURE, HCI_DISCONNECT_KEY_PAIRING_NOT_SUPPORTED HCI_DISCONNECT_UNACCEPTABLE_CONN_INTERVAL |
hciStatus_t HCI_EXT_AdvEventNoticeCmd | ( | uint8 | taskID, |
uint16 | taskEvent | ||
) |
This HCI Extension API is used to enable or disable a notification to the specified task using the specified task event whenever a Adv event ends. A non-zero taskEvent value is taken to be "enable", while a zero valued taskEvent is taken to be "disable".
taskID | - User's task ID. |
taskEvent | - User's task event. |
hciStatus_t HCI_EXT_BuildRevisionCmd | ( | uint8 | mode, |
uint16 | userRevNum | ||
) |
This HCI Extension API is used set a user revision number or read the build revision number.
mode | - HCI_EXT_SET_USER_REVISION | HCI_EXT_READ_BUILD_REVISION |
userRevNum | - user defined reviison number |
hciStatus_t HCI_EXT_ClkDivOnHaltCmd | ( | uint8 | control | ) |
Set whether the system clock will be divided when the MCU is halted.
Related Events: HCI_VendorSpecifcCommandCompleteEvent
control | - HCI_EXT_ENABLE_CLK_DIVIDE_ON_HALT, HCI_EXT_DISABLE_CLK_DIVIDE_ON_HALT |
hciStatus_t HCI_EXT_ConnEventNoticeCmd | ( | uint16 | connHandle, |
uint8 | taskID, | ||
uint16 | taskEvent | ||
) |
This HCI Extension API is used to enable or disable a notification to the specified task using the specified task event whenever a Connection event ends. A non-zero taskEvent value is taken to be "enable", while a zero valued taskEvent taken to be "disable".
Note: This command does not check if the taskID and/or taskEvent are valid!
connHandle | - The HCI connection ID for connection event notice. |
taskID | - User's task ID. |
taskEvent | - User's task event. |
hciStatus_t HCI_EXT_DeclareNvUsageCmd | ( | uint8 | mode | ) |
This HCI Extension API is used to indicate to the Controller whether or not the Host will be using the NV memory during BLE operations.
Related Events: HCI_VendorSpecifcCommandCompleteEvent
mode | - HCI_EXT_NV_IN_USE, HCI_EXT_NV_NOT_IN_USE |
hciStatus_t HCI_EXT_DecryptCmd | ( | uint8 * | key, |
uint8 * | encText | ||
) |
This HCI Extension API is used to decrypt encrypted data using AES128.
Related Events: HCI_VendorSpecifcCommandCompleteEvent
key | - Pointer to 16 byte encryption key. |
encText | - Pointer to 16 byte encrypted data. |
hciStatus_t HCI_EXT_DelaySleepCmd | ( | uint16 | delay | ) |
This HCI Extension API is used set the sleep delay.
delay | - 0..1000, in milliseconds. |
hciStatus_t HCI_EXT_DisconnectImmedCmd | ( | uint16 | connHandle | ) |
This HCI Extension API is used to disconnect the connection immediately.
Note: The connection (if valid) is immediately terminated without notifying the remote device. The Host is still notified.
connHandle | - Connection handle. |
hciStatus_t HCI_EXT_EnablePTMCmd | ( | void | ) |
This HCI Extension API is used to enable Production Test Mode.
Note: This function can only be directly called from the application and is not available via an external transport interface such as RS232. Also, no vendor specific command complete will be returned.
hciStatus_t HCI_EXT_EndModemTestCmd | ( | void | ) |
This API is used to shutdown a modem test. A complete Controller reset will take place.
hciStatus_t HCI_EXT_ExtendRfRangeCmd | ( | void | ) |
This HCI Extension API is used to Extend Rf Range using the TI CC2590 2.4 GHz RF Front End device.
Related Events: HCI_VendorSpecifcCommandCompleteEvent
hciStatus_t HCI_EXT_GetConnInfoCmd | ( | uint8 * | numAllocConns, |
uint8 * | numActiveConns, | ||
hciConnInfo_t * | activeConnInfo | ||
) |
Get Connection Info.
This API is used to get connection related information, which includes the number of allocated connections, the number of active connections, and for each active connection, the connection ID, the connection role (Master or Slave), the peer address and peer address type. The number of allocated connections is based on a default build value that can be changed using MAX_NUM_BLE_CONNS. The number of active connections refers to active BLE connections.
numAllocConns | - Pointer for number of build time connections. |
numActiveConns | - Pointer for number of active BLE connections. |
activeConnInfo | - Pointer for active connection information. |
numAllocConns | - Number of build time connections allowed. |
numActiveConns | - Number of active BLE connections. |
activeConnInfo | - Active connection information. |
hciStatus_t HCI_EXT_HaltDuringRfCmd | ( | uint8 | mode | ) |
Halt During RF Command.
Enable or disable halting the CPU during RF. The system defaults to enabled.
Related Events: HCI_VendorSpecifcCommandCompleteEvent
mode | - HCI_EXT_HALT_DURING_RF_ENABLE, HCI_EXT_HALT_DURING_RF_DISABLE |
hciStatus_t HCI_EXT_LLTestModeCmd | ( | uint8 | testCase | ) |
This HCI Extension API is used to send a LL Test Mode test case.
testCase | - See list of defines in ll_common.h. |
hciStatus_t HCI_EXT_MapPmIoPortCmd | ( | uint8 | ioPort, |
uint8 | ioPin | ||
) |
This HCI Extension API is used to configure and map a CC254x I/O Port as a General Purpose I/O (GPIO) output signal that reflects the Power Management (PM) state of the CC254x device. The GPIO output will be High on Wake, and Low upon entering Sleep. This feature can be disabled by specifying HCI_EXT_PM_IO_PORT_NONE for the ioPort (ioPin is then ignored). The system default value upon hardware reset is disabled. This command can be used to control an external DC-DC Converter (its actual intent) such has the TI TPS62730 (or any similar converter that works the same way). This command should be used with extreme care as it will override how the Port/Pin was previously configured! This includes the mapping of Port 0 pins to 32kHz clock output, Analog I/O, UART, Timers; Port 1 pins to Observables, Digital Regulator status, UART, Timers; Port 2 pins to an external 32kHz XOSC. The selected Port/Pin will be configured as an output GPIO with interrupts masked. Careless use can result in a reconfiguration that could disrupt the system. It is therefore the user's responsibility to ensure the selected Port/Pin does not cause any conflicts in the system.
Note: Only Pins 0, 3 and 4 are valid for Port 2 since Pins 1 and 2 are mapped to debugger signals DD and DC.
Note: Port/Pin signal change will only occur when Power Savings is enabled.
ioPort | - HCI_EXT_PM_IO_PORT_P0, HCI_EXT_PM_IO_PORT_P1, HCI_EXT_PM_IO_PORT_P2, HCI_EXT_PM_IO_PORT_NONE |
ioPin | - HCI_EXT_PM_IO_PORT_PIN0, HCI_EXT_PM_IO_PORT_PIN1, HCI_EXT_PM_IO_PORT_PIN2, HCI_EXT_PM_IO_PORT_PIN3, HCI_EXT_PM_IO_PORT_PIN4, HCI_EXT_PM_IO_PORT_PIN5, HCI_EXT_PM_IO_PORT_PIN6, HCI_EXT_PM_IO_PORT_PIN7 |
hciStatus_t HCI_EXT_ModemHopTestTxCmd | ( | void | ) |
Start Modem Hop Tx Test.
Start a continuous transmitter direct test mode test using a modulated carrier wave and transmitting a 37 byte packet of Pseudo-Random 9-bit data. A packet is transmitted on a different frequency (linearly stepping through all RF channels 0..39) every 625us. Use HCI_EXT_EndModemTestCmd command to end the test.
Note: A Controller reset will be issued by HCI_EXT_EndModemTest! Note: The BLE device will transmit at maximum power. Note: This API can be used to verify this device meets Japan's TELEC regulations.
hciStatus_t HCI_EXT_ModemTestRxCmd | ( | uint8 | rxChan | ) |
Start Modem Hop RX Test.
Start a continuous receiver modem test using a modulated carrier wave tone, at the frequency that corresponds to the specific RF channel. Any received data is discarded. Receiver gain may be adjusted using the HCI_EXT_SetRxGain command. RSSI may be read during this test by using the HCI_ReadRssi command. Use HCI_EXT_EndModemTest command to end the test.
Note: A Controller reset will be issued by HCI_EXT_EndModemTest! Note: The BLE device will transmit at maximum power.
rxChan | - Receiver RF channel k=0..39, where BLE F=2402+(k*2MHz). |
hciStatus_t HCI_EXT_ModemTestTxCmd | ( | uint8 | cwMode, |
uint8 | txChan | ||
) |
This API is used start a continuous transmitter modem test, using either a modulated or unmodulated carrier wave tone, at the frequency that corresponds to the specified RF channel. Use HCI_EXT_EndModemTest command to end the test.
Note: A Controller reset will be issued by HCI_EXT_EndModemTest! Note: The BLE device will transmit at maximum power. Note: This API can be used to verify this device meets Japan's TELEC regulations.
Related Events: HCI_VendorSpecifcCommandCompleteEvent
cwMode | - HCI_EXT_TX_MODULATED_CARRIER, HCI_EXT_TX_UNMODULATED_CARRIER |
txChan | - Transmit RF channel k=0..39, where BLE F=2402+(k*2MHz). |
hciStatus_t HCI_EXT_NumComplPktsLimitCmd | ( | uint8 | limit, |
uint8 | flushOnEvt | ||
) |
This HCI Extension API is used to set the minimum number of completed packets which must be met before a Number of Completed Packets event is returned. If the limit is not reach by the end of the connection event, then a Number of Completed Packets event will be returned (if non-zero) based on the flushOnEvt flag.
limit | - From 1 to HCI_MAX_NUM_DATA_BUFFERS. |
flushOnEvt | - HCI_EXT_DISABLE_NUM_COMPL_PKTS_ON_EVENT | HCI_EXT_ENABLE_NUM_COMPL_PKTS_ON_EVENT |
hciStatus_t HCI_EXT_OnePktPerEvtCmd | ( | uint8 | control | ) |
This HCI Extension API is used to set whether a connection will be limited to one packet per event.
Related Events: HCI_VendorSpecifcCommandCompleteEvent
control | - HCI_EXT_ENABLE_ONE_PKT_PER_EVT, HCI_EXT_DISABLE_ONE_PKT_PER_EVT |
hciStatus_t HCI_EXT_OverlappedProcessingCmd | ( | uint8 | mode | ) |
This HCI Extension API is used to enable or disable overlapped processing.
mode | - HCI_EXT_ENABLE_OVERLAPPED_PROCESSING | HCI_EXT_DISABLE_OVERLAPPED_PROCESSING |
hciStatus_t HCI_EXT_PacketErrorRateCmd | ( | uint16 | connHandle, |
uint8 | command | ||
) |
This function is used to Reset or Read the Packet Error Rate counters for a connection.
Note: The counters are only 16 bits. At the shortest connection interval, this provides a bit over 8 minutes of data.
connHandle | - The LL connection ID on which to send this data. |
command | - HCI_EXT_PER_RESET, HCI_EXT_PER_READ |
hciStatus_t HCI_EXT_PERbyChanCmd | ( | uint16 | connHandle, |
perByChan_t * | perByChan | ||
) |
This HCI Extension API is used to start or end Packet Error Rate by Channel counter accumulation for a connection. If the pointer is not NULL, it is assumed there is sufficient memory for the PER data, per the type perByChan_t. If NULL, then the operation is considered disabled.
Note: It is the user's responsibility to make sure there is sufficient memory for the data, and that the counters are cleared prior to first use.
Note: The counters are only 16 bits. At the shortest connection interval, this provides a bit over 8 minutes of data.
connHandle | - The LL connection ID on which to send this data. |
perByChan | - Pointer to PER by Channel data, or NULL. |
hciStatus_t HCI_EXT_ResetSystemCmd | ( | uint8 | mode | ) |
This HCI Extension API is used to issue a soft or hard system reset.
mode | - HCI_EXT_RESET_SYSTEM_HARD | HCI_EXT_RESET_SYSTEM_SOFT |
output parameters
hciStatus_t HCI_EXT_SaveFreqTuneCmd | ( | void | ) |
This HCI Extension API is used to save the frequency tuning value to flash.
Note: This is a Production Test Mode only command!
hciStatus_t HCI_EXT_ScanEventNoticeCmd | ( | uint8 | taskID, |
uint16 | taskEvent | ||
) |
Scan Event Notice Command.
This HCI Extension API is used to enable or disable a notification to the specified task using the specified task event whenever a Scan event ends. A non-zero taskEvent value is taken to be "enable", while a zero valued taskEvent is taken to be "disable".
taskID | - User's task ID. |
taskEvent | - User's task event. |
hciStatus_t HCI_EXT_ScanReqRptCmd | ( | uint8 | mode | ) |
This LE API is used to enable/disable Scan Request Reports.
mode | - HCI_EXT_DISABLE_SCAN_REQUEST_REPORT | HCI_EXT_ENABLE_SCAN_REQUEST_REPORT |
hciStatus_t HCI_EXT_SetBDADDRCmd | ( | uint8 * | bdAddr | ) |
This API is used to set this device's BLE address (BDADDR).
Note: This command is only allowed when the device's state is Standby.
Related Events: HCI_VendorSpecifcCommandCompleteEvent
bdAddr | - A pointer to a buffer to hold this device's address. An invalid address (i.e. all FF's) will restore this device's address to the address set at initialization. |
hciStatus_t HCI_EXT_SetFastTxResponseTimeCmd | ( | uint8 | control | ) |
This HCI Extension API is used to set whether transmit data is sent as soon as possible even when slave latency is used.
Related Events: HCI_VendorSpecifcCommandCompleteEvent
control | - HCI_EXT_ENABLE_FAST_TX_RESP_TIME, HCI_EXT_DISABLE_FAST_TX_RESP_TIME |
hciStatus_t HCI_EXT_SetFreqTuneCmd | ( | uint8 | step | ) |
This HCI Extension API is used to set the frequency tuning up or down. Setting the mode up/down decreases/increases the amount of capacitance on the external crystal oscillator.
Note: This is a Production Test Mode only command!
step | - HCI_PTM_SET_FREQ_TUNE_UP, HCI_PTM_SET_FREQ_TUNE_DOWN |
hciStatus_t HCI_EXT_SetLocalSupportedFeaturesCmd | ( | uint8 * | localFeatures | ) |
This HCI Extension API is used to write this device's supported features.
Related Events: HCI_VendorSpecifcCommandCompleteEvent
localFeatures | - Pointer to eight bytes of local features. |
hciStatus_t HCI_EXT_SetMaxDataLenCmd | ( | uint16 | txOctets, |
uint16 | txTime, | ||
uint16 | rxOctets, | ||
uint16 | rxTime | ||
) |
This LE API is used to set the maximum supported Rx and Tx Octets (in bytes) and Time (in us).
Note: Any parameter not within a valid range will leave the corresponding supportedMax value unchanged.
txOctets | - Value of maximum supported Tx octets (in bytes). |
txTime | - Value of maximum supported Tx time (in us). |
rxOctets | - Value of maximum supported Rx octets (in bytes). |
rxTime | - Value of maximum supported Rx time (in us). |
hciStatus_t HCI_EXT_SetMaxDtmTxPowerCmd | ( | uint8 | txPower | ) |
This HCI Extension API is used to set the maximum transmit output power for Direct Test Mode.
Related Events: HCI_VendorSpecifcCommandCompleteEvent
txPower | - For CC254x: LL_EXT_TX_POWER_MINUS_23_DBM, LL_EXT_TX_POWER_MINUS_6_DBM, LL_EXT_TX_POWER_0_DBM, LL_EXT_TX_POWER_4_DBM |
For CC26xx: HCI_EXT_TX_POWER_MINUS_21_DBM, HCI_EXT_TX_POWER_MINUS_18_DBM, HCI_EXT_TX_POWER_MINUS_15_DBM, HCI_EXT_TX_POWER_MINUS_12_DBM, HCI_EXT_TX_POWER_MINUS_9_DBM, HCI_EXT_TX_POWER_MINUS_6_DBM, HCI_EXT_TX_POWER_MINUS_3_DBM, HCI_EXT_TX_POWER_0_DBM, HCI_EXT_TX_POWER_1_DBM, HCI_EXT_TX_POWER_2_DBM, HCI_EXT_TX_POWER_3_DBM, HCI_EXT_TX_POWER_4_DBM, HCI_EXT_TX_POWER_5_DBM
hciStatus_t HCI_EXT_SetRxGainCmd | ( | uint8 | rxGain | ) |
Set the receiver gain.
Related Events: HCI_VendorSpecifcCommandCompleteEvent
rxGain | - HCI_EXT_RX_GAIN_STD, HCI_EXT_RX_GAIN_HIGH |
hciStatus_t HCI_EXT_SetSCACmd | ( | uint16 | scaInPPM | ) |
This API is used to set this device's Sleep Clock Accuracy.
Note: For a slave device, this value is directly used, but only if power management is enabled. For a master device, this value is converted into one of eight ordinal values representing a SCA range, as specified in Table 2.2, Vol. 6, Part B, Section 2.3.3.1 of the Core specification.
Note: This command is only allowed when the device is not in a connection.
Note: The device's SCA value remains unaffected by a HCI_Reset.
scaInPPM | - A SCA value in PPM from 0..500. |
hciStatus_t HCI_EXT_SetSlaveLatencyOverrideCmd | ( | uint8 | control | ) |
This HCI Extension API is used to to enable or disable suspending slave latency.
Related Events: HCI_VendorSpecifcCommandCompleteEvent
control | - HCI_EXT_ENABLE_SL_OVERRIDE, HCI_EXT_DISABLE_SL_OVERRIDE |
hciStatus_t HCI_EXT_SetTxPowerCmd | ( | uint8 | txPower | ) |
Set the transmit power.
Related Events: HCI_VendorSpecifcCommandCompleteEvent
txPower | - For CC254x: HCI_EXT_TX_POWER_MINUS_23_DBM, HCI_EXT_TX_POWER_MINUS_6_DBM, HCI_EXT_TX_POWER_0_DBM, HCI_EXT_TX_POWER_4_DBM |
For CC26xx: HCI_EXT_TX_POWER_MINUS_21_DBM, HCI_EXT_TX_POWER_MINUS_18_DBM, HCI_EXT_TX_POWER_MINUS_15_DBM, HCI_EXT_TX_POWER_MINUS_12_DBM, HCI_EXT_TX_POWER_MINUS_9_DBM, HCI_EXT_TX_POWER_MINUS_6_DBM, HCI_EXT_TX_POWER_MINUS_3_DBM, HCI_EXT_TX_POWER_0_DBM, HCI_EXT_TX_POWER_1_DBM, HCI_EXT_TX_POWER_2_DBM, HCI_EXT_TX_POWER_3_DBM, HCI_EXT_TX_POWER_4_DBM, HCI_EXT_TX_POWER_5_DBM
void HCI_ExtTaskRegister | ( | uint8 | taskID | ) |
HCI vendor specific registration for Host extended commands.
taskID | - The Host Extended Command OSAL task identifier. |
void HCI_GAPTaskRegister | ( | uint8 | taskID | ) |
HCI vendor specific registration for Host GAP.
taskID | - The Host GAP OSAL task identifier. |
hciStatus_t HCI_HostBufferSizeCmd | ( | uint16 | hostAclPktLen, |
uint8 | hostSyncPktLen, | ||
uint16 | hostTotalNumAclPkts, | ||
uint16 | hostTotalNumSyncPkts | ||
) |
This BT API is used by the Host to notify the Controller of the maximum size ACL buffer size the Controller can send to the Host.
hostAclPktLen | - Host ACL data packet length. |
hostSyncPktLen | - Host SCO data packet length . |
hostTotalNumAclPkts | - Host total number of ACL data packets. |
hostTotalNumSyncPkts | - Host total number of SCO data packets. |
hciStatus_t HCI_HostNumCompletedPktCmd | ( | uint8 | numHandles, |
uint16 * | connHandles, | ||
uint16 * | numCompletedPkts | ||
) |
This BT API is used by the Host to notify the Controller of the number of HCI data packets that have been completed for each connection handle since this command was previously sent to the controller.
The Host_Number_Of_Conpleted_Packets command is a special command. No event is normally generated after the command has completed. The command should only be issued by the Host if flow control in the direction from controller to the host is on and there is at least one connection, or if the controller is in local loopback mode.
Related Events: HCI_CommandCompleteEvent
numHandles | - Number of connection handles. |
connHandles | - Array of connection handles. |
numCompletedPkts | - Array of number of completed packets. |
void HCI_L2CAPTaskRegister | ( | uint8 | taskID | ) |
HCI vendor specific registration for Host L2CAP.
taskID | - The Host L2CAP OSAL task identifier. |
hciStatus_t HCI_LE_AddDeviceToResolvingListCmd | ( | uint8 | peerIdAddrType, |
uint8 * | peerIdAddr, | ||
uint8 * | peerIRK, | ||
uint8 * | localIRK | ||
) |
Add a device to the resolving list.
Add one device to the list of address translations used to resolve Resolvable Private Addresses in the Controller.
peerIdAddrType | - HCI_PUBLIC_DEVICE_ADDRESS, HCI_RANDOM_DEVICE_ADDRESS |
peerIdAddr | - Peer device Identity Address. |
peerIRK | - IRK of peer device. |
localIRK | - IRK for own device. |
hciStatus_t HCI_LE_AddWhiteListCmd | ( | uint8 | addrType, |
uint8 * | devAddr | ||
) |
Add a white list entry.
Related Events: HCI_CommandCompleteEvent
addrType | - HCI_PUBLIC_DEVICE_ADDRESS, HCI_RANDOM_DEVICE_ADDRESS |
devAddr | - Pointer to address of device to put in white list. |
hciStatus_t HCI_LE_ClearResolvingListCmd | ( | void | ) |
Remove all devices from the whitelist.
Remove all devices from the list of address translations used to resolve Resolvable Private addresses in the Controller.
hciStatus_t HCI_LE_ClearWhiteListCmd | ( | void | ) |
Clear the white list.
Related Events: HCI_CommandCompleteEvent
hciStatus_t HCI_LE_ConnUpdateCmd | ( | uint16 | connHandle, |
uint16 | connIntervalMin, | ||
uint16 | connIntervalMax, | ||
uint16 | connLatency, | ||
uint16 | connTimeout, | ||
uint16 | minLen, | ||
uint16 | maxLen | ||
) |
Update the connection parameters.
Related Events: HCI_CommandStatusEvent, ConnectionUpdateCompleteEvent
connHandle | - Connection handle. |
connIntervalMin | - Minimum allowed connection interval. |
connIntervalMax | - Maximum allowed connection interval. |
connLatency | - Number of skipped events (slave latency). |
connTimeout | - Connection supervision timeout. |
minLen | - Info parameter about min length of conn. |
maxLen | - Info parameter about max length of conn. |
hciStatus_t HCI_LE_CreateConnCancelCmd | ( | void | ) |
Cancel connection.
Related Events: HCI_CommandCompleteEvent
hciStatus_t HCI_LE_CreateConnCmd | ( | uint16 | scanInterval, |
uint16 | scanWindow, | ||
uint8 | initFilterPolicy, | ||
uint8 | addrTypePeer, | ||
uint8 * | peerAddr, | ||
uint8 | ownAddrType, | ||
uint16 | connIntervalMin, | ||
uint16 | connIntervalMax, | ||
uint16 | connLatency, | ||
uint16 | connTimeout, | ||
uint16 | minLen, | ||
uint16 | maxLen | ||
) |
Create a connection.
Related Events: HCI_CommandStatusEvent, ConnectionCompleteEvent
scanInterval | - Time between Init scan events. |
scanWindow | - Time of scan before Init scan event ends. Note: When the scanWindow equals the scanInterval then scanning is continuous. |
initFilterPolicy | - HCI_INIT_WL_POLICY_USE_PEER_ADDR, HCI_INIT_WL_POLICY_USE_WHITE_LIST |
addrTypePeer | - HCI_PUBLIC_DEVICE_ADDRESS, HCI_RANDOM_DEVICE_ADDRESS |
peerAddr | - Pointer to peer device's address. |
ownAddrType | - HCI_PUBLIC_DEVICE_ADDRESS, HCI_RANDOM_DEVICE_ADDRESS |
connIntervalMin | - Minimum allowed connection interval. |
connIntervalMax | - Maximum allowed connection interval. |
connLatency | - Number of skipped events (slave latency). |
connTimeout | - Connection supervision timeout. |
minLen | - Info parameter about min length of conn. |
maxLen | - Info parameter about max length of conn. |
hciStatus_t HCI_LE_EncryptCmd | ( | uint8 * | key, |
uint8 * | plainText | ||
) |
Perform an encryption using AES128.
Note: Input parameters are ordered MSB..LSB.
Related Events: HCI_CommandCompleteEvent
key | - Pointer to 16 byte encryption key. |
plainText | - Pointer to 16 byte plaintext data. |
hciStatus_t HCI_LE_EnhancedRxTestCmd | ( | uint8 | rxChan, |
uint8 | rxPhy, | ||
uint8 | modIndex | ||
) |
Start Enhanced RX Test.
Start a test where the DUT receives reference packets at a fixed interval. The tester generates the test reference packets.
rxChan | - Rx Channel k=0..39, where F=2402+(k*2MHz). |
rxPhy | - Rx PHY to use. |
modIndex | - HCI_DTM_STANDARD_MODULATION_INDEX, HCI_DTM_STABLE_MODULATION_INDEX |
hciStatus_t HCI_LE_EnhancedTxTestCmd | ( | uint8 | txChan, |
uint8 | payloadLen, | ||
uint8 | payloadType, | ||
uint8 | txPhy | ||
) |
Start Enhanced TX Test.
Start a test where the DUT generates test reference packets at a fixed interval. The Controller shall transmit at maximum power.
txChan | - Tx RF channel k=0..39, where F=2402+(k*2MHz). |
payloadLen | - Byte length (0..37) in payload for each packet. |
payloadType | - The type of pattern to transmit. |
txPhy | - Tx PHY to use. |
hciStatus_t HCI_LE_GenerateDHKeyCmd | ( | uint8 * | publicKey | ) |
Generate Diffie-Hellman Key.
This LE API is used to initiate the generation of a Diffie- Hellman key in the Controller for use over the LE transport. This command takes the remote P-256 public key as input. The Diffie-Hellman key generation uses the private key generated by LE_Read_Local_P256_Public_Key command.
Note: Generates LE DHKey Generation Complete event.
publicKey | The remote P-256 public key (X-Y format). |
hciStatus_t HCI_LE_LtkReqNegReplyCmd | ( | uint16 | connHandle | ) |
This LE API is used by the Host to send to the Controller a negative LTK reply.
Related Events: HCI_CommandCompleteEvent
connHandle | - Connection handle. |
hciStatus_t HCI_LE_LtkReqReplyCmd | ( | uint16 | connHandle, |
uint8 * | ltk | ||
) |
This LE API is used by the Host to send to the Controller a positive LTK reply.
Related Events: HCI_CommandCompleteEvent
connHandle | - Connection handle. |
ltk | - Pointer to 16 byte Long Term Key. |
hciStatus_t HCI_LE_RandCmd | ( | void | ) |
Generate a random number.
Related Events: HCI_CommandCompleteEvent
hciStatus_t HCI_LE_ReadAdvChanTxPowerCmd | ( | void | ) |
Read transmit power when Advertising.
Related Events: HCI_CommandCompleteEvent
hciStatus_t HCI_LE_ReadBufSizeCmd | ( | void | ) |
This LE API is used by the Host to determine the maximum ACL data packet size allowed by the Controller.
Related Events: HCI_CommandCompleteEvent
hciStatus_t HCI_LE_ReadChannelMapCmd | ( | uint16 | connHandle | ) |
Read a connection's data channel map.
Related Events: HCI_CommandCompleteEvent
connHandle | - Connection handle. |
hciStatus_t HCI_LE_ReadLocalP256PublicKeyCmd | ( | void | ) |
Read local P-256 Public Key.
Read the local P-256 public key from the Controller. The Controller shall generate a new P-256 public/ private key pair upon receipt of this command.
Note: Generates LE Read Local P256 Public Key Complete event.
hciStatus_t HCI_LE_ReadLocalResolvableAddressCmd | ( | uint8 | localIdAddrType, |
uint8 * | localIdAddr | ||
) |
Read Local Resolvable Private Address.
Get the current local Resolvable Private Address being used for the corresponding local Public or Random (Static) Identity Address.
localIdAddrType | - HCI_PUBLIC_DEVICE_ADDRESS, HCI_RANDOM_DEVICE_ADDRESS |
localIdAddr | - Local device Identity Address. |
hciStatus_t HCI_LE_ReadLocalSupportedFeaturesCmd | ( | void | ) |
Read the LE locally supported features.
Related Events: HCI_CommandCompleteEvent
hciStatus_t HCI_LE_ReadMaxDataLenCmd | ( | void | ) |
Read max data length.
Read the maximum supported transmit and receive payload octets and packet duration times.
hciStatus_t HCI_LE_ReadPeerResolvableAddressCmd | ( | uint8 | peerIdAddrType, |
uint8 * | peerIdAddr | ||
) |
Read the Peer Resolvable Address.
Get the current peer Resolvable Private Address being used for the corresponding peer Public or Random (Static) Identity Address.
peerIdAddrType | - HCI_PUBLIC_DEVICE_ADDRESS, HCI_RANDOM_DEVICE_ADDRESS |
peerIdAddr | - Peer device Identity Address. |
hciStatus_t HCI_LE_ReadPhyCmd | ( | uint16 | connHandle | ) |
Read the current transmitter and receiver PHY.
connHandle | - Connection handle. |
hciStatus_t HCI_LE_ReadRemoteUsedFeaturesCmd | ( | uint16 | connHandle | ) |
Read the remote device's used features.
Related Events: HCI_CommandStatusEvent, ReadRemoteUsedFeaturesCompleteEvent
connHandle | - Connection handle. |
hciStatus_t HCI_LE_ReadResolvingListSizeCmd | ( | void | ) |
Read Resolving List Size.
Read the total number of address translation entries in the resolving list that can be stored in the Controller.
hciStatus_t HCI_LE_ReadSuggestedDefaultDataLenCmd | ( | void | ) |
Read Suggested Default Data Length.
Read the default maximum trasmit packet size and the default maximum packet transmit time to be used for new connections.
hciStatus_t HCI_LE_ReadSupportedStatesCmd | ( | void | ) |
Read the Controller's supported states.
Related Events: HCI_CommandCompleteEvent
hciStatus_t HCI_LE_ReadWhiteListSizeCmd | ( | void | ) |
Read the white list.
Related Events: HCI_CommandCompleteEvent
hciStatus_t HCI_LE_ReceiverTestCmd | ( | uint8 | rxChan | ) |
Start the receiver Direct Test Mode test.
Related Events: HCI_CommandCompleteEvent
rxChan | - Rx Channel k=0..39, where F=2402+(k*2MHz). |
hciStatus_t HCI_LE_RemoteConnParamReqNegReplyCmd | ( | uint16 | connHandle, |
uint8 | reason | ||
) |
Negatively reply to the Conneciton Parameter Update Request.
This LE API is used to negatively reply to the HCI LE Remote Connection Parameter Request event from the Controller. This command indicates that the Host has denied the remote device's request to change connection parameters.
Related Events: HCI_CommandCompleteEvent
connHandle | - Connection handle. |
reason | - Reason connection parameter request was rejected. |
hciStatus_t HCI_LE_RemoteConnParamReqReplyCmd | ( | uint16 | connHandle, |
uint16 | connIntervalMin, | ||
uint16 | connIntervalMax, | ||
uint16 | connLatency, | ||
uint16 | connTimeout, | ||
uint16 | minLen, | ||
uint16 | maxLen | ||
) |
This LE API is used to positively reply to the HCI LE Remote Connection Parameter Request event from the Controller. This command indicates that the Host has accepted the remote device's request to change connection parameters.
Related Events: HCI_CommandCompleteEvent
connHandle | - Connection handle. |
connIntervalMin | - Minimum allowed connection interval. |
connIntervalMax | - Maximum allowed connection interval. |
connLatency | - Number of skipped events (slave latency). |
connTimeout | - Connection supervision timeout. |
minLen | - Info parameter about min length of conn. |
maxLen | - Info parameter about max length of conn. |
hciStatus_t HCI_LE_RemoveDeviceFromResolvingListCmd | ( | uint8 | peerIdAddrType, |
uint8 * | peerIdAddr | ||
) |
Remove a device from the whitelist.
Remove one device fromthe list of address translations used to resolve Resolvable Private Addresses in the Controller.
peerIdAddrType | - HCI_PUBLIC_DEVICE_ADDRESS, HCI_RANDOM_DEVICE_ADDRESS |
peerIdAddr | - Peer device Identity Address. |
hciStatus_t HCI_LE_RemoveWhiteListCmd | ( | uint8 | addrType, |
uint8 * | devAddr | ||
) |
Remove a white list entry.
Related Events: HCI_CommandCompleteEvent
addrType | - HCI_PUBLIC_DEVICE_ADDRESS, HCI_RANDOM_DEVICE_ADDRESS |
devAddr | - Pointer to address of device to remove from the white list. |
hciStatus_t HCI_LE_SetAddressResolutionEnableCmd | ( | uint8 | addrResolutionEnable | ) |
Disable / Enable Address Resolution.
Enable resolution of Resolvable Private Addresses in the Controller. This causes the Controller to use the resolving list whenever the Controller receives a local or peer Resolvable Private Address.
addrResolutionEnable | - HCI_DISABLE_ADDR_RESOLUTION, HCI_ENABLE_ADDR_RESOLUTION |
hciStatus_t HCI_LE_SetAdvDataCmd | ( | uint8 | dataLen, |
uint8 * | pData | ||
) |
Set the Advertising data.
Related Events: HCI_CommandCompleteEvent
dataLen | - Length of Advertising data. |
pData | - Pointer to Advertising data. |
hciStatus_t HCI_LE_SetAdvEnableCmd | ( | uint8 | advEnable | ) |
Turn Advertising on or off.
Related Events: HCI_CommandCompleteEvent
advEnable | - HCI_ENABLE_ADV, HCI_DISABLE_ADV |
hciStatus_t HCI_LE_SetAdvParamCmd | ( | uint16 | advIntervalMin, |
uint16 | advIntervalMax, | ||
uint8 | advType, | ||
uint8 | ownAddrType, | ||
uint8 | directAddrType, | ||
uint8 * | directAddr, | ||
uint8 | advChannelMap, | ||
uint8 | advFilterPolicy | ||
) |
Set the Advertising parameters.
Related Events: HCI_CommandCompleteEvent
advIntervalMin | - Minimum allowed advertising interval. |
advIntervalMax | - Maximum allowed advertising interval. |
advType | - HCI_CONNECTABLE_UNDIRECTED_ADV, HCI_CONNECTABLE_DIRECTED_HDC_ADV, HCI_SCANNABLE_UNDIRECTED, HCI_NONCONNECTABLE_UNDIRECTED_ADV HCI_CONNECTABLE_DIRECTED_LDC_ADV |
ownAddrType | - HCI_PUBLIC_DEVICE_ADDRESS, HCI_RANDOM_DEVICE_ADDRESS |
directAddrType | - HCI_PUBLIC_DEVICE_ADDRESS, HCI_RANDOM_DEVICE_ADDRESS |
directAddr | - Pointer to address of device when using directed advertising. |
advChannelMap | - HCI_ADV_CHAN_37, HCI_ADV_CHAN_38, HCI_ADV_CHAN_39, HCI_ADV_CHAN_37 | HCI_ADV_CHAN_38, HCI_ADV_CHAN_37 | HCI_ADV_CHAN_39, HCI_ADV_CHAN_38 | HCI_ADV_CHAN_39, HCI_ADV_CHAN_ALL |
advFilterPolicy | - HCI_ADV_WL_POLICY_ANY_REQ, HCI_ADV_WL_POLICY_WL_SCAN_REQ, HCI_ADV_WL_POLICY_WL_CONNECT_REQ, HCI_ADV_WL_POLICY_WL_ALL_REQ |
hciStatus_t HCI_LE_SetDataLenCmd | ( | uint16 | connHandle, |
uint16 | txOctets, | ||
uint16 | txTime | ||
) |
Set Data Length.
Set the maximum transmission packet size and the maximum packet transmission time for the connection.
connHandle | - Connection handle. |
txOctets | - Maximum transmit payload size (in bytes). |
txTime | - Maximum transmit time (in us). |
hciStatus_t HCI_LE_SetDefaultPhyCmd | ( | uint8 | allPhys, |
uint8 | txPhy, | ||
uint8 | rxPhy | ||
) |
Set Default PHY.
Allows the Host to specify its preferred values for the transmitter and receiver PHY to be used for all subsequent connections.
allPhys | - Host preference on how to handle txPhy and rxPhy. |
txPhy | - Bit field of Host preferred Tx PHY. |
rxPhy | - Bit field of Host preferred Rx PHY. |
hciStatus_t HCI_LE_SetEventMaskCmd | ( | uint8 * | pEventMask | ) |
This LE API is used to set the HCI LE event mask, which is used to determine which LE events are supported.
Related Events: HCI_CommandCompleteEvent
pEventMask | - Pointer to LE event mask of 8 bytes. |
hciStatus_t HCI_LE_SetHostChanClassificationCmd | ( | uint8 * | chanMap | ) |
Update the current data channel map.
Related Events: HCI_CommandCompleteEvent
chanMap | - Pointer to the new channel map. |
hciStatus_t HCI_LE_SetPhyCmd | ( | uint16 | connHandle, |
uint8 | allPhys, | ||
uint8 | txPhy, | ||
uint8 | rxPhy | ||
) |
This LE API is used to request a change to the transmitter and receiver PHY for a connection.
connHandle | - Connection handle. |
allPhys | - Host preference on how to handle txPhy and rxPhy. |
txPhy | - Bit field of Host preferred Tx PHY. |
rxPhy | - Bit field of Host preferred Rx PHY. |
hciStatus_t HCI_LE_SetRandomAddressCmd | ( | uint8 * | pRandAddr | ) |
Set this device's Random address.
Related Events: HCI_CommandCompleteEvent
pRandAddr | - Pointer to random address. |
hciStatus_t HCI_LE_SetResolvablePrivateAddressTimeoutCmd | ( | uint16 | rpaTimeout | ) |
Set Resolvable Private Address Timeout.
Set the length of time the Controller uses a Resolvable Private Address before a new Resolvable Private Address is generated and starts being used.
rpaTimeout | - RPA timeout (in secs). |
hciStatus_t HCI_LE_SetScanEnableCmd | ( | uint8 | scanEnable, |
uint8 | filterDuplicates | ||
) |
Turn Scanning on or off.
Related Events: HCI_CommandCompleteEvent, AdvReportEvent
scanEnable | - HCI_SCAN_START, HCI_SCAN_STOP |
filterDuplicates | - HCI_FILTER_REPORTS_ENABLE, HCI_FILTER_REPORTS_DISABLE |
hciStatus_t HCI_LE_SetScanParamCmd | ( | uint8 | scanType, |
uint16 | scanInterval, | ||
uint16 | scanWindow, | ||
uint8 | ownAddrType, | ||
uint8 | filterPolicy | ||
) |
Set the Scan parameters.
Related Events: HCI_CommandCompleteEvent
scanType | - HCI_SCAN_PASSIVE, HCI_SCAN_ACTIVE |
scanInterval | - Time between scan events. |
scanWindow | - Time of scan before scan event ends. Note: When the scanWindow equals the scanInterval then scanning is continuous. |
ownAddrType | - This device's address. |
filterPolicy | - HCI_SCAN_PASSIVE, HCI_SCAN_ACTIVE |
hciStatus_t HCI_LE_SetScanRspDataCmd | ( | uint8 | dataLen, |
uint8 * | pData | ||
) |
Set the Advertising Scan Response data.
Related Events: HCI_CommandCompleteEvent
dataLen | - Length of Scan Response data. |
pData | - Pointer to Scan Response data. |
hciStatus_t HCI_LE_StartEncyptCmd | ( | uint16 | connHandle, |
uint8 * | random, | ||
uint8 * | encDiv, | ||
uint8 * | ltk | ||
) |
Start encryption in a connection.
Related Events: HCI_CommandStatusEvent, EncChangeEvent or EncKeyRefreshEvent
connHandle | - Connection handle. |
random | - Pointer to eight byte Random number. |
encDiv | - Pointer to two byte Encrypted Diversifier. |
ltk | - Pointer to 16 byte Long Term Key. |
hciStatus_t HCI_LE_TestEndCmd | ( | void | ) |
End the Direct Test Mode test.
Related Events: HCI_CommandCompleteEvent
hciStatus_t HCI_LE_TransmitterTestCmd | ( | uint8 | txChan, |
uint8 | dataLen, | ||
uint8 | pktPayload | ||
) |
This LE API is used to start the transmit Direct Test Mode test.
txChan | - Tx RF frequency k=0..39, where F=2402+(k*2MHz). |
dataLen | - Test data length: 0..37 bytes |
pktPayload | - Type of packet payload, per Direct Test Mode spec: HCI_DIRECT_TEST_PAYLOAD_PRBS9, HCI_DIRECT_TEST_PAYLOAD_0x0F, HCI_DIRECT_TEST_PAYLOAD_0x55, HCI_DIRECT_TEST_PAYLOAD_PRBS15, HCI_DIRECT_TEST_PAYLOAD_0xFF, HCI_DIRECT_TEST_PAYLOAD_0x00, HCI_DIRECT_TEST_PAYLOAD_0xF0, HCI_DIRECT_TEST_PAYLOAD_0xAA |
hciStatus_t HCI_LE_WriteSuggestedDefaultDataLenCmd | ( | uint16 | txOctets, |
uint16 | txTime | ||
) |
Write Suggested Default Data Length.
Set the default maximum transmission packet size and the default maximum packet transmission time for the connection.
txOctets | - Maximum transmit payload size (in bytes). |
txTime | - Maximum transmit time (in us). |
hciStatus_t HCI_ReadAuthPayloadTimeoutCmd | ( | uint16 | connHandle, |
uint16 * | aptoValue | ||
) |
Read the connection's Authenticated Payload Timeout value.
connHandle | - The LL connection ID to read the APTO value from. |
aptoValue | - Pointer to current APTO value, in units of 10ms. |
hciStatus_t HCI_ReadBDADDRCmd | ( | void | ) |
Read this device's BLE address (BDADDR).
Related Events: HCI_CommandCompleteEvent
hciStatus_t HCI_ReadLocalSupportedCommandsCmd | ( | void | ) |
Read the locally supported commands.
Related Events: HCI_CommandCompleteEvent
hciStatus_t HCI_ReadLocalSupportedFeaturesCmd | ( | void | ) |
Read the locally supported features.
Related Events: HCI_CommandCompleteEvent
hciStatus_t HCI_ReadLocalVersionInfoCmd | ( | void | ) |
Read the local version information.
Related Events: HCI_CommandCompleteEvent
hciStatus_t HCI_ReadRemoteVersionInfoCmd | ( | uint16 | connHandle | ) |
This BT API is used to request version information from the the remote device in a connection.
Related Events: HCI_CommandStatusEvent, ReadRemoteVersionInfoEvent
connHandle | - Connection handle. |
hciStatus_t HCI_ReadRssiCmd | ( | uint16 | connHandle | ) |
Read RSSI of last packet.
Read the RSSI of the last packet received on a connection given by the connection handle. If the Receiver Modem test is running (HCI_EXT_ModemTestRx), then the RF RSSI for the last received data will be returned. If there is no RSSI value, then HCI_RSSI_NOT_AVAILABLE will be returned.
Related Events: HCI_CommandCompleteEvent
connHandle | - Connection handle. |
hciStatus_t HCI_ReadTransmitPowerLevelCmd | ( | uint16 | connHandle, |
uint8 | txPwrType | ||
) |
Read the transmit power level.
Related Events: HCI_CommandCompleteEvent
connHandle | - Connection handle. |
txPwrType | - HCI_READ_CURRENT_TX_POWER_LEVEL, HCI_READ_MAXIMUM_TX_POWER_LEVEL |
hciStatus_t HCI_ResetCmd | ( | void | ) |
Reset the Link Layer.
Related Events: HCI_CommandCompleteEvent
hciStatus_t HCI_SendDataPkt | ( | uint16 | connHandle, |
uint8 | pbFlag, | ||
uint16 | pktLen, | ||
uint8 * | pData | ||
) |
This API is used to send a ACL data packet over a connection.
connHandle | - Connection ID (handle). |
pbFlag | - Packet Boundary Flag. |
pktLen | - Number of bytes of data to transmit. |
*pData | - Pointer to data buffer to transmit. |
hciStatus_t HCI_SetControllerToHostFlowCtrlCmd | ( | uint8 | flowControlEnable | ) |
This BT API is used by the Host to turn flow control on or off for data sent from the Controller to Host. Related Events: HCI_CommandCompleteEvent.
flowControlEnable | - HCI_CTRL_TO_HOST_FLOW_CTRL_OFF, HCI_CTRL_TO_HOST_FLOW_CTRL_ACL_ON_SYNCH_OFF, HCI_CTRL_TO_HOST_FLOW_CTRL_ACL_OFF_SYNCH_ON, HCI_CTRL_TO_HOST_FLOW_CTRL_ACL_ON_SYNCH_ON |
hciStatus_t HCI_SetEventMaskCmd | ( | uint8 * | pMask | ) |
This BT API is used to set the HCI event mask, which is used to determine which events are supported.
Related Events: HCI_CommandCompleteEvent
pMask | - Pointer to an eight byte event mask. |
hciStatus_t HCI_SetEventMaskPage2Cmd | ( | uint8 * | pMask | ) |
This BT API is used to set the HCI event mask page 2, which is used to determine which events are supported.
Related Events: HCI_CommandCompleteEvent
pMask | - Pointer to an eight byte event mask. |
void HCI_SMPTaskRegister | ( | uint8 | taskID | ) |
HCI vendor specific registration for Host SMP.
taskID | - The Host SMP OSAL task identifier. |
void HCI_TestAppTaskRegister | ( | uint8 | taskID | ) |
HCI vendor specific registration for HCI Test Application.
taskID | - The HCI Test Application OSAL task identifier. |
uint8 HCI_ValidConnTimeParams | ( | uint16 | connIntervalMin, |
uint16 | connIntervalMax, | ||
uint16 | connLatency, | ||
uint16 | connTimeout | ||
) |
This API is used to check that the connection time parameter ranges are valid, and that the connection time parameter combination is valid. It also checks if the min/max CI range is valid.
connIntervalMin | - Minimum connection interval. |
connIntervalMax | - Maximum connection interval. |
connLatency | - Connection slave latency. |
connTimeout | - Connection supervision timeout. |
hciStatus_t HCI_WriteAuthPayloadTimeoutCmd | ( | uint16 | connHandle, |
uint16 | aptoValue | ||
) |
Used to write the connection's Authenticated Payload Timeout value.
connHandle | - The LL connection ID to write the APTO value to. |
aptoValue | - The APTO value, in units of 10ms. |