TI BLE Stack API Documentation
2.03.08
|
Macros | |
#define | TGAP_GEN_DISC_ADV_MIN 0 |
Minimum time to remain advertising, when in Discoverable mode (mSec). Setting this parameter to 0 turns off the timeout (default). | |
#define | TGAP_LIM_ADV_TIMEOUT 1 |
Maximum time to remain advertising, when in Limited Discoverable mode. In seconds (default 180 seconds) | |
#define | TGAP_GEN_DISC_SCAN 2 |
Minimum time to perform scanning, when performing General Discovery proc (mSec) | |
#define | TGAP_LIM_DISC_SCAN 3 |
Minimum time to perform scanning, when performing Limited Discovery proc (mSec) | |
#define | TGAP_CONN_EST_ADV_TIMEOUT 4 |
Advertising timeout, when performing Connection Establishment proc (mSec) | |
#define | TGAP_CONN_PARAM_TIMEOUT 5 |
Link Layer connection parameter update notification timer, connection parameter update proc (mSec) | |
#define | TGAP_LIM_DISC_ADV_INT_MIN 6 |
Minimum advertising interval, when in limited discoverable mode (n * 0.625 mSec) | |
#define | TGAP_LIM_DISC_ADV_INT_MAX 7 |
Maximum advertising interval, when in limited discoverable mode (n * 0.625 mSec) | |
#define | TGAP_GEN_DISC_ADV_INT_MIN 8 |
Minimum advertising interval, when in General discoverable mode (n * 0.625 mSec) | |
#define | TGAP_GEN_DISC_ADV_INT_MAX 9 |
Maximum advertising interval, when in General discoverable mode (n * 0.625 mSec) | |
#define | TGAP_CONN_ADV_INT_MIN 10 |
Minimum advertising interval, when in Connectable mode (n * 0.625 mSec) | |
#define | TGAP_CONN_ADV_INT_MAX 11 |
Maximum advertising interval, when in Connectable mode (n * 0.625 mSec) | |
#define | TGAP_CONN_SCAN_INT 12 |
Scan interval used during Link Layer Initiating state, when in Connectable mode (n * 0.625 mSec) | |
#define | TGAP_CONN_SCAN_WIND 13 |
Scan window used during Link Layer Initiating state, when in Connectable mode (n * 0.625 mSec) | |
#define | TGAP_CONN_HIGH_SCAN_INT 14 |
Scan interval used during Link Layer Initiating state, when in Connectable mode, high duty scan cycle scan parameters (n * 0.625 mSec) | |
#define | TGAP_CONN_HIGH_SCAN_WIND 15 |
Scan window used during Link Layer Initiating state, when in Connectable mode, high duty scan cycle scan parameters (n * 0.625 mSec) | |
#define | TGAP_GEN_DISC_SCAN_INT 16 |
Scan interval used during Link Layer Scanning state, when in General Discovery proc (n * 0.625 mSec) | |
#define | TGAP_GEN_DISC_SCAN_WIND 17 |
Scan window used during Link Layer Scanning state, when in General Discovery proc (n * 0.625 mSec) | |
#define | TGAP_LIM_DISC_SCAN_INT 18 |
Scan interval used during Link Layer Scanning state, when in Limited Discovery proc (n * 0.625 mSec) | |
#define | TGAP_LIM_DISC_SCAN_WIND 19 |
Scan window used during Link Layer Scanning state, when in Limited Discovery proc (n * 0.625 mSec) | |
#define | TGAP_CONN_EST_ADV 20 |
Advertising interval, when using Connection Establishment proc (n * 0.625 mSec). Obsolete - Do not use. | |
#define | TGAP_CONN_EST_INT_MIN 21 |
Minimum Link Layer connection interval, when using Connection Establishment proc (n * 1.25 mSec) | |
#define | TGAP_CONN_EST_INT_MAX 22 |
Maximum Link Layer connection interval, when using Connection Establishment proc (n * 1.25 mSec) | |
#define | TGAP_CONN_EST_SCAN_INT 23 |
Scan interval used during Link Layer Initiating state, when using Connection Establishment proc (n * 0.625 mSec) | |
#define | TGAP_CONN_EST_SCAN_WIND 24 |
Scan window used during Link Layer Initiating state, when using Connection Establishment proc (n * 0.625 mSec) | |
#define | TGAP_CONN_EST_SUPERV_TIMEOUT 25 |
Link Layer connection supervision timeout, when using Connection Establishment proc (n * 10 mSec) | |
#define | TGAP_CONN_EST_LATENCY 26 |
Link Layer connection slave latency, when using Connection Establishment proc (in number of connection events) | |
#define | TGAP_CONN_EST_MIN_CE_LEN 27 |
Local informational parameter about min len of connection needed, when using Connection Establishment proc (n * 0.625 mSec) | |
#define | TGAP_CONN_EST_MAX_CE_LEN 28 |
Local informational parameter about max len of connection needed, when using Connection Establishment proc (n * 0.625 mSec) | |
#define | TGAP_PRIVATE_ADDR_INT 29 |
Minimum Time Interval between private (resolvable) address changes. In minutes (default 15 minutes) | |
#define | TGAP_CONN_PAUSE_CENTRAL 30 |
Central idle timer. In seconds (default 1 second) | |
#define | TGAP_CONN_PAUSE_PERIPHERAL 31 |
Minimum time upon connection establishment before the peripheral starts a connection update procedure. In seconds (default 5 seconds) | |
#define | TGAP_SM_TIMEOUT 32 |
SM Message Timeout (milliseconds). Default 30 seconds. | |
#define | TGAP_SM_MIN_KEY_LEN 33 |
SM Minimum Key Length supported. Default 7. | |
#define | TGAP_SM_MAX_KEY_LEN 34 |
SM Maximum Key Length supported. Default 16. | |
#define | TGAP_FILTER_ADV_REPORTS 35 |
Filter duplicate advertising reports. Default TRUE. | |
#define | TGAP_SCAN_RSP_RSSI_MIN 36 |
Minimum RSSI required for scan responses to be reported to the app. Default -127. | |
#define | TGAP_REJECT_CONN_PARAMS 37 |
Whether or not to reject Connection Parameter Update Request received on Central device. Default FALSE. | |
#define | TGAP_AUTH_TASK_ID 38 |
Task ID override for Task Authentication control (for stack internal use only) | |
#define | TGAP_VERIFY_CAR 39 |
Verify CAR is true before sending ADV DIR using RPA. | |
#define | TGAP_PARAMID_MAX 40 |
ID MAX-valid Parameter ID. | |
Used in place of gapParamIDs_t.