MSP430UltrasonicLibrary
02_20_00_15
|
Contains USS SW Lib Measurement Configuration. More...
#include <ussSwLib.h>
Data Fields | |
USS_measurement_capture_sequence | sequenceSelection |
USS_measurement_end_of_sequence_state | eofSequenceState |
USS_measurement_drive_strength | ch0DriveStrength |
USS_measurement_drive_strength | ch1DriveStrength |
USS_Pulse_Configuration * | pulseConfig |
uint_least16_t | startPPGCount |
uint_least16_t | turnOnADCCount |
uint_least16_t | startPGAandINBiasCount |
uint_least16_t | startADCsamplingCount |
uint_least16_t | restartCaptureCount |
uint_least16_t | captureTimeOutCount |
uint_least16_t | restartLowPowerCaptureCount |
USS_measurement_ULP_bias_delay | ulpBiasDelay |
USS_measurement_bias_impedance | biasImpedance |
Allows user to control bias channel bias impedance. More... | |
USS_measurement_mux_charge_pump | muxChargePumpMode |
Allows user to control multiplexer charge pump during capture. More... | |
uint16_t | startRxEnCount |
Contains USS SW Lib Measurement Configuration.
USS_measurement_capture_sequence _USS_Measurement_Configuration_::sequenceSelection |
USS_measurement_end_of_sequence_state _USS_Measurement_Configuration_::eofSequenceState |
USS_measurement_drive_strength _USS_Measurement_Configuration_::ch0DriveStrength |
Referenced by USS_updateSAPHConfiguration().
USS_measurement_drive_strength _USS_Measurement_Configuration_::ch1DriveStrength |
Referenced by USS_updateSAPHConfiguration().
USS_Pulse_Configuration* _USS_Measurement_Configuration_::pulseConfig |
uint_least16_t _USS_Measurement_Configuration_::startPPGCount |
This count determines the time to start the PPG pulse trigger. The count is based on 1 ASQ clock = (HSPLL_CLOCK_FREQ/16) period. For examples if startPPGCount = 15 and ASQ clock is 68 MHz, then PPG pulse will be triggered
(16/68MHz)*(1)*(startPPGCount) = (16/68MHz)*(1)*(15)= 3.52 usec, after
acquisiton sequence has been triggered.
"startPPGCount" valid range (0x0002 - 0xFFFF)
Registers modified: SAPH.ATM_A.TimeMarkA
Referenced by commonValidateSAPHconfigruation(), and USS_updateSAPHConfiguration().
uint_least16_t _USS_Measurement_Configuration_::turnOnADCCount |
This count determines the time to arm (turn on ADC). This count is based on 1 ASQ clock = (HSPLL_CLOCK_FREQ/16) period. For examples if turnOnADCCount = 15 and ASQ clock is 68 MHz, then ADC will be turned on
(1/ASQ_clock_freq)*(1)*(turnOnADCCount)= (1/68MHz)*(1)*(15) =0.22 usec,
after acquisiton sequence has been triggered.
"turnOnADCCount" valid range (0x0002 - 0xFFFF)
Registers modified: SAPH.ATM_B.TimeMarkB
Referenced by commonValidateSAPHconfigruation(), and USS_updateSAPHConfiguration().
uint_least16_t _USS_Measurement_Configuration_::startPGAandINBiasCount |
This count determines the time start the PGA and input biasing. This count is based on 1 ASQ clock = (HSPLL_CLOCK_FREQ/16) period. For examples if turnOnADCCount = 15 and ASQ clock is 68 MHz, then ADC will be turned on
(1/ASQ_clock_freq)*(1)*(turnOnADCCount)= (1/68MHz)*(1)*(15)=0.22 usec,
after acquisiton sequence has been triggered.
"turnOnADCCount" valid range (0x0002 - 0xFFFF)
Registers modified: SAPH.ATM_C.TimeMarkC
Referenced by commonValidateSAPHconfigruation(), and USS_updateSAPHConfiguration().
uint_least16_t _USS_Measurement_Configuration_::startADCsamplingCount |
This count determines the time to start the ADC acquisition. This count is based on 1 ASQ clock = (HSPLL_CLOCK_FREQ/16) period. For examples if turnOnADCCount = 15 and ASQ clock is 68 MHz, then ADC sampling will start
(1/ASQ_clock_freq)*(1)*(startADCsamplingCount) = (1/68MHz)*(1)*(15) = 0.22 usec
after acquisiton sequence has been triggered.
"startADCsamplingCount" valid range (0x0002 - 0xFFFF)
Registers modified: SAPH.ATM_D.TimeMarkD
Referenced by commonValidateSAPHconfigruation(), and USS_updateSAPHConfiguration().
uint_least16_t _USS_Measurement_Configuration_::restartCaptureCount |
This count determined the time to trigger next capture. This count is based on 16 ASQ clock= (HSPLL_CLOCK_FREQ/256) period. For examples if turnOnADCCount = 15 and ASQ clock is 68 MHz, then next capture will be triggered
(16/ASQ_clock_freq)*(16)*(startADCsamplingCount) = (16/68MHz)*(16)*(15) = 56.4 usec
after acquisiton sequence has been triggered.
"restartCaptureCount" valid range (0x0002 - 0xFFFF)
Registers modified: SAPH.ATM_E.TimeMarkE
Referenced by commonValidateSAPHconfigruation(), and USS_updateSAPHConfiguration().
uint_least16_t _USS_Measurement_Configuration_::captureTimeOutCount |
This count determined the time from start to acknowledge of acquisition data complete. This count is based on 4 ASQ clock = (HSPLL_CLOCK_FREQ/64) period. For examples if turnOnADCCount = 15 and ASQ clock is 68 MHz, then time out event will happen
(1/ASQ_clock_freq)*(64)*(startADCsamplingCount) = (16/68MHz)*(4)*(15) = 14.08 usec
after acquisiton sequence has been triggered.
"captureTimeOutCount" valid range (0x0002 - 0xFFFF)
Registers modified: SAPH.ATM_F.TimeMarkF
Referenced by commonValidateSAPHconfigruation(), and USS_updateSAPHConfiguration().
uint_least16_t _USS_Measurement_Configuration_::restartLowPowerCaptureCount |
This should be calculated using the following formula restartLowPowerCaptureCount=F1/F2*restartCaptureCnt where (F1=PLL/16, F2=32k)
Referenced by USS_startLowPowerUltrasonicCapture().
USS_measurement_ULP_bias_delay _USS_Measurement_Configuration_::ulpBiasDelay |
Allows user to specify delay between triggering an acquisition sequence and starting the acquisition sequence. This delay is used to allow PGA to settle.
Referenced by commonUpdateUSSULPbiasDelay(), and commonValidateSAPHconfigruation().
USS_measurement_bias_impedance _USS_Measurement_Configuration_::biasImpedance |
Allows user to control bias channel bias impedance.
Referenced by commonValidateSAPHconfigruation(), and USS_updateSAPHConfiguration().
USS_measurement_mux_charge_pump _USS_Measurement_Configuration_::muxChargePumpMode |
Allows user to control multiplexer charge pump during capture.
Referenced by commonValidateSAPHconfigruation(), and USS_updateSAPHConfiguration().
uint16_t _USS_Measurement_Configuration_::startRxEnCount |
This parameter is only required when controlling external AFE startRxEnCount are based of SMCLK cycles
Referenced by USS_configureUltrasonicMeasurement().