MSP430UltrasonicLibrary  02_30_00_03
Data Fields
_USS_SW_Library_configuration_ Struct Reference

Contains USS SW Lib configuration. More...

#include <ussSwLib.h>

Collaboration diagram for _USS_SW_Library_configuration_:
Collaboration graph
[legend]

Data Fields

USS_System_ConfigurationsystemConfig
 Pointer to USS_System_Configuration struct. More...
 
USS_Meter_ConfigurationmeterConfig
 Pointer to USS_Meter_Configuration struct. More...
 
USS_Measurement_ConfigurationmeasurementConfig
 Pointer to USS_Measurement_Configuration struct. More...
 
USS_HSPLL_ConfigurationpllConfiguration
 Pointer to USS_HSPLL_Configuration struct. More...
 
USS_Capture_ConfigurationcaptureConfig
 Pointer to USS_Capture_Configuration struct. More...
 
USS_Trigger_ConfigurationtriggerConfig
 Pointer to USS_Trigger_Configuration struct. More...
 
USS_Algorithms_User_ConfigurationalgorithmsConfig
 Pointer to USS_Algorithms_Configuration struct. More...
 
USS_Interrupt_ConfigurationinterruptConfig
 Pointer to USS_Interrupt_Configuration struct. More...
 
uint16_t validationKey
 

Detailed Description

Contains USS SW Lib configuration.

Field Documentation

§ systemConfig

USS_System_Configuration* _USS_SW_Library_configuration_::systemConfig

§ meterConfig

USS_Meter_Configuration* _USS_SW_Library_configuration_::meterConfig

Pointer to USS_Meter_Configuration struct.

Referenced by USS_scaleVolumeFlowRate().

§ measurementConfig

USS_Measurement_Configuration* _USS_SW_Library_configuration_::measurementConfig

§ pllConfiguration

USS_HSPLL_Configuration* _USS_SW_Library_configuration_::pllConfiguration

§ captureConfig

USS_Capture_Configuration* _USS_SW_Library_configuration_::captureConfig

§ triggerConfig

USS_Trigger_Configuration* _USS_SW_Library_configuration_::triggerConfig

Pointer to USS_Trigger_Configuration struct.

Referenced by USS_startUltrasonicMeasurement(), and USS_updateUUPSConfiguration().

§ algorithmsConfig

USS_Algorithms_User_Configuration* _USS_SW_Library_configuration_::algorithmsConfig

§ interruptConfig

USS_Interrupt_Configuration* _USS_SW_Library_configuration_::interruptConfig

Pointer to USS_Interrupt_Configuration struct.

Referenced by USS_updateUSSInterruptsConfiguration().

§ validationKey

uint16_t _USS_SW_Library_configuration_::validationKey

Validation Key (used when USS_SW_Library_configuration struct is loaded from non-volatile location)


The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale