MSP430UltrasonicLibrary  02_30_00_03
Data Fields
_USS_Measurement_Configuration_ Struct Reference

Contains USS SW Lib Measurement Configuration. More...

#include <ussSwLib.h>

Collaboration diagram for _USS_Measurement_Configuration_:
Collaboration graph
[legend]

Data Fields

uint8_t sequenceSelection
 
USS_measurement_end_of_sequence_state eofSequenceState
 
USS_measurement_drive_strength ch0DriveStrength
 
USS_measurement_drive_strength ch1DriveStrength
 
USS_Pulse_ConfigurationpulseConfig
 
uint_least16_t startPPGCount
 
uint_least16_t turnOnADCCount
 
uint_least16_t startPGAandINBiasCount
 
uint_least16_t startADCsamplingCount
 
uint_least16_t restartCaptureCount
 
uint_least16_t captureTimeOutCount
 
uint_least16_t restartLowPowerCaptureCount
 
USS_measurement_ULP_bias_delay ulpBiasDelay
 
USS_measurement_bias_impedance biasImpedance
 Allows user to control bias channel bias impedance. More...
 
USS_measurement_mux_charge_pump muxChargePumpMode
 Allows user to control multiplexer charge pump during capture. More...
 
uint16_t startRxEnCount
 

Detailed Description

Contains USS SW Lib Measurement Configuration.

Field Documentation

§ sequenceSelection

uint8_t _USS_Measurement_Configuration_::sequenceSelection

§ eofSequenceState

USS_measurement_end_of_sequence_state _USS_Measurement_Configuration_::eofSequenceState

§ ch0DriveStrength

USS_measurement_drive_strength _USS_Measurement_Configuration_::ch0DriveStrength

§ ch1DriveStrength

USS_measurement_drive_strength _USS_Measurement_Configuration_::ch1DriveStrength

§ pulseConfig

USS_Pulse_Configuration* _USS_Measurement_Configuration_::pulseConfig

§ startPPGCount

uint_least16_t _USS_Measurement_Configuration_::startPPGCount

This count determines the time to start the PPG pulse trigger. The count is based on 1 ASQ clock = (HSPLL_CLOCK_FREQ/16) period. For examples if startPPGCount = 15 and ASQ clock is 68 MHz, then PPG pulse will be triggered
(16/68MHz)*(1)*(startPPGCount) = (16/68MHz)*(1)*(15)= 3.52 usec, after
acquisiton sequence has been triggered.

"startPPGCount" valid range (0x0002 - 0xFFFF)

Registers modified: SAPH.ATM_A.TimeMarkA

Referenced by commonValidateSAPHconfigruation(), and USS_updateSAPHConfiguration().

§ turnOnADCCount

uint_least16_t _USS_Measurement_Configuration_::turnOnADCCount

This count determines the time to arm (turn on ADC). This count is based on 1 ASQ clock = (HSPLL_CLOCK_FREQ/16) period. For examples if turnOnADCCount = 15 and ASQ clock is 68 MHz, then ADC will be turned on
(1/ASQ_clock_freq)*(1)*(turnOnADCCount)= (1/68MHz)*(1)*(15) =0.22 usec,
after acquisiton sequence has been triggered.

"turnOnADCCount" valid range (0x0002 - 0xFFFF)

Registers modified: SAPH.ATM_B.TimeMarkB

Referenced by commonValidateSAPHconfigruation(), and USS_updateSAPHConfiguration().

§ startPGAandINBiasCount

uint_least16_t _USS_Measurement_Configuration_::startPGAandINBiasCount

This count determines the time start the PGA and input biasing. This count is based on 1 ASQ clock = (HSPLL_CLOCK_FREQ/16) period. For examples if turnOnADCCount = 15 and ASQ clock is 68 MHz, then ADC will be turned on
(1/ASQ_clock_freq)*(1)*(turnOnADCCount)= (1/68MHz)*(1)*(15)=0.22 usec,
after acquisiton sequence has been triggered.

"turnOnADCCount" valid range (0x0002 - 0xFFFF)

Registers modified: SAPH.ATM_C.TimeMarkC

Referenced by commonValidateSAPHconfigruation(), and USS_updateSAPHConfiguration().

§ startADCsamplingCount

uint_least16_t _USS_Measurement_Configuration_::startADCsamplingCount

This count determines the time to start the ADC acquisition. This count is based on 1 ASQ clock = (HSPLL_CLOCK_FREQ/16) period. For examples if turnOnADCCount = 15 and ASQ clock is 68 MHz, then ADC sampling will start
(1/ASQ_clock_freq)*(1)*(startADCsamplingCount) = (1/68MHz)*(1)*(15) = 0.22 usec
after acquisiton sequence has been triggered.

"startADCsamplingCount" valid range (0x0002 - 0xFFFF)

Registers modified: SAPH.ATM_D.TimeMarkD

Referenced by commonValidateSAPHconfigruation(), and USS_updateSAPHConfiguration().

§ restartCaptureCount

uint_least16_t _USS_Measurement_Configuration_::restartCaptureCount

This count determined the time to trigger next capture. This count is based on 16 ASQ clock= (HSPLL_CLOCK_FREQ/256) period. For examples if turnOnADCCount = 15 and ASQ clock is 68 MHz, then next capture will be triggered
(16/ASQ_clock_freq)*(16)*(startADCsamplingCount) = (16/68MHz)*(16)*(15) = 56.4 usec
after acquisiton sequence has been triggered.

"restartCaptureCount" valid range (0x0002 - 0xFFFF)

Registers modified: SAPH.ATM_E.TimeMarkE

Referenced by commonValidateSAPHconfigruation(), and USS_updateSAPHConfiguration().

§ captureTimeOutCount

uint_least16_t _USS_Measurement_Configuration_::captureTimeOutCount

This count determined the time from start to acknowledge of acquisition data complete. This count is based on 4 ASQ clock = (HSPLL_CLOCK_FREQ/64) period. For examples if turnOnADCCount = 15 and ASQ clock is 68 MHz, then time out event will happen
(1/ASQ_clock_freq)*(64)*(startADCsamplingCount) = (16/68MHz)*(4)*(15) = 14.08 usec
after acquisiton sequence has been triggered.

"captureTimeOutCount" valid range (0x0002 - 0xFFFF)

Registers modified: SAPH.ATM_F.TimeMarkF

Referenced by commonValidateSAPHconfigruation(), and USS_updateSAPHConfiguration().

§ restartLowPowerCaptureCount

uint_least16_t _USS_Measurement_Configuration_::restartLowPowerCaptureCount

This should be calculated using the following formula restartLowPowerCaptureCount=F1/F2*restartCaptureCnt where (F1=PLL/16, F2=32k)

Referenced by USS_startLowPowerUltrasonicCapture().

§ ulpBiasDelay

USS_measurement_ULP_bias_delay _USS_Measurement_Configuration_::ulpBiasDelay

Allows user to specify delay between triggering an acquisition sequence and starting the acquisition sequence. This delay is used to allow PGA to settle.

Referenced by commonUpdateUSSULPbiasDelay(), and commonValidateSAPHconfigruation().

§ biasImpedance

USS_measurement_bias_impedance _USS_Measurement_Configuration_::biasImpedance

Allows user to control bias channel bias impedance.

Referenced by commonValidateSAPHconfigruation(), and USS_updateSAPHConfiguration().

§ muxChargePumpMode

USS_measurement_mux_charge_pump _USS_Measurement_Configuration_::muxChargePumpMode

Allows user to control multiplexer charge pump during capture.

Referenced by commonValidateSAPHconfigruation(), and USS_updateSAPHConfiguration().

§ startRxEnCount

uint16_t _USS_Measurement_Configuration_::startRxEnCount

This parameter is only required when controlling external AFE startRxEnCount are based of SMCLK cycles

Referenced by USS_configureUltrasonicMeasurement().


The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale