128 #ifndef ti_display_DisplayUart__include
129 #define ti_display_DisplayUart__include
131 #include <ti/drivers/dpl/SemaphoreP.h>
137 #ifndef DisplayUart_fxnTable
138 # define DisplayUart_fxnTable DisplayUartMin_fxnTable
142 #define DisplayUart_SCROLLING 0xFF
182 uint8_t column,
char *fmt, va_list va);
184 uint8_t column,
char *fmt, va_list va);
const Display_FxnTable DisplayUartMin_fxnTable
SemaphoreP_Handle mutex
Definition: DisplayUart.h:160
unsigned int DisplayUartMin_getType(void)
void DisplayUartMin_clear(Display_Handle handle)
char * lineClearSeq
Definition: DisplayUart.h:161
const Display_FxnTable DisplayUartAnsi_fxnTable
void DisplayUartAnsi_vprintf(Display_Handle handle, uint8_t line, uint8_t column, char *fmt, va_list va)
void DisplayUartAnsi_clear(Display_Handle handle)
unsigned int mutexTimeout
Definition: DisplayUart.h:151
Display Parameters.
Definition: Display.h:442
UART Global configuration.
Definition: UART.h:691
Definition: DisplayUart.h:157
void DisplayUartAnsi_clearLines(Display_Handle handle, uint8_t fromLine, uint8_t toLine)
struct DisplayUart_Object * DisplayUart_Handle
Generic interface for text output.
void DisplayUartMin_clearLines(Display_Handle handle, uint8_t fromLine, uint8_t toLine)
unsigned int uartIdx
Definition: DisplayUart.h:149
void DisplayUartAnsi_init(Display_Handle handle)
char * strBuf
Definition: DisplayUart.h:152
Definition: DisplayUart.h:147
unsigned int DisplayUartAnsi_getType(void)
uint16_t strBufLen
Definition: DisplayUart.h:153
UART_Handle hUart
Definition: DisplayUart.h:159
void DisplayUartMin_vprintf(Display_Handle handle, uint8_t line, uint8_t column, char *fmt, va_list va)
unsigned int baudRate
Definition: DisplayUart.h:150
The definition of a Display function table that contains the required set of functions to control a s...
Definition: Display.h:501
int DisplayUartAnsi_control(Display_Handle handle, unsigned int cmd, void *arg)
void DisplayUartMin_init(Display_Handle handle)
void DisplayUartMin_close(Display_Handle)
Display_Handle DisplayUartAnsi_open(Display_Handle, Display_Params *params)
int DisplayUartMin_control(Display_Handle handle, unsigned int cmd, void *arg)
Display_Handle DisplayUartMin_open(Display_Handle, Display_Params *params)
Display Global configuration.
Definition: Display.h:524
struct DisplayUart_HWAttrs DisplayUart_HWAttrs
void DisplayUartAnsi_close(Display_Handle)
struct DisplayUart_Object DisplayUart_Object