33 #ifndef ti_display_DisplayHost__include
34 #define ti_display_DisplayHost__include
66 uint8_t column,
char *fmt, va_list va);
void DisplayHost_clear(Display_Handle handle)
unsigned int DisplayHost_getType(void)
int dummy
Definition: DisplayHost.h:51
uint16_t strBufLen
Definition: DisplayHost.h:46
Definition: DisplayHost.h:49
Display Parameters.
Definition: Display.h:442
void DisplayHost_vprintf(Display_Handle handle, uint8_t line, uint8_t column, char *fmt, va_list va)
struct DisplayHost_HWAttrs DisplayHost_HWAttrs
Display_Handle DisplayHost_open(Display_Handle, Display_Params *params)
Generic interface for text output.
Definition: DisplayHost.h:43
struct DisplayHost_Object DisplayHost_Object
The definition of a Display function table that contains the required set of functions to control a s...
Definition: Display.h:501
struct DisplayHost_Object * DisplayHost_Handle
void DisplayHost_clearLines(Display_Handle handle, uint8_t fromLine, uint8_t toLine)
char * strBuf
Definition: DisplayHost.h:45
Display Global configuration.
Definition: Display.h:524
void DisplayHost_close(Display_Handle)
const Display_FxnTable DisplayHost_fxnTable
int DisplayHost_control(Display_Handle handle, unsigned int cmd, void *arg)
void DisplayHost_init(Display_Handle handle)