187 #ifndef ti_display_Display__include
188 #define ti_display_Display__include
209 #define Display_Type_ANY 0xFFFFFFFF
210 #define Display_Type_INVALID 0x00000000
211 #define Display_Type_LCD 0x80000000
212 #define Display_Type_UART 0x40000000
213 #define Display_Type_LOG 0x20000000
214 #define Display_Type_ITM 0x10000000
215 #define Display_Type_HOST 0x08000000
216 #define Display_Type_ANSI 0x04000000
217 #define Display_Type_GRLIB 0x00100000
221 #define Display_MAXINDEX 15
240 #define DISPLAY_CMD_RESERVED 32
254 #define DISPLAY_STATUS_RESERVED -32
269 #define DISPLAY_STATUS_SUCCESS 0
277 #define DISPLAY_STATUS_ERROR -1
286 #define DISPLAY_STATUS_UNDEFINEDCMD -2
307 #define DISPLAY_CMD_TRANSPORT_CLOSE 0
317 #define DISPLAY_CMD_TRANSPORT_OPEN 1
326 #define Display_clearLine(handle, n) Display_clearLines(handle, n, 0)
327 #define Display_isIndex(i) (i <= Display_MAXINDEX)
328 #define Display_isMetaType(i) (i > Display_MAXINDEX)
330 #if !defined(Display_DISABLE_ALL) || (!Display_DISABLE_ALL)
333 # define Display_init() \
337 # define Display_open(id, params) \
338 Display_doOpen(id, params)
341 # define Display_Params_init(params) \
342 Display_doParamsInit(params)
345 # define Display_clear(handle) \
346 Display_doClear(handle)
349 # define Display_clearLines(handle, fromLine, toLine) \
350 Display_doClearLines(handle, fromLine, toLine)
353 # define Display_printf Display_doPrintf
356 # define Display_print0(handle, line, col, fmt) \
357 Display_printf(handle, line, col, fmt)
360 # define Display_print1(handle, line, col, fmt, a0) \
361 Display_printf(handle, line, col, fmt, a0)
364 # define Display_print2(handle, line, col, fmt, a0, a1) \
365 Display_printf(handle, line, col, fmt, a0, a1)
368 # define Display_print3(handle, line, col, fmt, a0, a1, a2) \
369 Display_printf(handle, line, col, fmt, a0, a1, a2)
372 # define Display_print4(handle, line, col, fmt, a0, a1, a2, a3) \
373 Display_printf(handle, line, col, fmt, a0, a1, a2, a3)
376 # define Display_print5(handle, line, col, fmt, a0, a1, a2, a3, a4) \
377 Display_printf(handle, line, col, fmt, a0, a1, a2, a3, a4)
380 # define Display_getType(handle) \
381 Display_doGetType(handle)
384 # define Display_control(handle, cmd, arg) \
385 Display_doControl(handle, cmd, arg)
388 # define Display_close(handle) \
389 Display_doClose(handle)
391 # define Display_init()
392 # define Display_open(id, params) NULL
393 # define Display_Params_init(params)
394 # define Display_clear(handle)
395 # define Display_clearLines(handle, fromLine, toLine)
396 # define Display_printf(handle, line, col, fmt, ...)
397 # define Display_print0(handle, line, col, fmt)
398 # define Display_print1(handle, line, col, fmt, a0)
399 # define Display_print2(handle, line, col, fmt, a0, a1)
400 # define Display_print3(handle, line, col, fmt, a0, a1, a2)
401 # define Display_print4(handle, line, col, fmt, a0, a1, a2, a3)
402 # define Display_print5(handle, line, col, fmt, a0, a1, a2, a3, a4)
403 # define Display_getType(handle) Display_Type_INVALID
404 # define Display_control(handle, cmd, arg) NULL
405 # define Display_close(handle)
681 #endif //ti_display_Display__include
void Display_doClose(Display_Handle handle)
Closes selected Display implementations.
Display_vprintfFxn vprintfFxn
Definition: Display.h:507
struct Display_Config * Display_Handle
A handle for specific Display implementations.
Definition: Display.h:415
struct Display_Config Display_Config
Display Global configuration.
void(* Display_clearLinesFxn)(Display_Handle handle, uint8_t fromLine, uint8_t toLine)
A function pointer to a specific implementation of Display_clearLines().
Definition: Display.h:463
void Display_doParamsInit(Display_Params *params)
Initializes parameter structure with default parameters.
void * object
Definition: Display.h:530
void Display_doInit(void)
Function to initializes the Display driver.
Display_Handle(* Display_openFxn)(Display_Handle handle, Display_Params *params)
A function pointer to a specific implementation of Display_open().
Definition: Display.h:451
unsigned int(* Display_getTypeFxn)(void)
A function pointer to a specific implementation of Display_getType().
Definition: Display.h:494
void Display_doClear(Display_Handle handle)
Calls the clear fxn of all opened Display implementations.
Display Parameters.
Definition: Display.h:442
void const * hwAttrs
Definition: Display.h:533
uint32_t Display_doGetType(Display_Handle handle)
Gets the type of display for the handle.
Definition: Display.h:428
void Display_doControl(Display_Handle handle, unsigned int cmd, void *arg)
Function performs implementation specific features on a given Display_Handle.
Display_clearFxn clearFxn
Definition: Display.h:505
Display_controlFxn controlFxn
Definition: Display.h:509
void(* Display_vprintfFxn)(Display_Handle handle, uint8_t line, uint8_t column, char *fmt, va_list va)
A function pointer to a specific implementation of Display_vprintf().
Definition: Display.h:471
void Display_doPrintf(Display_Handle handle, uint8_t line, uint8_t column, char *fmt,...)
Calls the output function of all opened Display implementations.
void(* Display_clearFxn)(Display_Handle handle)
A function pointer to a specific implementation of Display_clear().
Definition: Display.h:457
Display_initFxn initFxn
Definition: Display.h:503
Definition: Display.h:430
The definition of a Display function table that contains the required set of functions to control a s...
Definition: Display.h:501
Display_openFxn openFxn
Definition: Display.h:504
void(* Display_initFxn)(Display_Handle handle)
A function pointer to a specific implementation of Display_initFxn().
Definition: Display.h:421
Definition: Display.h:429
Display_getTypeFxn getTypeFxn
Definition: Display.h:510
void Display_doClearLines(Display_Handle handle, uint8_t fromLine, uint8_t toLine)
Calls the clearLines fxn of all opened Display implementations.
struct Display_FxnTable Display_FxnTable
The definition of a Display function table that contains the required set of functions to control a s...
Display_LineClearMode lineClearMode
Definition: Display.h:444
Display_Handle Display_doOpen(uint32_t id, Display_Params *params)
Initialize all the selected Display implementations.
Display Global configuration.
Definition: Display.h:524
struct Display_Params Display_Params
Display Parameters.
Display_FxnTable const * fxnTablePtr
Definition: Display.h:527
int(* Display_controlFxn)(Display_Handle handle, unsigned int cmd, void *arg)
A function pointer to a driver specific implementation of Display_control().
Definition: Display.h:487
Display_closeFxn closeFxn
Definition: Display.h:508
Display_LineClearMode
How to treat existing elements on a line when writing text.
Definition: Display.h:426
Definition: Display.h:431
Display_clearLinesFxn clearLinesFxn
Definition: Display.h:506
void(* Display_closeFxn)(Display_Handle)
A function pointer to a specific implementation of Display_close().
Definition: Display.h:481