Speech Recognizer Project API Guide
v
|
Build-time configuration parameters that specify what functions and capabilities were included when the MinHMM Library was built. More...
Macros | |
#define | MINHMM_FILEIO (0) |
Configure capabiliity to read and write models from/to files. More... | |
Build-time configuration parameters that specify what functions and capabilities were included when the MinHMM Library was built.
#define MINHMM_FILEIO (0) |
Configure capabiliity to read and write models from/to files.
If MINHMM_FILEIO != 0 then the library provides functions to read and write model data from/to files.