Speech Recognizer Project API Guide
v
|
The MinHMM API is the top-level API. More...
Modules | |
MinHMM Configuration | |
Build-time configuration parameters that specify what functions and capabilities were included when the MinHMM Library was built. | |
MinHMM Memory Allocation Defines | |
Macro definitions that the application uses to allocate memory for MinHMM. | |
MinHMM Structs and Types | |
Structures and types used in performing the tasks of the top-level user interface functions of MinHMM. | |
MinHMM User Functions | |
The top-level user interface functions within MinHMM. | |
The MinHMM API is the top-level API.
It contains the structures, types, and functions provided to use the MinHMM recognizer.