Build date: 02282020
MSP430 Driver Library is a collection of high level APIs that speed up software development for MSP430. The MSP430 Driver Library package includes API documentaion and examples to help you get started.
This release of MSP430 Driver Library supports all of the following device families:
MSP430 Driver Library is available as a standalone BSD released package. To use the library simply download and unzip the package below. Please read the included user's guide to learn about adding driver library to a new or existing project.
MSP430 Driver Library is also released as a component of MSP430Ware. You can import and run examples from driver library from the TI Resouce Explorer GUI within the Code Composer Studio (CCS) window when you have MSP430Ware installed. For more information about MSP430Ware check the table below for a link to the latest version.
What is the difference between MSP430Ware and Driver Library?MSP430Ware is a collection of MSP430 software and tools. One of the main components of MSP430Ware is Driver Library (DriverLib).
Why are there multiple driverlib folders within MSP430Ware?MSP430Ware contains many different software libraries and projects. Some of these components depend on a specific version of Driver Library. Each component ships the version of Driver Library they tested with to ensure that all software works for you out of the box.
Can I have multiple versions of MSP430Ware installed?Yes! MSP430Ware installations can exist alongside each other. You should only see the latest installed version within the TI Resource Explorer window of Code Composer Studio however.
How can I get support for MSP430Ware?Feel free to use the TI E2E forum to ask anything MSP430Ware related.
Fill in Form. Approved users receive download URL in 1 minute.
Fill in Form. TI will contact you in 1-2+ business days.