MSP DSP Library
|
Parameter structure for Q15 split operation. More...
#include <DSPLib_transform.h>
Data Fields | |
uint16_t | length |
const _q15 * | twiddleTable |
Parameter structure for Q15 split operation.
uint16_t msp_split_q15_params::length |
Length of the source data, must be a power of two.
const _q15* msp_split_q15_params::twiddleTable |
Pointer to the twiddle coefficient table with size greater than or equal to the source length. When using LEA this can be a NULL pointer.