![]() |
![]() |
GPIO driver implementation for CC26xx/CC13xx devices.
============================================================================
The GPIO header file should be included in an application as follows:
Refer to GPIO.h for a complete description of the GPIO driver APIs provided and examples of their use.
In order to use the GPIO APIs, the application is required to provide 3 structures in the Board.c file:
Go to the source code of this file.
Data Structures | |
| struct | GPIOCC26XX_Config |
| GPIO device specific driver configuration structure. More... | |
Macros | |
Device specific GPIO port/pin identifiers to be used within the board's GPIO_PinConfig table. | |
| #define | GPIOCC26XX_EMPTY_PIN |
| #define | GPIOCC26XX_DIO_00 |
| #define | GPIOCC26XX_DIO_01 |
| #define | GPIOCC26XX_DIO_02 |
| #define | GPIOCC26XX_DIO_03 |
| #define | GPIOCC26XX_DIO_04 |
| #define | GPIOCC26XX_DIO_05 |
| #define | GPIOCC26XX_DIO_06 |
| #define | GPIOCC26XX_DIO_07 |
| #define | GPIOCC26XX_DIO_08 |
| #define | GPIOCC26XX_DIO_09 |
| #define | GPIOCC26XX_DIO_10 |
| #define | GPIOCC26XX_DIO_11 |
| #define | GPIOCC26XX_DIO_12 |
| #define | GPIOCC26XX_DIO_13 |
| #define | GPIOCC26XX_DIO_14 |
| #define | GPIOCC26XX_DIO_15 |
| #define | GPIOCC26XX_DIO_16 |
| #define | GPIOCC26XX_DIO_17 |
| #define | GPIOCC26XX_DIO_18 |
| #define | GPIOCC26XX_DIO_19 |
| #define | GPIOCC26XX_DIO_20 |
| #define | GPIOCC26XX_DIO_21 |
| #define | GPIOCC26XX_DIO_22 |
| #define | GPIOCC26XX_DIO_23 |
| #define | GPIOCC26XX_DIO_24 |
| #define | GPIOCC26XX_DIO_25 |
| #define | GPIOCC26XX_DIO_26 |
| #define | GPIOCC26XX_DIO_27 |
| #define | GPIOCC26XX_DIO_28 |
| #define | GPIOCC26XX_DIO_29 |
| #define | GPIOCC26XX_DIO_30 |
| #define | GPIOCC26XX_DIO_31 |
Typedefs | |
| typedef struct GPIOCC26XX_Config | GPIOCC26XX_Config |
| GPIO device specific driver configuration structure. More... | |
Functions | |
| void | GPIOCC26xx_release (int index) |
| Un-oonfigure a GPIO pin. More... | |
| typedef struct GPIOCC26XX_Config GPIOCC26XX_Config |
GPIO device specific driver configuration structure.
The device specific GPIOCC26XX_Config structure that tells the GPIO driver where the two aforementioned arrays are and the number of elements in each. The interrupt priority of all pins configured to generate interrupts is also specified here. Values for the interrupt priority are device-specific. You should be well-acquainted with the interrupt controller used in your device before setting this parameter to a non-default value. The sentinel value of (~0) (the default value) is used to indicate that the lowest possible priority should be used.
Below is an example of an initialized GPIOCC26XX_Config structure:
| void GPIOCC26xx_release | ( | int | index | ) |
Un-oonfigure a GPIO pin.
Disables pin interrupt, clears callback, restores pin to default setting, removes pin from PIN object
| index | GPIO index |