65 #ifndef TIVX_TENSOR_H_ 66 #define TIVX_TENSOR_H_ 89 VX_TYPE_TENSOR = 0x815,
95 enum vx_ext_context_attribute_e {
VX_API_ENTRY vx_status VX_API_CALL vxReleaseTensor(vx_tensor *tensor)
Releases a reference to a tensor data object. The object may not be garbage collected until its total...
fixed point position of the scaling divisor Read-Write.
struct _vx_context * vx_context
fixed point position when the input element type is integer. Read-Write.
VX_API_ENTRY vx_status VX_API_CALL vxSetTensorAttribute(vx_tensor tensor, vx_enum attribute, const void *ptr, vx_size size)
Sets attributes of a tensor object.
VX_API_ENTRY vx_status VX_API_CALL vxQueryTensor(vx_tensor tensor, vx_enum attribute, void *ptr, vx_size size)
Retrieves various attributes of a tensor data.
#define VX_ATTRIBUTE_BASE(vendor, object)
scaling divisor to be applied to each element when the input element type is integer. Read-Write.
vx_tensor_attribute_e
tensor Data attributes.
tensor Data element data type. vx_type_e
VX_API_ENTRY vx_status VX_API_CALL tivxUnmapTensorPatch(vx_tensor tensor, vx_map_id map_id)
Unmap and commit potential changes to a tensor object patch that were previously mapped. Unmapping a tensor patch invalidates the memory location from which the patch could be accessed by the application. Accessing this memory location after the unmap function completes has an undefined behavior.
VX_API_ENTRY vx_tensor VX_API_CALL vxCreateTensor(vx_context context, vx_size number_of_dims, const vx_size *dims, vx_enum data_type, vx_int8 fixed_point_position)
Creates an opaque reference to a tensor data buffer.
VX_API_ENTRY vx_status VX_API_CALL tivxMapTensorPatch(vx_tensor tensor, vx_size number_of_dims, const vx_size *view_start, const vx_size *view_end, vx_map_id *map_id, vx_size *stride, void **ptr, vx_enum usage, vx_enum mem_type)
Allows the application to get direct access to a patch of tensor object.
VX_API_ENTRY vx_status VX_API_CALL vxCopyTensorPatch(vx_tensor tensor, vx_size number_of_dims, const vx_size *view_start, const vx_size *view_end, const vx_size *user_stride, void *user_ptr, vx_enum usage, vx_enum user_memory_type)
Allows the application to copy a view patch from/into an tensor object .
struct _vx_tensor * vx_tensor
The multidimensional data object (Tensor).
vx_status(* VX_API_CALL)(vx_reference *ref)
Callback type used to register release callbacks from object derived from references.