![]() |
TIOVX User Guide
|
Interface to kernel APIs on target. More...
#include <TI/tivx_obj_desc.h>
Go to the source code of this file.
Typedefs | |
typedef struct _tivx_target_kernel * | tivx_target_kernel |
Handle to kernel on a target. | |
typedef struct _tivx_target_kernel_instance * | tivx_target_kernel_instance |
Handle to instance of kernel on a target. | |
typedef vx_status(VX_CALLBACK * | tivx_target_kernel_f) (tivx_target_kernel_instance kernel, tivx_obj_desc_t *obj_desc[], uint16_t num_params, void *priv_arg) |
The target kernel callback. More... | |
typedef vx_status(VX_CALLBACK * | tivx_target_kernel_control_f) (tivx_target_kernel_instance kernel, uint32_t node_cmd_id, tivx_obj_desc_t *obj_desc[], uint16_t num_params, void *priv_arg) |
The target kernel callback for control command. More... | |
Functions | |
VX_API_ENTRY tivx_target_kernel VX_API_CALL | tivxAddTargetKernel (vx_enum kernel_id, const char *target_name, tivx_target_kernel_f process_func, tivx_target_kernel_f create_func, tivx_target_kernel_f delete_func, tivx_target_kernel_control_f control_func, void *priv_arg) |
Allows users to add native kernels implementation to specific targets. More... | |
VX_API_ENTRY tivx_target_kernel VX_API_CALL | tivxAddTargetKernelByName (const char *kernel_name, const char *target_name, tivx_target_kernel_f process_func, tivx_target_kernel_f create_func, tivx_target_kernel_f delete_func, tivx_target_kernel_control_f control_func, void *priv_arg) |
Allows users to add native kernels implementation to specific targets. More... | |
VX_API_ENTRY vx_status VX_API_CALL | tivxRemoveTargetKernel (tivx_target_kernel target_kernel) |
Allows users to remove native kernels implementation to specific targets. | |
VX_API_ENTRY vx_status VX_API_CALL | tivxQueryNumTargetKernel (vx_uint32 *ptr) |
Queries the framework to determine the number of target kernels on the target from which it is called. More... | |
VX_API_ENTRY vx_status VX_API_CALL | tivxSetTargetKernelInstanceContext (tivx_target_kernel_instance target_kernel_instance, void *kernel_context, uint32_t kernel_context_size) |
Associate a kernel function context or handle with a target kernel instance. More... | |
VX_API_ENTRY vx_status VX_API_CALL | tivxGetTargetKernelInstanceContext (tivx_target_kernel_instance target_kernel_instance, void **kernel_context, uint32_t *kernel_context_size) |
Get a kernel function context or handle with a target kernel instance. More... | |
VX_API_ENTRY vx_status VX_API_CALL | tivxGetTargetKernelInstanceState (tivx_target_kernel_instance target_kernel_instance, vx_enum *state) |
Get a kernel state with a target kernel instance. More... | |
VX_API_ENTRY vx_status VX_API_CALL | tivxGetTargetKernelTargetId (tivx_target_kernel_instance target_kernel_instance, uint32_t *targetId) |
Get a kernel target id with a target kernel instance. More... | |
VX_API_ENTRY void | tivxGetTargetKernelInstanceBorderMode (tivx_target_kernel_instance target_kernel_instance, vx_border_t *border_mode) |
Get the border mode for the target kernel instance. More... | |
VX_API_ENTRY vx_bool | tivxIsTargetKernelInstanceReplicated (tivx_target_kernel_instance kernel_instance) |
Checks if supplied node is replicated. Returns vx_true if the given node is replicated and vx_false if not. | |
tivx_target_kernel | tivxTargetKernelInstanceGetKernel (tivx_target_kernel_instance target_kernel_instance) |
Get target kernel for a given target kernel instance. | |
static vx_bool | tivxFlagIsBitSet (uint32_t flag_var, uint32_t flag_val) |
Macro to check if flag is set, flag MUST be of bit type. | |
static void | tivxFlagBitSet (volatile uint32_t *flag_var, uint32_t flag_val) |
Macro to set flag value, flag MUST be of bit type. | |
static void | tivxFlagBitClear (volatile uint32_t *flag_var, uint32_t flag_val) |
Macro to clear flag value, flag MUST be of bit type. | |
void | tivxLogRtTraceKernelInstanceAddEvent (vx_node node, uint16_t event_index, char *event_name) |
Add real-time log event in host side initialize callback for user kernel. More... | |
void | tivxLogRtTraceKernelInstanceRemoveEvent (vx_node node, uint16_t event_index) |
Remove real-time log event in host side deinitilize callback for user kernel. More... | |
void | tivxLogRtTraceKernelInstanceExeStart (tivx_target_kernel_instance kernel, uint16_t event_index) |
Log trace on target kernel instance execute start. More... | |
void | tivxLogRtTraceKernelInstanceExeEnd (tivx_target_kernel_instance kernel, uint16_t event_index) |
Log trace on target kernel instance execute end. More... | |
void | tivxLogRtTraceKernelInstanceExeStartTimestamp (tivx_target_kernel_instance kernel, uint16_t event_index, uint64_t timestamp) |
Log trace on target kernel instance execute start with timestamp given externally. More... | |
void | tivxLogRtTraceKernelInstanceExeEndTimestamp (tivx_target_kernel_instance kernel, uint16_t event_index, uint64_t timestamp) |
Log trace on target kernel instance execute end with timestamp given externally. More... | |
Interface to kernel APIs on target.
Definition in file tivx_target_kernel.h.