TIOVX User Guide
tiovx.enums.DfImage Class Reference

Image data format (OpenVX equivalent = vx_df_image_e) More...

Inherits Enum.

Static Public Attributes

int INVALID = 0
 Place holder for invalid data format.
 
int VIRT = 1
 OpenVX equivalent = VX_DF_IMAGE_VIRT.
 
int RGB = 2
 OpenVX equivalent = VX_DF_IMAGE_RGB.
 
int RGBX = 3
 OpenVX equivalent = VX_DF_IMAGE_RGBX.
 
int NV12 = 4
 OpenVX equivalent = VX_DF_IMAGE_NV12.
 
int NV21 = 5
 OpenVX equivalent = VX_DF_IMAGE_NV21.
 
int UYVY = 6
 OpenVX equivalent = VX_DF_IMAGE_UYVY.
 
int YUYV = 7
 OpenVX equivalent = VX_DF_IMAGE_YUYV.
 
int IYUV = 8
 OpenVX equivalent = VX_DF_IMAGE_IYUV.
 
int YUV4 = 9
 OpenVX equivalent = VX_DF_IMAGE_YUV4.
 
int U8 = 10
 OpenVX equivalent = VX_DF_IMAGE_U8.
 
int U16 = 11
 OpenVX equivalent = VX_DF_IMAGE_U16.
 
int S16 = 12
 OpenVX equivalent = VX_DF_IMAGE_S16.
 
int U32 = 13
 OpenVX equivalent = VX_DF_IMAGE_U32.
 
int S32 = 14
 OpenVX equivalent = VX_DF_IMAGE_S32.
 
int P12 = 15
 OpenVX equivalent = TIVX_DF_IMAGE_P12.
 
int NV12_P12 = 16
 OpenVX equivalent = TIVX_DF_IMAGE_NV12_P12.
 
int RGB565 = 17
 OpenVX equivalent = TIVX_DF_IMAGE_RGB565.
 
int BGRX = 18
 OpenVX equivalent = TIVX_DF_IMAGE_BGRX.
 

Detailed Description

Image data format (OpenVX equivalent = vx_df_image_e)

Example usage:
DfImage.VIRT
DfImage.U8

Definition at line 263 of file enums.py.


The documentation for this class was generated from the following file: