![]() |
TIOVX User Guide
|
APIs for application interface accessible only on host.
Modules | |
| Super Node Framework Type APIs | |
| APIs creating and using super node framework type. | |
| Kernel Helper APIs | |
| Helper APIs used used for host side kernel validation. | |
| Utility APIs | |
| Utility APIs available for the application running on the host. | |
| Platform OSAL APIs | |
| Platform operating system abstraction layer on the host. | |
| Debug APIs | |
| APIs for debug operations on the host. | |
| Real-time Trace APIs | |
| APIs for real-time event trace operations on the host. | |
| Tensor Data Type APIs | |
| APIs creating and using tensor data type (note: this is not included in OpenVX 1.1 and thus added to TI extensions) | |
| Raw Image Data Type APIs | |
| APIs creating and using raw image data type. | |
| Node APIs | |
| TIOVX APIs for node operations in the processing graph. | |
| Reference APIs | |
| APIs for handling references, handles, and data pointers. | |
| Graph APIs | |
| APIs for querying and manipulating the OpenVX graph. | |
| Kernel APIs | |
| APIs for working with compute kernels, target selection, and execution control. | |
| Attribute Extension APIs | |
| TI attribute extensions for OpenVX objects. | |
Defines | |
| #define | TIVX_TARGET_MAX_NAME (64u) |
| Max possible name of a target. | |
| #define | TIVX_TARGET_HOST "HOST" |
| String to name a OpenVX Host. More... | |
| #define | TIVX_CONFIG_PATH_LENGTH (512u) |
| Max size of config file path. | |
| #define | dimof(x) (sizeof(x)/sizeof(x[0])) |
| Macro to find size of array. | |
Enumerations | |
| enum | tivx_df_image_e { TIVX_DF_IMAGE_P12 = VX_DF_IMAGE('P','0','1','2'), TIVX_DF_IMAGE_NV12_P12 = VX_DF_IMAGE('N','1','2','P'), TIVX_DF_IMAGE_RGB565 = VX_DF_IMAGE('R','5','6','5'), TIVX_DF_IMAGE_BGRX = VX_DF_IMAGE('B','G','R','A') } |
| Based on the VX_DF_IMAGE definition. More... | |
| enum | tivx_status_e { TIVX_STATUS_BASE = -(vx_int32)100 } |
| The enumeration of all TIVX operational error codes. More... | |
| enum | tivx_cpu_id_e { TIVX_CPU_ID_DSP1 = 0, TIVX_CPU_ID_DSP2 = 1, TIVX_CPU_ID_DSP_C7_1 = 2, TIVX_CPU_ID_MCU2_0 = 3, TIVX_CPU_ID_VPAC1 = TIVX_CPU_ID_MCU2_0, TIVX_CPU_ID_VIDEO_IO = TIVX_CPU_ID_MCU2_0, TIVX_CPU_ID_MCU2_1 = 4, TIVX_CPU_ID_DMPAC = TIVX_CPU_ID_MCU2_1, TIVX_CPU_ID_MPU_0 = 5, TIVX_CPU_ID_MCU3_0 = 6, TIVX_CPU_ID_MCU3_1 = 7, TIVX_CPU_ID_MAX = 8, TIVX_CPU_ID_INVALID = 0xFF } |
| CPU ID for supported CPUs. More... | |
Functions | |
| void | tivxInit (void) |
| Function to initialize OpenVX framework. More... | |
| void | tivxDeInit (void) |
| Function to de-initialize OpenVX framework. More... | |
| void | tivxHostInit (void) |
| Function to initialize OpenVX HOST side functionality. More... | |
| void | tivxHostDeInit (void) |
| Function to de-initialize OpenVX HOST side functionality. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | tivxRegisterModule (const char *name, vx_publish_kernels_f publish, vx_unpublish_kernels_f unpublish) |
| Register publish and unpublish functions against a module name. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | tivxUnRegisterModule (const char *name) |
| UnRegister publish and unpublish functions if previously registered. More... | |
| vx_enum | tivxGetSelfCpuId (void) |
| Return CPU ID of the CPU on which this API is called. More... | |
| vx_bool | tivxIsTargetEnabled (const char target_name[]) |
| Utility function to know if target is enabled or not. More... | |
| uint64_t | tivxPlatformGetTimeInUsecs (void) |
| Get the time in micro seconds. More... | |
| #define TIVX_TARGET_HOST "HOST" |
| enum tivx_df_image_e |
Based on the VX_DF_IMAGE definition.
vx_df_image to contain these values. | enum tivx_status_e |
| enum tivx_cpu_id_e |
CPU ID for supported CPUs.
CPU ID is defined in platform module since depending on platform the CPUs could be different
Current CPU IDs are defined assuming J721E SoC
Caution: This enum is used as index into the array #g_ipc_cpu_id_map, so change in this enum will require change in this array as well.
Definition at line 343 of file tivx_soc_j721e.h.
| void tivxInit | ( | void | ) |
Function to initialize OpenVX framework.
Should be called during system init on all OpenVX HOST as well as OpenVX target CPUs
NOTE: In Vision SDK, this function is called during VIsion SDK system init so user need not call this explicitly
| void tivxDeInit | ( | void | ) |
Function to de-initialize OpenVX framework.
Should be called during system init on all OpenVX HOST as well as OpenVX target CPUs
NOTE: In Vision SDK, this function is called during VIsion SDK system init so user need not call this explicitly
| void tivxHostInit | ( | void | ) |
Function to initialize OpenVX HOST side functionality.
Should be called during system init after tivxInit() on HOST CPUs only
NOTE: In Vision SDK, this function is called during VIsion SDK system init so user need not call this explicitly
| void tivxHostDeInit | ( | void | ) |
Function to de-initialize OpenVX HOST side functionality.
Should be called during system init before tivxDeInit() on HOST CPUs only
NOTE: In Vision SDK, this function is called during VIsion SDK system init so user need not call this explicitly
| VX_API_ENTRY vx_status VX_API_CALL tivxRegisterModule | ( | const char * | name, |
| vx_publish_kernels_f | publish, | ||
| vx_unpublish_kernels_f | unpublish | ||
| ) |
Register publish and unpublish functions against a module name.
These functions are invoked when vxLoadKernels is called with the registered name.
This is alternative instead of dynamically loading kernels during vxLoadKernels
Duplicate module names not checked by this API.
API is not reentrant, user is recommended to call all tivxRegisterModule during system init before vxCreateContext() from a single thread.
Modules registered against TIVX_MODULE_NAME are called during vxCreateContext so user MUST ensure tivxRegisterModule() is called for TIVX_MODULE_NAME module
| VX_API_ENTRY vx_status VX_API_CALL tivxUnRegisterModule | ( | const char * | name | ) |
UnRegister publish and unpublish functions if previously registered.
| [in] | name | Module name to unregister |
vx_status_e enumeration. | VX_SUCCESS | No errors. |
| VX_FAILURE | Unable to find module "name" in list of registered modules |
| vx_enum tivxGetSelfCpuId | ( | void | ) |
Return CPU ID of the CPU on which this API is called.
vx_emum enumeration of the CPU_ID. | vx_bool tivxIsTargetEnabled | ( | const char | target_name[] | ) |
Utility function to know if target is enabled or not.
| [in] | target_name | String specifying the target name |
vx_bool value. | vx_true_e | The target is enabled |
| vx_false_e | The target is not enabled |
| uint64_t tivxPlatformGetTimeInUsecs | ( | void | ) |
Get the time in micro seconds.